SMI Arg Blocks.
Data Structures | |
| struct | IOLM_SMI_SVoidArgBlock |
| This structure is used as general and void ArgBlock. More... | |
| struct | IOLM_SMI_SJobError |
| This structure is used as JobError ArgBlock. More... | |
| struct | IOLM_SMI_SMasterident |
| This structure is used to get Master identification. More... | |
| struct | IOLM_SMI_SFSMasterAccess |
| This structure is used to get FS Master access. More... | |
| struct | IOLM_SMI_SFSCPAuthenticity |
| This structure is used to retrieve FSCPAuthenticity. More... | |
| struct | IOLM_SMI_SWMasterConfigListOld |
| This structure is obsolete. It used for the wireless Master configuration before V1.1.3 release. More... | |
| struct | IOLM_SMI_SWPortConfigList |
| This structure is used for the wireless port configuration. More... | |
| struct | IOLM_SMI_SWPortConfigListOld |
| This structure is obsolete. It used for the wireless port configuration before V1.1.3 release. More... | |
| struct | IOLM_SMI_SFSPortConfigList |
| This structure is used to store FS port configuration. More... | |
| struct | IOLM_SMI_SPortConfigList |
| This structure is used to store port configuration. More... | |
| struct | IOLM_SMI_SWPortStatusList |
| This structure is used to store wireless port status. More... | |
| struct | IOLM_SMI_V113_SWPortStatusList |
| This structure is used to store wireless port status in V1.1.3. More... | |
| struct | IOLM_SMI_SWTrackStatusList |
| This structure is used to store track status. More... | |
| struct | IOLM_SMI_SWScanConfigList |
| This structure is used to trigger a scan request. More... | |
| struct | IOLM_SMI_SWPairingList |
| This structure is used to trigger a pairing request. More... | |
| struct | IOLM_SMI_SWTrackConfigList |
| This structure is used for the track configuration. More... | |
| struct | IOLM_SMI_SPortStatusList |
| This structure is used to store port status. More... | |
| struct | IOLM_SMI_SPDIn |
| This structure is used for Process Data input. More... | |
| struct | IOLM_SMI_SPDOut |
| This structure is used for Process Data output. More... | |
| struct | IOLM_SMI_SPDInIQ |
| This structure is used for IQ input. More... | |
| struct | IOLM_SMI_SPDOutIQ |
| This structure is used for IQ output. More... | |
| struct | IOLM_SMI_SSPDUIn |
| This structure is used for SPDU input. More... | |
| struct | IOLM_SMI_SSPDUOut |
| This structure is used for SPDU output. More... | |
| struct | IOLM_SMI_SPDInOut |
| This structure is used for Process Data input and output read back. More... | |
| struct | IOLM_SMI_SFSPDInOut |
| This structure is used for FS Process Data input and output read back. More... | |
| struct | IOLM_SMI_SPortEvent |
| This generic structure is used for events. More... | |
| struct | IOLM_SMI_SScanResult |
| This structure is used for scan results. More... | |
| struct | IOLM_SMI_SScanStatusResult |
| This structure is used for a single scan result. More... | |
| struct | IOLM_SMI_SWScanStatusList |
| This structure is used for the Scan Status List. More... | |
| struct | IOLM_SMI_SWSingleScanStatusList |
| This structure is used for the Scan Status List of a single scan result. More... | |
| struct | IOLM_SMI_SOnRequestData |
| This structure is used for On-request Data. More... | |
| struct | IOLM_SMI_SPortPowerOffOn |
| This structure is used for PortPowerOffOn requests. More... | |
| struct | IOLM_SMI_SDSData |
| This structure is used for DataStorage Data. More... | |
| struct | IOLM_SMI_SHeader |
| SGI dependent types. More... | |
| struct | IOLM_SMI_SStdHeader |
| struct | IOLM_SMI_SArgBlockParam |
| This structure follows the IOLM_SMI_SHeader struct. More... | |
| struct | IOLM_SMI_SDeviceEvent |
| This structure is used for Device Events (remote). More... | |
| struct | IOLM_SMI_SPortEvent |
| This structure is used for port events (local). More... | |
Macros | |
| #define | IOLM_SMI_CLIENTID_INTERN (0xFE) |
| Used for internal communication. | |
| #define | IOLM_SMI_CLIENTID_BROADCAST (0x00) |
| Used for broadcasting (events). | |
| #define | IOLM_SGI_CLIENT_MAX_NAME_LENGTH (128u) |
| SGI dependent defines. | |
| #define | IOLM_SGI_AUTO_RELEASE_TIME_MIN (1u) |
| Minimal auto release timeout (in seconds) in case of idle communication state. | |
| #define | IOLM_SGI_AUTO_RELEASE_TIME_MAX (10u) |
| Maximal auto release timeout (in seconds) in case of idle communication state. | |
| #define | IOLM_SGI_EXCLUSIVE_ACYCLIC_TIMEOUT_MIN (1u) |
| Minimal release timeout (in seconds) in case of delegation of the exclusive rights. | |
| #define | IOLM_SGI_EXCLUSIVE_ACYCLIC_TIMEOUT_MAX (600u) |
| Maximal release timeout (in seconds) in case of delegation of the exclusive rights. | |
| #define | SGI_MANAGER_CLIENT_ID (240u) |
| The id of the client which is allowed to setup rights. | |
| #define | IOLM_SMI_PQI_PQ (1<<7) |
| #define | IOLM_SMI_PQI_DEVERR (1<<6) |
| #define | IOLM_SMI_PQI_DEVCOM (1<<5) |
| #define | IOLM_SMI_FEATURE_PARBATCHWRITE (1<<0) |
| #define | IOLM_SMI_FEATURE_PARBATCHREAD (1<<1) |
| #define | IOLM_SMI_FEATURE_POWEROFFON (1<<2) |
| #define | IOLM_SMI_ARGBLOCK_PDIN_LEN(Datalen) (sizeof(IOLM_SMI_SPDIn) - 32 + (Datalen)) |
| #define | IOLM_SMI_ARGBLOCK_PDOUT_LEN(Datalen) (sizeof(IOLM_SMI_SPDOut) - 32 + (Datalen)) |
| #define | IOLM_SMI_ARGBLOCK_SSPDUIN_LEN(Datalen) (sizeof(IOLM_SMI_SSPDUIn) - 32 + (Datalen)) |
| #define | IOLM_SMI_ARGBLOCK_SSPDUOUT_LEN(Datalen) (sizeof(IOLM_SMI_SSPDUOut) - 32 + (Datalen)) |
| #define | IOLM_SMI_ARGBLOCK_PDINOUT_LEN(InputLen, OutputLen) (4 + 2 + (InputLen) + (OutputLen)) |
| #define | IOLM_SMI_ARGBLOCK_FSPDINOUT_LEN(InputLen, OutputLen) (4 + 4 + (InputLen) + (OutputLen)) |
| #define | IOLM_SMI_ARGBLOCK_ONREQ_LEN(Datalen) (sizeof(IOLM_SMI_SOnRequestData) - IOLM_MAX_ISDU_LENGTH + Datalen) |
| #define | IOLM_SMI_ENDIAN_32(x) |
| #define | IOLM_SMI_ENDIAN_16(x) ( (((x) >> 8) & 0x00FF) | (((x) << 8) & 0xFF00) ) |
Typedefs | |
| typedef IOLM_SMI_SVoidArgBlock | IOLM_SMI_SGeneralArgBlock |
Enumerations | |
| enum | IOLM_SGI_SClientRole { IOLM_SMI_CLIENT_ROLE_NO_ACCESS = 0x00000000 , IOLM_SMI_CLIENT_ROLE_MASTER_SUPERUSER = 0x00000001 , IOLM_SMI_CLIENT_ROLE_MASTER_COMMISSIONING = 0x00000002 , IOLM_SMI_CLIENT_ROLE_PORT_SUPERUSER = 0x00000004 , IOLM_SMI_CLIENT_ROLE_DEVICE_COMMISSIONING = 0x00000008 , IOLM_SMI_CLIENT_ROLE_MONITORING = 0x00000010 } |
| SGI dependent enums. More... | |
| enum | IOLM_SGI_SRight { IOLM_SMI_PORT_NO_ACCESS = 0x00000000 , IOLM_SMI_PORT_CFG_WR_ACCESS = 0x00000001 , IOLM_SMI_PORT_CFG_RD_ACCESS = 0x00000002 , IOLM_SMI_PORT_PDIN_ACCESS = 0x00000004 , IOLM_SMI_PORT_ISDU_RD_ACCESS = 0x00000008 , IOLM_SMI_PORT_ISDU_WR_ACCESS = 0x00000010 , IOLM_SMI_PORT_ISDU_EXCLUSIVE = 0x00000020 , IOLM_SMI_PORT_PDOUT_ACCESS = 0x00000040 , IOLM_SMI_PORT_EVENT_SUBSCRIPTION = 0x00000080 , IOLM_SMI_PORT_TEMP_PDOUT_ACCESS = 0x00000100 , IOLM_SMI_PORT_FORCE_PDIN_ACCESS = 0x00000200 , IOLM_SMI_PORT_POWER_CFG_ACCESS = 0x00000400 , IOLM_SMI_MASTER_CFG_ACCESS = 0x00001000 , IOLM_SMI_TRACK_CFG_ACCESS = 0x00002000 } |
| enum | IOLM_SGI_EAccessCommand { IOLM_SGI_eSet = 0x00 , IOLM_SGI_eRemove = 0x01 , IOLM_SGI_eAdd = 0x02 } |
| enum | IOLM_SGI_EGatewayStatusInfo { IOLM_SGI_eStop = 0x00 , IOLM_SGI_eRunning = 0x01 , IOLM_SGI_eProcessDataOverride = 0x02 } |
| enum | IOLM_SMI_EServiceID { IOLM_SMI_eServiceID_MasterIdentification = 0x00 , IOLM_SMI_eServiceID_PortConfiguration = 0x01 , IOLM_SMI_eServiceID_ReadbackPortConfiguration = 0x02 , IOLM_SMI_eServiceID_PortStatus = 0x03 , IOLM_SMI_eServiceID_DSBackupToParServ = 0x04 , IOLM_SMI_eServiceID_DSRestoreFromParServ = 0x05 , IOLM_SMI_eServiceID_DeviceWrite = 0x06 , IOLM_SMI_eServiceID_DeviceRead = 0x07 , IOLM_SMI_eServiceID_PortPairing = 0x08 , IOLM_SMI_eServiceID_DeviceEvent = 0x09 , IOLM_SMI_eServiceID_PortEvent = 0x0A , IOLM_SMI_eServiceID_PDIn = 0x0B , IOLM_SMI_eServiceID_PDOut = 0x0C , IOLM_SMI_eServiceID_PDInOut = 0x0D , IOLM_SMI_eServiceID_PDInIQ = 0x0E , IOLM_SMI_eServiceID_PDOutIQ = 0x0F , IOLM_SMI_eServiceID_MasterConfiguration = 0x10 , IOLM_SMI_eServiceID_ReadbackMasterConfiguration = 0x11 , IOLM_SMI_eServiceID_TrackConfiguration = 0x12 , IOLM_SMI_eServiceID_ReadbackTrackConfiguration = 0x13 , IOLM_SMI_eServiceID_TrackScanResult = 0x14 , IOLM_SMI_eServiceID_TrackScanEnd = 0x15 , IOLM_SMI_eServiceID_TrackStatus = 0x16 , IOLM_SMI_eServiceID_Scan = 0x17 , IOLM_SMI_eServiceID_FSMasterAccess = 0x18 , IOLM_SMI_eServiceID_SPDUIn = 0x19 , IOLM_SMI_eServiceID_SPDUOut = 0x1A , IOLM_SMI_eServiceID_PortPowerOffOn = 0x1B , IOLM_SMI_eServiceID_FSPDInOut = 0x1C , IOLM_SMI_eServiceID_PDReadbackOutIQ = 0x1D , IOLM_SMI_V113_eServiceID_WMasterConfiguration = 0x20 , IOLM_SMI_V113_eServiceID_ReadbackWMasterConfiguration = 0x21 , IOLM_SMI_V113_eServiceID_WScanConfig = 0x22 , IOLM_SMI_V113_eServiceID_WScanStatus = 0x23 , IOLM_SMI_V113_eServiceID_WPortPairing = 0x24 , IOLM_SMI_V113_eServiceID_WTrackStatus = 0x25 , IOLM_SMI_V113_eServiceID_WQualityStatus = 0x26 , IOLM_SMI_eServiceID_GetChipInfo = 0x80 , IOLM_SMI_eServiceID_ResetDefaults = 0x81 , IOLM_SMI_eServiceID_Settings = 0x82 , IOLM_SMI_eServiceID_DataLog = 0x83 , IOLM_SMI_eServiceID_FWUpdate = 0x90 , IOLM_SMI_eServiceID_FSPDIn = 0xA0 , IOLM_SMI_eServiceID_FSPDOut = 0xA1 , IOLM_SMI_eServiceID_SCLEnabled = 0xA2 , IOLM_SMI_eServiceID_VerifyRecordSent = 0xA3 , IOLM_SMI_eServiceID_TestCommand = 0xA4 , IOLM_SMI_eServiceID_GatewayManagerIdentification = 0xB0 , IOLM_SMI_eServiceID_GatewayManagerStatus = 0xB1 , IOLM_SMI_eServiceID_RegisterClient = 0xB2 , IOLM_SMI_eServiceID_SetClientName = 0xB3 , IOLM_SMI_eServiceID_GetClientName = 0xB4 , IOLM_SMI_eServiceID_SetAccessRights = 0xB6 , IOLM_SMI_eServiceID_GetAccessRights = 0xB7 , IOLM_SMI_eServiceID_SetPDOutAccessRight = 0xB9 , IOLM_SMI_eServiceID_SubscribeForEvent = 0xBA , IOLM_SMI_eServiceID_GetEventSubscription = 0xBB , IOLM_SMI_eServiceID_TemporaryPDOutAccess = 0xBD , IOLM_SMI_eServiceID_ExclusiveAcyclicAccess = 0xBE , IOLM_SMI_eServiceID_ForcePDIn = 0xBF , IOLM_SMI_eServiceID_SetGWMAccessRights = 0xC0 , IOLM_SMI_eServiceID_GetGWMAccessRights = 0xC1 , IOLM_SMI_eServiceID_Unknown = 0xFE , IOLM_SMI_eServiceID_KeepAlive = 0xFF } |
| SMI ServiceIDs (IDs >= 0x80 are used for non standard, proprietary services). | |
| enum | IOLM_SMI_EArgBlockID { IOLM_SMI_eArgBlockID_Reserved = 0x0000 , IOLM_SMI_eArgBlockID_MasterIdent = 0x0001 , IOLM_SMI_eArgBlockID_FSMasterAccess = 0x0100 , IOLM_SMI_eArgBlockID_FSCPAuthenticity = 0x0101 , IOLM_SMI_eArgBlockID_WMasterConfig = 0x0200 , IOLM_SMI_eArgBlockID_PDIn = 0x1001 , IOLM_SMI_eArgBlockID_PDOut = 0x1002 , IOLM_SMI_eArgBlockID_PDInOut = 0x1003 , IOLM_SMI_eArgBlockID_SPDUIn = 0x1101 , IOLM_SMI_eArgBlockID_SPDUOut = 0x1102 , IOLM_SMI_eArgBlockID_FSPDInOut = 0x1103 , IOLM_SMI_eArgBlockID_PDInIQ = 0x1FFE , IOLM_SMI_eArgBlockID_PDOutIQ = 0x1FFF , IOLM_SMI_eArgBlockID_OnRequestDataWrite = 0x3000 , IOLM_SMI_eArgBlockID_OnRequestDataRead = 0x3001 , IOLM_SMI_eArgBlockID_DS_Data = 0x7000 , IOLM_SMI_eArgBlockID_DeviceParBatch = 0x7001 , IOLM_SMI_eArgBlockID_IndexList = 0x7002 , IOLM_SMI_eArgBlockID_PortPowerOffOn = 0x7003 , IOLM_SMI_eArgBlockID_WPortPairing = 0x7200 , IOLM_SMI_eArgBlockID_PortConfigList = 0x8000 , IOLM_SMI_eArgBlockID_FSPortConfigList = 0x8100 , IOLM_SMI_eArgBlockID_WTrackConfigList = 0x8200 , IOLM_SMI_eArgBlockID_WPortConfigList = 0x8201 , IOLM_SMI_eArgBlockID_WScan = 0x8202 , IOLM_SMI_eArgBlockID_PortStatusList = 0x9000 , IOLM_SMI_eArgBlockID_FSPortStatusList = 0x9100 , IOLM_SMI_eArgBlockID_WTrackStatusList = 0x9200 , IOLM_SMI_eArgBlockID_ScanResult = 0x9201 , IOLM_SMI_eArgBlockID_WPortStatusList = 0x9202 , IOLM_SMI_V113_eArgBlockID_WPortConfigList = 0x8200 , IOLM_SMI_V113_eArgBlockID_WScanConfigList = 0x8201 , IOLM_SMI_V113_eArgBlockID_WPortStatusList = 0x9200 , IOLM_SMI_V113_eArgBlockID_WScanStatusList = 0x9201 , IOLM_SMI_V113_eArgBlockID_WTrackStatusList = 0x9202 , IOLM_SMI_V113_eArgBlockID_WQualityStatusList = 0x9203 , IOLM_SMI_eArgBlockID_DeviceEvent = 0xA000 , IOLM_SMI_eArgBlockID_PortEvent = 0xA001 , IOLM_SMI_eArgBlockID_PDInAllConnectedPorts = 0xB001 , IOLM_SMI_eArgBlockID_PDInAllUpdatedPorts = 0xB002 , IOLM_SMI_eArgBlockID_PDOutMultiplePorts = 0xB003 , IOLM_SMI_eArgBlockID_PDInOutMultiplePorts = 0xB004 , IOLM_SMI_eArgBlockID_FSPDIn = 0xB101 , IOLM_SMI_eArgBlockID_FSPDOut = 0xB102 , IOLM_SMI_eArgBlockID_StackInformation = 0xE000 , IOLM_SMI_eArgBlockID_DataLog = 0xE001 , IOLM_SMI_eArgBlockID_TestCommand = 0xE002 , IOLM_SMI_eArgBlockID_Firmware = 0xE003 , IOLM_SMI_eArgBlockID_Settings = 0xE004 , IOLM_SMI_eArgBlockID_CPULoad = 0xE005 , IOLM_SMI_eArgBlockID_GatewayManagerIdentification = 0xFF00 , IOLM_SMI_eArgBlockID_GatewayManagerStatus = 0xFF01 , IOLM_SMI_eArgBlockID_RegisterClient = 0xFF02 , IOLM_SMI_eArgBlockID_SetClientName = 0xFF03 , IOLM_SMI_eArgBlockID_GetClientNameReq = 0xFF04 , IOLM_SMI_eArgBlockID_GetClientNameResp = 0xFF05 , IOLM_SMI_eArgBlockID_SetAccessRights = 0xFF06 , IOLM_SMI_eArgBlockID_GetAccessRightsReq = 0xFF07 , IOLM_SMI_eArgBlockID_GetAccessRightsResp = 0xFF08 , IOLM_SMI_eArgBlockID_SetPDOutAccessRight = 0xFF09 , IOLM_SMI_eArgBlockID_EventSubscription = 0xFF0A , IOLM_SMI_eArgBlockID_EventSubscriptionReq = 0xFF0B , IOLM_SMI_eArgBlockID_EventSubscriptionResp = 0xFF0C , IOLM_SMI_eArgBlockID_TemporaryPDOutAccess = 0xFF0D , IOLM_SMI_eArgBlockID_ExclusiveAcyclicAccess = 0xFF0E , IOLM_SMI_eArgBlockID_ForcePDIn = 0xFF0F , IOLM_SMI_eArgBlockID_SetGWMAccessRights = 0xFF10 , IOLM_SMI_eArgBlockID_GetGWMAccessRightsReq = 0xFF11 , IOLM_SMI_eArgBlockID_GetGWMAccessRightsResp = 0xFF12 , IOLM_SMI_eArgBlockID_VoidBlock = 0xFFF0 , IOLM_SMI_eArgBlockID_JobError = 0xFFFF } |
| SMI ArgBlock IDs. More... | |
| enum | IOLM_SMI_EMasterTypes { IOLM_SMI_eMasterTypes_Unspecific = 0 , IOLM_SMI_eMasterTypes_Reserved = 1 , IOLM_SMI_eMasterTypes_Master_acc = 2 , IOLM_SMI_eMasterTypes_FS_Master = 3 , IOLM_SMI_eMasterTypes_W_Master = 4 } |
| SMI Master types. | |
| enum | IOLM_SMI_EPortTypes { IOLM_SMI_ePortTypes_ClassA = 0 , IOLM_SMI_ePortTypes_ClassAWithPowerOffOn = 1 , IOLM_SMI_ePortTypes_ClassB = 2 , IOLM_SMI_ePortTypes_FSPortAWithoutOSSDe = 3 , IOLM_SMI_ePortTypes_FSPortAwithOSSDe = 4 , IOLM_SMI_ePortTypes_FSPortB = 5 , IOLM_SMI_ePortTypes_WMaster = 6 } |
| SMI port types. | |
| enum | IOLM_SMI_EPortMode { IOLM_SMI_ePortMode_DEACTIVATED = 0 , IOLM_SMI_ePortMode_IOL_MANUAL = 1 , IOLM_SMI_ePortMode_IOL_AUTOSTART = 2 , IOLM_SMI_ePortMode_DI_CQ = 3 , IOLM_SMI_ePortMode_DO_CQ = 4 , IOLM_SMI_ePortMode_SAFETYCOM = 49 , IOLM_SMI_ePortMode_OSSDE = 50 , IOLM_SMI_ePortMode_CYCLIC_AUTO = 52 , IOLM_SMI_ePortMode_CYCLIC = 53 , IOLM_SMI_ePortMode_ROAMING_AUTO = 54 , IOLM_SMI_ePortMode_ROAMING = 55 } |
| SMI port mode. | |
| enum | IOLM_SMI_EPortModeOld { IOLM_SMI_ePortModeOld_DEACTIVATED = 0 , IOLM_SMI_ePortModeOld_IOL_MANUAL = 1 , IOLM_SMI_ePortModeOld_IOL_AUTOSTART = 2 , IOLM_SMI_ePortModeOld_DI_CQ = 3 , IOLM_SMI_ePortModeOld_DO_CQ = 4 , IOLM_SMI_ePortModeOld_SAFETYCOM = 49 , IOLM_SMI_ePortModeOld_MIXEDSAFETYCOM = 50 , IOLM_SMI_ePortModeOld_OSSDE = 51 , IOLM_SMI_ePortModeOld_CYCLIC = 52 , IOLM_SMI_ePortModeOld_ROAMING = 53 } |
| SMI port mode (only used for compatibility to old V1.1). | |
| enum | IOLM_SMI_EPairCmd { IOLM_SMI_ePairCmd_Unpairing = 0 , IOLM_SMI_ePairCmd_PairingUnique = 1 , IOLM_SMI_ePairCmd_PairingButton = 2 , IOLM_SMI_ePairCmd_AbortPairing = 4 } |
| SMI pairing commands. | |
| enum | IOLM_SMI_EValidationBackup { IOLM_SMI_ePortValBack_NoDeviceCheck = 0 , IOLM_SMI_ePortValBack_V10 = 1 , IOLM_SMI_ePortValBack_V11 = 2 , IOLM_SMI_ePortValBack_V11_BackupRestore = 3 , IOLM_SMI_ePortValBack_V11_Restore = 4 } |
| SMI port validation and backup. | |
| enum | IOLM_SMI_EIQBehavior { IOLM_SMI_ePortIQBehavior_NotSupported = 0 , IOLM_SMI_ePortIQBehavior_DigitalInput = 1 , IOLM_SMI_ePortIQBehavior_DigitalOutput = 2 , IOLM_SMI_ePortIQBehavior_Power2 = 5 } |
| SMI port IQ behavior. | |
| enum | IOLM_SMI_EPortStatus { IOLM_SMI_ePortStatus_NO_DEVICE = 0 , IOLM_SMI_ePortStatus_DEACTIVATED = 1 , IOLM_SMI_ePortStatus_PORT_DIAG = 2 , IOLM_SMI_ePortStatus_RESERVED = 3 , IOLM_SMI_ePortStatus_OPERATE = 4 , IOLM_SMI_ePortStatus_DI_CQ = 5 , IOLM_SMI_ePortStatus_DO_CQ = 6 , IOLM_SMI_ePortStatus_OSSDE = 7 , IOLM_SMI_ePortStatus_SCL_ENABLED = 8 , IOLM_SMI_ePortStatus_PAIRING_FAULT = 10 , IOLM_SMI_ePortStatus_PORT_POWER_OFF = 254 , IOLM_SMI_ePortStatus_NOT_AVAILABLE = 255 } |
| SMI port status. | |
| enum | IOLM_SMI_ServiceTrackMode { IOLM_SMI_ServiceTrackMode_CYCLIC = 0 , IOLM_SMI_ServiceTrackMode_ROAMING = 1 } |
| SMI service track mode. | |
| enum | IOLM_SMI_ETrackMode { IOLM_SMI_eTrackMode_STOP = 0 , IOLM_SMI_eTrackMode_CYCLIC = 1 , IOLM_SMI_eTrackMode_ROAMING = 2 , IOLM_SMI_eTrackMode_SERVICE = 3 } |
| SMI track mode. | |
| enum | IOLM_SMI_ETrackStatus { IOLM_SMI_eTrackStatus_STOP = 0 , IOLM_SMI_eTrackStatus_CYCLIC = 1 , IOLM_SMI_eTrackStatus_ROAMING = 2 , IOLM_SMI_eTrackStatus_SCAN = 3 , IOLM_SMI_eTrackStatus_PAIRING = 4 } |
| SMI track status. | |
| enum | IOLM_SMI_EScanBehavior { IOLM_SMI_eScanBehavior_POLL_RESULT = 0 , IOLM_SMI_eScanBehavior_SINGLE_RESULT_BROADCAST = 1 , IOLM_SMI_eScanBehavior_FINAL_RESULT_BROADCAST = 2 } |
| SMI scan behavior. | |
| enum | IOLM_SMI_EScanStatus { IOLM_SMI_eScanStatus_NOT_PERFORMED_YET = 0 , IOLM_SMI_eScanStatus_IN_PROGRESS = 1 , IOLM_SMI_eScanStatus_ENDED = 2 } |
| SMI scan status. | |
| enum | IOLM_SMI_EPortPowerMode { IOLM_SMI_ePortPowerMode_ONE_TIME_SWITCH_OFF = 0 , IOLM_SMI_ePortPowerMode_OFF = 1 , IOLM_SMI_ePortPowerMode_ON = 2 } |
| SMI port power mode. | |
| #define IOLM_SGI_CLIENT_MAX_NAME_LENGTH (128u) |
SGI dependent defines.
Max lengh of the client name.
| #define IOLM_SMI_ENDIAN_32 | ( | x | ) |
| enum IOLM_SGI_SClientRole |
SGI dependent enums.
SMI client role
structure contains the roles of a smi client
IOLM_SMI_CLIENT_ROLE_NO_ACCESS: - Gateway management blocks the whole functionality (read/ write). Therefore, the IO-Link system is not visible from client point of view
IOLM_SMI_CLIENT_ROLE_MASTER_SUPERUSER: - Writable access to all services of Master / Port / Device
IOLM_SMI_CLIENT_ROLE_MASTER_COMMISSIONING : - Writable access to all services of Master/Port/Device except for output data
IOLM_SMI_CLIENT_ROLE_PORT_SUPERUSER: - Writable access to all services of Device
IOLM_SMI_CLIENT_ROLE_DEVICE_COMMISSIONING: - Writable access to all services of Device except for output data
IOLM_SMI_CLIENT_ROLE_MONITORING: - Readable access to all services of Master/Port/Device
| enum IOLM_SMI_EArgBlockID |
SMI ArgBlock IDs.
Coding: 0x N4 N3 N2 N1
N4 - Service group:
N3 - Domain:
N2/N1
For a list of all currently available ArgBlock IDs, see the overview above.