| Feature |
|---|
| PROFINET Isochronous mode support |
| PROFINET MRPD support |
| EtherNet/IP - Device Level Ring (DLR) Supervisor support added in the FWHAL. |
| HSR-PRP 100M support added. Refer HSR/PRP. |
| SOC | Supported CPUs | Boards | Host PC |
|---|---|---|---|
| AM261x | R5F | AM261x LaunchPad Revision A (referred to as am261x-lp in code). | Windows 10 64b or Ubuntu 18.04 64b or MacOS |
| Tools / SW module | Supported CPUs | Version |
|---|---|---|
| Code Composer Studio | R5F | 20.3.0 |
| SysConfig | R5F | 1.25.0, build 4268 |
| TI ARM CLANG | R5F | 4.0.3.LTS |
| MCU-PLUS-SDK-AM261X | R5F | 11.00.00.29 |
| FreeRTOS Kernel | R5F | 11.1.0 |
| LwIP | R5F | STABLE-2_2_1_RELEASE |
| Mbed-TLS | R5F | mbedtls-2.13.1 |
| ID | Head Line | Module | Applicable Releases | Resolution/Comments |
|---|---|---|---|---|
| PINDSW-7640 | Fix PHY LED configuration on DP83826E PHY Devices | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-8354 | Update ESI Product Code for AM26x platforms | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-8463 | Enable usage of ICSSM1 for EtherCAT on AM261x SysConfig | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-8469 | Remove IEP Clock Sync code sequence from application as the same is done from Sysconfig | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-8527 | Sync Jitter mismatch when Continous Sync Monitoring enabled in Acontis based MainDevices | EtherCAT SubDevice | 10.02.00 | More details in EtherCAT_SubDevice_Errata.pdf |
| PINDSW-9140 | Use MDIO link interrupt along with MII Link interrupt for improved link detection | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-9142 | Enable Enhanced Link by default in the EEPROM contents for ESC Configuration | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-9148 | Optimize MBX Write (FPWR) Path | EtherCAT SubDevice | 10.02.00 | More details in EtherCAT_SubDevice_Errata.pdf |
| PINDSW-9284 | Malformed packets observed in CTT (Conformance Test Tool) when using more than 4 SyncManagers | EtherCAT SubDevice | 10.02.00 | More details in EtherCAT_SubDevice_Errata.pdf |
| PINDSW-9412 | Sync0 drift happening after a month of continous run | EtherCAT SubDevice | 10.02.00 | More details in EtherCAT_SubDevice_Errata.pdf |
| PINDSW-9565 | Incorrect length computation for SM Write | EtherCAT SubDevice | 10.02.00 | More details in EtherCAT_SubDevice_Errata.pdf |
| PINDSW-9587 | Use IO Expander for programming MDIO MUX SEL in AM261x-LP RevA | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-9675 | Incorrect Interrupt Number used for bsp_global_mutex_lock and bsp_global_mutex_unlock | EtherCAT SubDevice | 10.02.00 | The interrupt number was not compensated correctly in bsp_global_mutex_lock() and bsp_global_mutex_unlock() |
| PINDSW-8027 | ISOM interrupt mode triggered at same time for both Ti and To interrupts | PROFINET Device | 10.02.00 | Separate interrupts configured for both Ti and To events. |
| PINDSW-8112 | Cycle time support for multiple of 125 us | PROFINET Device | 11.00.00 | All cycle time multiple of 125us(minimum 250us) are supported |
| PINDSW-9216 | Fix incorrect RTC3 port state during startup | PROFINET Device | 11.00.00 | RTC3 Port state set to "RUN" only after device in sync. |
| PINDSW-9237 | Incorrect dynamic cycle time configuration behavior | PROFINET Device | 11.00.00 | Cycle time can be re-configured without device power reset. |
| PINDSW-9553 | Fix DCP response sent when targeted to Port MAC address | PROFINET Device | 11.00.00 | DCP frames targeted to port MAC address are dropped |
| ID | Head Line | Module | Applicable Releases | Workaround |
|---|---|---|---|---|
| MCUSDK-14709 | Flash verification error: Read data using Flash_read does not match Flash_write data | Flash | 10.02.00 | Disable "--use_memcpy=fast" and "--use_memset=fast" flags in linker options. Also make sure 'Enable PHY Mode' is checked in Sysconfig OSPI module. |
| PINDSW-8498 | PPM frames transmit with incorrect cycle counter | PROFINET Device | 11.00.00 | Update cycle counter before transmission of PPM |
| PINDSW-8517 | SYNC1 Generated 1 cycle after first SYNC0 pulse when SYNC1 shift is configured from MainDevice | EtherCAT SubDevice | 10.02.00 | |
| PINDSW-8333 | Provide option for setting Sync ISR (FIQ) flag to reduce latency on SYNC0 interrupt | EtherCAT SubDevice | 10.02.00 | Modify PRUICSS_registerIrqHandler in mcu_plus_sdk\source\drivers\pruicss\m_v0\pruicss_m_v0.c with an additional argument for setting/unsetting FIQ: --- a/source/drivers/pruicss/m_v0/pruicss.h
+++ b/source/drivers/pruicss/m_v0/pruicss.h
@@ -427,6 +427,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
int32_t intrNum,
int32_t eventNum,
uint8_t waitEnable,
+ uint8_t isFIQFlagSet,
PRUICSS_IrqHandler irqHandler);
/**
diff --git a/source/drivers/pruicss/m_v0/pruicss_m_v0.c b/source/drivers/pruicss/m_v0/pruicss_m_v0.c
index 3a65ff4f..f61ed9c6 100644
--- a/source/drivers/pruicss/m_v0/pruicss_m_v0.c
+++ b/source/drivers/pruicss/m_v0/pruicss_m_v0.c
@@ -249,6 +249,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
int32_t intrNum,
int32_t eventNum,
uint8_t waitEnable,
+ uint8_t isFIQFlagSet,
PRUICSS_IrqHandler irqHandler)
{
PRUICSS_Object *object;
@@ -281,6 +282,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
/*TODO: Take priority as an argument to this function*/
hwiParams.priority = 0x1;
hwiParams.intNum = intrNum;
+ hwiParams.isFIQ = isFIQFlagSet;
hwiParams.callback = (HwiP_FxnCallback)PRUICSS_hwiIntHandler;
retVal = HwiP_construct(&(object->pruEvntOutFnMapArray[pruEvtoutNum].hwiObj), &hwiParams);
gmake -s -f makefile.am261x drivers_r5f.ti-arm-clang.freertos PROFILE=debug
gmake -s -f makefile.am261x drivers_r5f.ti-arm-clang.freertos PROFILE=release
|
This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.
| Module | Affected API | Change | Additional Remarks |
|---|---|---|---|
| EtherCAT SubDevice Beckhoff SSC Demo | N/A | Naming convention change from "EtherCAT slave" to "EtherCAT SubDevice" accross directories | The changes are applicable for TI EtherCAT Beckhoff SSC Demo at examples/industrial_comms/ethercat_subdevice_beckhoff_ssc_demo/ and TI EtherCAT SubDevice source directory at source/industrial_comms/ethercat_subdevice/ |
| EtherCAT SubDevice Demo | N/A | Naming convention change from "EtherCAT slave" to "EtherCAT SubDevice" accross directories | The changes are applicable only for TI Integrated EtherCAT Stack Examples at examples/industrial_comms/ethercat_subdevice_demo. Refer to EtherCAT TI Integrated Stack Release Notes |
| EtherNet/IP Adapter Demo | N/A | Refactor folder structures and naming convention for the Examples. | Refer to Overview of EtherNet/IP Adapter Demo |
| Module | Affected API | Change | Additional Remarks |
|---|---|---|---|
| PROFINET Device | setCpmDHT | Check updated API arguments | Change required to check for MRPD flag |
| PROFINET Device | insPpmList | Check updated API arguments | Change required to check for MRPD communication |
| PROFINET Device | insCpmList | Check updated API arguments | Change required to check for MRPD communication |
| PROFINET Device | PN_setCpmDHT | Check updated API arguments | Change required to check for MRPD flag |
| PROFINET Device | PN_insPpmList | Check updated API arguments | Change required to check for MRPD communication |
| PROFINET Device | PN_insCpmList | Check updated API arguments | Change required to check for MRPD communication |
| PROFINET Device | PN_MRP_setPortState | Check updated API arguments | Change required to check for MRPD communication |