EtherCAT SubDevice2.02.00
 
Loading...
Searching...
No Matches
Release Notes

Overview

The Software Development Kit (SDK) for EtherCAT allows you to quickly integrate EtherCAT SubDevice functionality into your device. The SDK is supported for Sitara processors by Texas Instruments Incorporated and currently available for AM64x, AM243x, AM263Px and AM261x series of Cortex®-R5 based devices.

This document collection contains a Quickstart Guide, the User Manual, and the API Reference Manual for the EtherCAT SubDevice SDK. The API consists of the following modules: an API to access the basic EtherCAT SubDevice functionality, the API for the CiA 402 (Drives and Motion Control), the cyclic buffer handling API, and a board support package API.

Licensing

Copyright © 2025, Texas Instruments Incorporated
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
  3. Neither the name of the Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Release Version 2.02.00

New Features:

  • [ICSTACK-394] Support Backup Parameter store and restore functionalityℹ️.
  • [ICSTACK-574] Activate Act/Link LED on LP-AM261x.
    • Change Act/Link LED blink rate to 50ms.
    • Adapt GPIO mapping in Sysconfig.
  • [ICSTACK-604] Rename ethercat_slave to ethercat_subdevice in ICSDK source path.
    • Adapt source path rename changes in source files.
    • Update documentation with source path rename changes.
  • [ICSTACK-681] Add Conformance Test Certificate for AM261x target.
  • [ICSTACK-669] Support both AM261x Rev.A Launchpad and AM261x Rev.E2 Launchpad boards.
    • Separate syscfg files are provided.
    • Setup section is updated for AM261x target.
  • [ICSTACK-617] Get PHY link polarity and PHY address from syscfg.
    • Application takes PHY link polarity and PHY address from syscfg.
  • [ICSTACK-739] Update EtherCAT SubDevice Simple-401 Demo in TwinCAT3 page.
    • Replace outdated screenshots and include additional screenshots for better user experience.
    • Enhance the instructions by updating existing steps and adding new ones to provide a more comprehensive guide.
  • [ICSTACK-751] Update Setup page.
    • Restructured the subsections and updated the images/links for improved user experience.
    • Revised the instructions to make them more concise and clear.

Bugfixes:

  • [ICSTACK-602] Add a mutex lock to NVM write request queue handling APIs.
    • Create a dedicated mutex lock for NVM write request queue access.
    • Renamed NVM error type 'NVM_ERR_SUCCESS' to 'NVM_SUCCESS'.
    • Update Non-Volatile Memory (NVM) documentation.
  • [ICSTACK-630] Fix statusWord not being updated from CiA402 state machine.
    • Create API to get the PDO type.
    • Create API to get the CiA402 axis activate status.
    • New APIs Signatures documented on API Changes.
  • [ICSTACK-584] Update makefile to correct Beckhoff custom SSC lib name and copy to expected location.
    • Custom SSC libs are copied to ethercat_subdevice\stack\lib directory.
  • [ICSTACK-666] Fix CiA402 state machine state after power up.
    • CiA402 default state is 'switch on disabled' after subdevice goes to OP state.
  • [ICSTACK-695] Fix CiA402 state machine state when ESM leaves OP state.
    • CiA402 state is switched to 'switch on disabled' after subdevice leaves from OP state.
  • [ICSTACK-720] Fix CiA402 drive function status update in application.
    • Added new API to get servo drive function status from the CIA402 state machine. Updated API Changes page.
    • Update all axis parameters in the motor control application.

Release Version 2.01.01

New Features:

  • [ICSTACK-493] Support AM261x/AM263Px on INDUSTRIAL-COMMUNICATIONS-SDK 10.02.
    Also containing support for:
    • CCS 12.8.1
    • SysConfig 1.23.0
    • TI Clang 4.0.1 LTS
    • OSAL 1.3.1
    • HWAL 2.1.0
  • [ICSTACK-133] Add Ethernet over EtherCAT example.
    • Add Ethernet over EtherCAT example for all targets.
    • Integrate LWIP library.
    • Add / Update Ethernet over EtherCAT documentation.

Release Version 2.01.00

New Features:

  • [ICSTACK-460] Support AM64x/AM243x on INDUSTRIAL-COMMUNICATIONS-SDK 11.00.
    Also containing support for:
    • CCS 12.8.1
    • SysConfig 1.22.0
    • TI Clang 4.0.1 LTS
    • OSAL 1.3.1
    • HWAL 2.1.0
  • [ICSTACK-312] Enable firmware update over FoE.
    • Firmware update is supported in Bootstrap state.
    • New API which is called during state transition from Init to Bootstrap.
    • New API which is called during state transition from Bootstrap to Init.
    • Updated File access over EtherCAT documentation page.
  • [ICSTACK-267] Adopt ETG naming convention.
    • Use of SubDevice and MainDevice.
    • Exception: No API name changes.
  • [ICSTACK-409] Remove PHY APIs from stack.
    • Remove: EC_API_SLV_cbRegisterPhyReset.
    • Remove: EC_API_SLV_cbRegisterPhyLibDetect.
    • Remove: EC_API_SLV_phyRegRead.
    • Remove: EC_API_SLV_phyRegWrite.
  • [ICSTACK-419] Update CiA402 documentation.
    • Added steps to extend the CiA402 example to 6-axis control.

Bugfixes:

  • [ICSTACK-307] Fix to Cycle Time Too Short Counter increment and Sync Error set at all DC cycle times.
    • Cycle Time Too Short Counter is incremented based on the PDI ISR period.
    • Macro SUPPORT_TI_ESC_CYCLE_EXCEEDED_COUNTER enables the PDI ISR period measurement.
  • [ICSTACK-312] Large size file download over FoE is supported.
    • Newer implementation for existing FoE APIs.
    • Large size files can be downloaded into the flash over FoE.
    • Newer implementation for NVM APIs to support auto erase during consecutive flash writes.
  • [ICSTACK-330] Fixed PDO mapping callback not triggered when PDO is assigned with mapping changes.
    • PDO mapping callback triggered when PDO is assigned with mapping changes.

Release Version 2.00.04

New Features:

  • [ICSTACK-279] Migration to latest INDUSTRIAL-COMMUNICATIONS-SDK 10.00.
    Also containing support for:
    • CCS 12.8.0
    • SysConfig 1.21.0
    • TI Clang 4.0.0 LTS
    • OSAL 1.3.0
    • HWAL 2.1.0
  • [ICSTACK-93] Create project for AM263Px LP.
    • Created new Code Composer Studio project for AM263PX LP and created documentation for the new platform.
  • [ICSTACK-235] Enable explicit device ID for EtherCATℹ️.
    Major changes:
    • New API to set the explicit device ID EC_API_SLV_setExplicitDeviceId.
    • New API to get the explicit device ID EC_API_SLV_getExplicitDeviceId.

Bugfixes:

  • [ICSTACK-197] Returning Error Code from AoE Callback functions will lead to timeout in MainDevice.
    • Return 32-bit error code to MainDevice.
  • [ICSTACK-223] Callback for mapping change is not triggered when reconfiguring PDOs with padded entries.
    • Callback is triggered when PDOs with padded entries are reconfigured from MainDevice.

Release Version 2.00.03

New Features:

  • [OSS1-2982] Add example documentation for usage of DP83826 PHY.
    Major changes:
    Add page which describes
    • what changes are necessary to the example code to use DP83826 PHY.
    • what changes are necessary to the Sysconfig file to use DP83826 PHY.

Release Version 2.00.02

New Features:

  • [ICSTACK-30] Migration to latest INDUSTRIAL-COMMUNICATIONS-SDK 09.02.
    Also containing support for:
    • OSAL 1.2.2
    • HWAL 2.0.2
    Further changes:
    • Rework of EC_API_SLV_load parameters to reduce stack size. Signature changes documented on API Changes.
    • Enabled DP83826 PHY in custom PHY library.
  • [ICSTACK-18] Stack size of PDI-, LED-, Sync0- and Sync1-Task configurable from application.
    Major changes:
    • Stack size of PDI-, Sync0- and Sync1-Task can be configured with EC_API_SLV_prepareTasks.
    • Signature changes documented on API Changes.
  • [ICSTACK-44] Increase stack size of PDI-, Sync0- and Sync1-Task.
    Major changes:
    • Stack size of PDI-, Sync0- and Sync1-Task increased.
    • Prevents memory overflow in memory demanding applications.
  • [OSS1-3289] Added memory configurator in SysConfig.
    Major changes:
    • Added memory configurator in SysConfig for demo applications.
    • Automatically generates linker.cmd file from SysConfig.
  • [OSS1-3288] Support for modelling the relation between Rx-PDOs and Tx-PDOs with EC_API_SLV_PDO_CBAssignmentChanges_t callback.
    Major changes:
    • The callback function use RxPDO and TxPDO reconfigure assignment map structures as a second and third parameter respectively.
    • The page Process data reconfiguration updated with new PDO assignment and mapping changes callback log screenshots.
    • Signature changes documented on API Changes.

Bugfixes:

  • Change ADS error size of AoE write and read request callbacks.
    • Change ADS error size of AoE write request callback EC_API_SLV_AoE_CBWriteRequestHandler_t.
    • Change ADS error size of AoE read request callback EC_API_SLV_AoE_CBReadRequestHandler_t.
    • Signature changes documented on API Changes.
  • [OSS1-3295] Process data input and output buffer callbacks receives invalid bit length.
    • Process data input buffer callbacks receive TxPDOs bit length.
    • Process data output buffer callbacks receive RxPDOs bit length.

Release Version 2.00.01

New Features:

  • [OSS1-3262] Migration to latest INDUSTRIAL-COMMUNICATIONS-SDK 09.02.
    Also containing support for:
    • CCS 12.7.0
    • SysConfig 1.20.0
    • TI Clang 3.2.2
    • OSAL 1.2.1
    • HWAL 2.0.1
  • [OSS1-3251] Access to PDO entry size in PDO mapping change callback function
    • PDO entry size change triggers the PDO mapping change callback.

Release Version 2.00.00

New Features:

  • [OSS1-2390] Ethernet over EtherCAT EoE
    Major changes:
    • Open API to implement third party TCP/IP Stacks.
    • Example provided for AM64x-EVM on Linux SDK.
    • Simple example mailbox size incremented to 1024 bytes.
  • [OSS1-2697] CoE complete access API updated
    • The API functions used for object complete access now have subIndex as parameter.
    • Only subIndex values 0 and 1 are valid.
  • [OSS1-2911] Update ESI files
    • Tested with EtherCAT Conformance Test Tool 2.5.0.
    • Added missing content.
    • Replaced all tabs by spaces.
  • [OSS1-2603] Allow applications without RX or TX Process Data
    • Input or output SyncManagers are not configured if RX or TX PDOs are not present.
  • [OSS1-2934] Remove base data types in the reserved index area
    • Data types from index 0x0260 till 0x07FF are removed.
    • Data type OCTET_STRING can be used instead of removed data type ARRAY_OF_SINT.
    • Data type UNICODE_STRING can be used instead of removed data type ARRAY_OF_INT.
  • [OSS1-2906] Support mapping of objects larger than 30 Bytes
    • Objects larger than 30 Bytes can be mapped now to the process data.
    • The documentation has been extended with more detailed information.
  • [OSS1-2966] Integration of INDUSTRIAL-COMMUNICATIONS-SDK 09.02.
    Also containing support for:
    • CCS 12.6.0
    • SysConfig 1.19.0
    • TI Clang 3.2.1
    • OSAL 1.2.0
    • HWAL 2.0.0
  • [OSS1-3067] Integrate NVM library for persistent data storage
    • EtherCAT examples updated with NVM library.
    • EtherCAT examples now use EEPROM and not Flash memory to store EtherCAT EEPROM data.
  • [OSS1-1043] File access over EtherCAT FoE
    • Demo supports the file transfer over EtherCAT
    • FoE APIs use NVM library to access the FoE data
    • The documentation has been extended with a new page for FOE.

Bugfixes:

  • [OSS1-2841] Disabled PDOs can't increase process data length
    • If a PDO is disabled, then the process data length is not updated.

Release Version 1.99.00

New Features:

  • [OSS1-1678] Refactoring of EtherCAT API
    Major changes:
    • All functions return uint32_t as error code
    • All functions use API handle as first parameter
    • API split in categorized header files
    • Signature changes documented on API Changes
  • [OSS1-1533] Fix CiA402 mode change problem
    Switching between drive modes (torque mode, velocity mode, position mode) that crashed the example application has been fixed.
  • [OSS1-2241] Fix CiA402 velocity mode
    If the target position was set to zero, the application was not performing any operation mode (csp, csv or cst).

Release Version 1.13.00

Bugfixes:

  • [OSS1-1476] Fix customer ssc
    missing diag file compile for customer ssc did cause linker error on customer compiled libs.
  • [OSS1-1302] Integration of latest INDUSTRIAL-COMMUNICATIONS-SDK 09.00. Also containing support for:
    • CCS 12.4
    • SysConfig 1.17.0
    • TI Clang 2.1.3
    • OSAL 1.01.01
    • HWAL 1.00.06
  • [OSS1-613] Upgrade to OSAL 1.1
    Fixed warnings and corrected inconsistencies between function names and arguments.
  • [OSS1-586] Bool and bit type objects in process data mapping.
    The process data offsets for types smaller than a byte has been fixed.
  • [OSS1-594] Fix record object names.
    The composed string for record objects is properly configured when: subIndexes are registered in an unsorted manner.
    no subIndexes registered between two of them.
  • [OSS1-596] Record entries registered in an unsorted manner are now shown correctly.

New Features:

  • [OSS1-1302] Update to INDUSTRIAL-COMMUNICATIONS-SDK 09.00.
    Integration into new SDK deployment structure of TI.
  • [OSS1-609] Integrate A53 -> R5F FBTL support.
  • [OSS1-597] Optimize record object configuration time.
  • [OSS1-633] Implement enumeration types in CoE Object Dictionary.
    Enumeration types now can be created and used in combination with variable, array and record objects.
  • [OSS1-615] Configure max subIndexes for SyncManager.
    SyncManager subIndex count is now freely configurable.
  • [OSS1-601] Signature change for EtherCAT state machine callbacks.
    Callbacks must return uint16_t value instead of EC_API_SLV_EUserRetCodes_t.
    uint16_t values must be AL Status codes defined in the stack.
  • [OSS-613] Upgrade to OSAL 1.1
    Fixed warnings and corrected inconsistencies between function names and arguments.
  • [OSS-586] Bool and bit type objects in process data mapping.
    The process data offsets for types smaller than a byte has been fixed.
  • [OSS-609] Integrate A53 -> R5F FBTL support.
    Simple and CTT demo did pass conformance tests.

ul> [OSS-597] Optimize record object configuration time. /ul>

  • [OSS-633] Implement enumeration types in CoE Object Dictionary.
    Enumeration types now can be created and used in combination with variable, array and record objects.
  • [OSS-615] Configure max subIndexes for SyncManager.
    SyncManager subIndex count is now freely configurable.
  • [OSS-601] Signature change for EtherCAT state machine callbacks.
    Callbacks must return uint16_t value instead of EC_API_SLV_EUserRetCodes_t.
    uint16_t values must be AL Status codes defined in the stack.

Release Version 1.12.02

New Features:

  • [OSS1-211] Add support for MCU+ SDK 08.06.00.22.

Release Version 1.12.01

  • [P2101-89] Add support for FBTL over UART. For testing purposes and prove of concept FBTL over UART line is added.

Release Version 1.12.00

New Features:

  • [DTKEC-1333] Add API to load custom PRU firmware from application.
  • [DTKEC-1184] Diagnosis history object 0x10F3 is now supported.
    New API implemented to enable the diagnosis object and to send diagnosis messages.

Bugfixes:

  • [DTKEC-1286] Correct duplicated error class entries EC_API_eERR_DEPRECATED, EC_API_eERR_GROUP_TYPE_NOT_SET
    The error entries previous contained the same ID. This has been corrected:
    1. EC_API_eERR_GROUP_TYPE_NOT_SET: 0x0039
    2. EC_API_eERR_DEPRECATED: 0x003A
  • [DTKEC-1295] Fix cppcheck usage
  • [DTKEC-1289] Add error code for object index below manufacturer specific area (0x2000)
    for these functions:
    1. EC_API_SLV_CoE_odAddVariable
    2. EC_API_SLV_CoE_odAddArray
    3. EC_API_SLV_CoE_odAddRecord
  • [DTKEC-1290] EC_API_SLV_PDO_createEntry returns an error code if an object without PDO mapping flag
    or incompatible flag is mapped to a PDO:
    1. EC_API_eERR_INVALID if object does not contain OBJACCESS_TXPDOMAPPING or OBJACCESS_RXPDOMAPPING flags.
    2. EC_API_eERR_INVALID if PDO is RX type and object contains only OBJACCESS_TXPDOMAPPING flag.
    3. EC_API_eERR_INVALID if PDO is TX type and object contains only OBJACCESS_RXPDOMAPPING flag.
  • [DTKEC-1345] Increase mailbox maximum size from 256 to 1024 Bytes.
  • [DTKEC-1270] Start and Stop output handler callbacks fixed for 2 CPU solution.
  • [DTKEC-1060] Array and Record objects with 255 subIndex never return from function.

Release Version 1.11.00

New Features:

  • [DTKEC-1251] Add support for mdio manual mode workaround
  • [DTKEC-1214] Refactor EC_API_SLV_setState function.
    Added error code parameter to inform about an application error.
  • [DTKEC-1088] Support for MCU+ SDK 8.05.00.01
  • [OSAL-315] Support for CCS 12.1 and SysCfg 1.14. (OSAL)
  • [OSAL-256] Support for CCS 12.1 and SysCfg 1.14. (HWAL)
  • [OSAL-257] OSAL V 1.00.09.
  • [OSAL-270] HWAL V 1.00.03.
    Improved license detection speed
  • [OSAL-315] Support MCU+ SDK 8.04.00.17.

Release Version 1.10.01

New Features:

  • [DTKEC-1191] Documentation improvements
    Changed placement of EtherCAT logo to top of documentation, grammatical corrections and minor formatting changes.

Release Version 1.10.00

New Features:

  • [OSAL-254] Support for CCS 12 and SysCfg 1.13. (OSAL)
  • [OSAL-256] Support for CCS 12 and SysCfg 1.13. (HWAL)
  • [OSAL-257] OSAL V 1.00.07.
  • [OSAL-270] HWAL V 1.00.01.
    Improved license detection speed

Bugfixes:

  • [DTKEC-339] F030h object description is corrupted after setting SubIdx 0 RW flag.
    F030h Object appears to be corrupted after calling the service DPR_eService_EC_CoESubIdx0WrFlag
    which sets the subIndex 0 with RW flag. By default array subIndex 0 flags use to be RO. This has been corrected

Release Version 1.09.00

New Features:

  • [OSAL-218] Support for MCU+ SDK 8.04.00.01.
  • [DTKEC-900] Added new tools for improved code quality.
    Extended existing and added static code analysis tools as well as automated additional tests in CI environment.

Bugfixes:

  • [DTKEC-840] Custom PHY Lib iterators caused data abort
    Custom PHY lib list handler did not properly check length of the list. This has been corrected.
  • [OSAL-218] Invalid PHY reset pins on AM243x LP
    Fixed syscfg error on Launchpad PHY reset lines (exchanged).

Release Version 1.08.00

New Features:

  • [DTKEC-956] Support for MCU+ SDK 8.03.00.05.

Bugfixes:

  • [DTKEC-852] Beckhoff Stack 5.13 fix bitmaps in ESI file
  • [DTKEC-933] Fix timeout issue on eval version.
    On specific circumstance eval limit was expired before expected.
  • [DTKEC-893] Register permission tests failing with 1.7.0 release
    Fix RegPerm set value where Bitwise or was logical or (by error)

Release Version 1.07.00

New Features:

  • [DTKEC-839] Add TI logo to ESI files
    Replaced generic logo icon in ESI with TI icon.
  • [DTKEC-825] Integrate Timesync Router configuration
    Added static Timesync Router configuration to DTK (PRU Integration).
  • [DTKEC-823] PRU/MDIO clock frequency change
    PRU/MDIO clock frequency increased to 333MHz to improve performance.
  • [DTKEC-822] Add support for MCU+ SDK 8.3.x
    Add SDK 8.3 basic support with experimental enhancement of PRU/MDIO API.
  • [DTKEC-824] Use newly created PRU firmware from changed path
  • [DTKEC-752] Minor documentation changes
    Minor changes in the documentation: corrected formatting in known issues, replace DTK with SDK, corrected link to FAQ.
  • [DTKEC-744] Customer Slave Sample Code (SSC) for Windows and Linux Operating Systems
    In ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/stack/patch there are a new makefile.custom-ssc and readme.md. Please follow the instructions in the readme.md to build your own SSC library from the available sources by ETG.
  • [DTKEC-453] Integrate Beckhoff Stack 5.13
    Customer Slave Sample Code (SSC) is compiled using Beckhoff Stack sources with a patch applied. Both patch and build process were adapted to the recently released SSC_V5i13.
  • [OSAL-148] OSAL revision 1.0.3
    Feature: new OSAL revision supporting MCU+ SDK 8.03.xx

Bugfixes:

  • [DTKEC-792] Hotfix custom SSC
    Some flags on custom built Beckhoff library have been missing blocking status/error LEDs and DC from working on customer created libbkhfSsc.a.
  • [DTKEC-748] Second Vendor ID is set in custom SSC
    Second vendor id was still shown on valid Beckhoff SSC compile.
  • [DTKEC-773] Custom PHY interface provided by stack.
    For evaluation hardware an example implementation is provided for DP83869.

Release Version 1.06.01

New Features:

  • [DTKEC-693] Build SSC Library with EC patch standalone
    Provide a patch for users to build the Beckhoff SSC Library with support for non-evaluation hardware.
  • [DTKEC-301] Test on AM243x EVM Hardware
    Stack on AM243x EVM passed ETG conformance tool automated tests.
  • [DTKEC-732] Integrate documentation of the OBD and Process Data configuration in Doxygen
    Extended documentation from ETG documents. See chapter EtherCAT SDK FAQ.

Bugfixes:

  • [DTKEC-742] Improve firmware load stability on AM243EVM and AM64EVM
    • a former need call has been removed, which makes download of EtherCAT SDK more likely successful
  • [DTKEC-730] Build Warning still prevalent on the AM243x LP
    Removed duplicate definitions from board config code.
  • [DTKEC-731] Solve issue of loading firmware to the core
    Removed stale MPU configuration entry from sysconfig for AM64x-EVM.

Release Version 1.06.00

New Features:

Bugfixes:

  • [DTKEC-673] FreeRTOS debug support
    • Fix linker files to make examples debuggable again
    • Reduce memory usage of IP protection security algorithms
  • [DTKEC-675] FreeRTOS thread stacks
    • Move thread stack variables to dedicated linker / memory section to avoid overwrite from stack manager

Release Version 1.05.02

Bugfixes:

  • [DTKEC-645] Version incorrectly displayed
    • Incorrect version was displayed in the previous release.

Release Version 1.05.01

Bugfixes:

  • [DTKEC-631] Datasheet memory information missing
    • Minor documentation corrections

Release Version 1.05.00

New Features:

  • [DTKEC-573] MCU+ SDK 8.01.00.35
    • Update to MCU+ SDK 8.01.00.35
  • [DTKEC-342] Protection of intellectual property
    • Add new chip-based license verification

Release Version 1.04.06

New Features:

  • [DTKEC-528] MCU+ SDK 8.01.00.26
    • Updated to MCU+ SDK 8.01.00.26 to and Code Composer 11

Release Version 1.04.05

New Features:

  • [DTKEC-474] Documentation
    • Update datasheet and add key performance parameter information
    • Remove references to SDK API from CiA-402 example
    • Fixed hyperlinks from Simple example documentation
  • [DTKEC-473] SysConfig AM243-EVM
    Remove obsolete DDR4 RAM entry from MPU configuration on AM64-EVM and AM243-EVM
  • [DTKEC-472] Analyze library size differences
    Use optimization for linkage Oz for all MCUs on FreeRTOS

Release Version 1.04.04

New Features:

  • [DTKEC-477] Automatic versioning
    Add automatic global versioning to demo apps and remove some compile time warning.

  • [DTKEC-448] Documentation automation
    Add size measurement to documentation

  • [DTKEC-403] Performance improvement
    Add measurement callback functions and additional APIs which allow to directly access CoE objects to improve performance while accessing objects in control cycle (e.g. CiA 402).

  • [DTKEC-455] Remove next steps to build an example
    Build an example description removed from documentation and replaced by Steps to Run the Example.

Release Version 1.04.03

New Features:

  • [DTKEC-372] Move "Supported Functionality" to the top level
    The "Supported Functionality" section in the documentation has been moved from "General Information" to the top-level.

  • [DTKEC-402] Project name change
    The project name has been changed from ethercat_linux to product_ethercat_slave.

  • [DTKEC-381] Reduce memory footprint

    Stack is now compiled with THUMB mode. Additionally, the ESI parser has been moved to the application.

  • [DTKEC-394] Suppress linker warnings
    The linker warnings have been corrected.

  • [DTKEC-395] OSAL_error 0x40000001 EC
    Missing defines have been added to TI shipped example.projectspec(s) accordingly

  • [DTKEC-396] MCU+ SDK 8.01.00.10 Support
    EtherCAT has been updated to support MCU+SDK 8.01.00.10.

  • [DTKEC-398] AM243x Heap size
    The heap size for the AM243x applications has been reduced.

Release Version 1.04.02

New Features:

  • [DTKEC-343] MCU+ SDK 8.01.00.02 Support
    MCU+ SDK 8.01.0.02 is now supported.
  • [DTKEC-243] Run and Error LED migrated TEST_LED_1 and TEST_LED_2
    The run and error LEDs have been migrated to TEST_LED_1 and TEST_LED_2, respectively.
  • [DTKEC-167] Memory allocation reduction
    The dynamically allocated memory footprint of the stack has been reduced. Additionally, the stack
    memory access has been migrated from DDR to MSRAM.

Bug Fixes:

  • [DTKEC-348] Both ports not working with AM243x LP
    Corrected issue with no communication on the second port.
  • [DTKEC-334] Update linker files to load apps only from MSRAM
    The linker scripts were not fully adjusted to support MSRAM. This has been corrected.
  • [DTKEC-318] Repeating "Data Transfer failed with transfer status -2" Message
    The "Data Transfer failed with transfer status -2" message that repeatedly displayed in the console output has been resolved.

Release Version 1.04.01

New Features:

  • [DTKEC-303] Create Project for AM243X EVM
    Created new Code Composer Studio project for AM243X EVM and created documentation for the new platform.

Bug Fixes:

  • [DTKEC-317] Fix startup stability issue
    Allocation of the stack size has been changed to the expected value. The larger size led to instabilities while booting up.

Release Version 1.04.00

New Features:

  • [DTKEC-256] MCU+ SDK 08.00.00.08 Support
    EtherCAT has been updated to support MCU+ SDK 08.00.00.08.
  • [DTKEC-283] Create Project for AM24X
    Created new Code Composer Studio project for AM243 and created documentation for the new platform.

Bug Fixes:

  • [DTKEC-250] Fix ESI file content for Simple, CTT and CIA402
    Corrected inconsistencies between all ESI files.
  • [DTKEC-247] AM64x ESI file fix
    Corrected access to PDO Mapping.

Release Version 1.03.01

New Features:

  • [DTKEC-237] AM64 Demo refactoring
    Split of OS and MCU support files in DemoApps
    Add conformance test tool Demo sources
    Add CiA402 Demo sources

Release Version 1.03.00

New Features:

  • [DTKEC-162] CiA402 3 axes application example
    Configuration of the CiA402 Object Dictionary and Process Data mapping described on ETG6010 Chapter 11 & 16.
    ESI File (EtherCAT Device Description file) for the CiA402 example.
    CiA402 state machine test. CiA402 is based on a state machine described in ETG6010 Chapter 5.
  • [DTKEC-147] Set GroupType Parameter from ESI Parser
    GroupType parameter describes which set of devices the SubDevice is associated with. This parameter is set on the ESI file as well as on the EEPROM.

  • [DTKEC-200] Images in Quickstart are not up to date
    The Quickstart guide images are not representative (release V1.3.0) and have been updated.

Bug Fixes:

  • [DTKEC-228] AM64 Startup problems corrected
    Updated to support MCU plus 7.3.1.07.

Release Version 1.02.03

New Features:

  • [P2102-1] EtherCAT AM64 Porting to FreeRTOS
    Support for FreeRTOS R5 on AM64 controller has been added. Tickets included: P2101-2->9; P2101-11->16; P2101-19->29
  • [DTKEC-197] AM64x FreeRTOS update to MCU plus 7.3.0.18
    Updated to support MCU plus 7.3.0.18.

Release Version 1.02.00

New Features:

  • [DTKEC-180] EtherCAT AM64 Porting to TI-RTOS
    Support for AM64x (BETA) based on TI-RTOS SDK 7.2.1.11

  • [DTKEC-163] SDK Migration to TI SDK 7.0.1.6
    Updated to support TI SDK 7.0.1.6

Release Version 1.01.01

New Features:

  • Abstraction Layer baseline adopted to migrate to SDK7 in next Release

Release Version 1.01.00

New Features:

  • Initial Release

‍ℹ️ This feature is part of premium SDK. In case you are using standard and need premium, please contact your regional TI sales representative for additional details.