AM261x MCU+ SDK  10.02.00

Detailed Description

Structure containing parameters for STC module configuration.

Data Fields

uint32_t lpScanMode
 
uint32_t codecSpreadMode
 
uint32_t capIdleCycle
 
uint32_t scanEnHighCap_idleCycle
 

Field Documentation

◆ lpScanMode

uint32_t SDL_STC_ScanModeconfig::lpScanMode

Scan mode configuration. Fixed Configuration – Only this configuration value is supported.

◆ codecSpreadMode

uint32_t SDL_STC_ScanModeconfig::codecSpreadMode

Scan mode configuration. Fixed Configuration – Only this configuration value is supported

◆ capIdleCycle

uint32_t SDL_STC_ScanModeconfig::capIdleCycle

Scan mode configuration. Fixed Configuration – Only this configuration value is supported

◆ scanEnHighCap_idleCycle

uint32_t SDL_STC_ScanModeconfig::scanEnHighCap_idleCycle

Scan mode configuration. Fixed Configuration – Only this configuration value is supported