AM261x MCU+ SDK  10.02.00
APIs for CCM MODULE

Introduction

The SDL CCM module provides API for CCM Diagnostics

Sub Modules

 CCM API
 
 CCM Low-Level API
 

Typedefs

typedef uint32_t SDL_CCM_Inst
 CCM Instance supported. More...
 

Macros

#define SDL_CCM_ESM_U_BASE   (SDL_ESM0_CCM_0_SELFTEST_ERR)
 
#define SDL_INTR_GROUP_NUM   1U
 
#define BASEADDRESS   SDL_R5SS0_CCMR_U_BASE
 
#define ESM_INSTANCE   SDL_ESM_INST_MAIN_ESM0
 
#define SDL_R5SS0_CCM   0U
 
#define SDL_CCM_MAX_INSTANCE   (SDL_R5SS0_CCM + 1U)
 

Macro Definition Documentation

◆ SDL_CCM_ESM_U_BASE

#define SDL_CCM_ESM_U_BASE   (SDL_ESM0_CCM_0_SELFTEST_ERR)

◆ SDL_INTR_GROUP_NUM

#define SDL_INTR_GROUP_NUM   1U

◆ BASEADDRESS

#define BASEADDRESS   SDL_R5SS0_CCMR_U_BASE

◆ ESM_INSTANCE

#define ESM_INSTANCE   SDL_ESM_INST_MAIN_ESM0

◆ SDL_R5SS0_CCM

#define SDL_R5SS0_CCM   0U

CCM INSTANCE R5F0

◆ SDL_CCM_MAX_INSTANCE

#define SDL_CCM_MAX_INSTANCE   (SDL_R5SS0_CCM + 1U)

Maximum

Typedef Documentation

◆ SDL_CCM_Inst

typedef uint32_t SDL_CCM_Inst

CCM Instance supported.

Variable Documentation

◆ SDL_CCM_baseAddress

uint32_t SDL_CCM_baseAddress[SDL_CCM_MAX_INSTANCE]
static
Initial value:
=
{
SDL_R5SS0_CCMR_U_BASE,
}

This API is used to get the base address of the instance.