AM261x MCU+ SDK  10.02.00
APIs for Secure IPC Notify

Introduction

See SIPC Notify for more details.

Data Structures

struct  SIPC_Params
 Parameters used by SIPC_init. More...
 
struct  SIPC_SwQueue
 SIPC swQ structure which holds the data pointer to a fifo Queue in HSM MBOX memory. More...
 

Functions

void SIPC_Params_init (SIPC_Params *params)
 Set default value to SIPC_Params. More...
 
int32_t SIPC_init (SIPC_Params *params)
 Initialize Secure IPC notify module. More...
 
void SIPC_deInit (void)
 De-initialize secure IPC Notify module. More...
 
int32_t SIPC_sendMsg (uint8_t remoteSecCoreId, uint8_t remoteClientId, uint8_t localClientId, uint8_t *msgValue, SIPC_fifoFlags waitForFifoNotFull)
 Send message to a specific remote core and specific client ID on that remote core. More...
 
int32_t SIPC_registerClient (uint8_t localClientId, SIPC_FxnCallback msgCallback, void *args)
 Register a callback to handle messages received from a specific remote core and for a specific local client ID. More...
 
int32_t SIPC_unregisterClient (uint16_t localClientId)
 Un-register a previously registered callback. More...
 
uint32_t SIPC_getSelfCoreId (void)
 Return current core ID. More...
 
uint32_t SIPC_getSelfSecMasterId (void)
 Return current core sec master ID. More...
 
uint32_t SIPC_isCoreEnabled (uint32_t coreId)
 Check if a core is enabled for SIPC. More...
 

Typedefs

typedef void(* SIPC_FxnCallback) (uint8_t remoteSecCoreId, uint8_t localClientId, uint8_t remoteClientId, uint8_t *msgValue, void *args)
 User callback that is invoked when a message is received from a reote core for a given client ID. More...
 

Enumerations

enum  SIPC_fifoFlags { ABORT_ON_FIFO_FULL, WAIT_IF_FIFO_FULL }
 flags to pass with the SIPC_sendMsg Api which indicates the flow of execution when the write FIFO is full More...
 
enum  SIPC_coreId {
  CORE_ID_R5FSS0_0 = 0, CORE_ID_R5FSS0_1, CORE_ID_R5FSS1_0, CORE_ID_R5FSS1_1,
  CORE_ID_HSM0_0, CORE_ID_MAX
}
 Core Ids to identify different cores. More...
 
enum  SIPC_SecCoreId { CORE_INDEX_SEC_MASTER_0 = 0, CORE_INDEX_SEC_MASTER_1, CORE_INDEX_HSM, MAX_SEC_CORES_WITH_HSM }
 Secure host Id to identify different secure hosts. Max number of secure host on AM263x is 2. More...
 

Typedef Documentation

◆ SIPC_FxnCallback

typedef void(* SIPC_FxnCallback) (uint8_t remoteSecCoreId, uint8_t localClientId, uint8_t remoteClientId,uint8_t *msgValue, void *args)

User callback that is invoked when a message is received from a reote core for a given client ID.

Before invoking the API, the IPC module would have 'popped` the message from the HW or SW FIFO already. This callback is called frm ISR context, so all constraints of ISR should be applied by the callback, e.g. no blocking wait, quickly handle message and exit ISR.

For most applications, it is recommended to put the message value into a local SW queue and defer the message handling itself to a application task.

Note
This callback will process the *msgValue . Registered function should not be blocking. as this is called from isr context.
Parameters
remoteSecCoreId[in] Remote core that has sent the message
localClientId[in] Local client ID to which the message is sent
remoteClientId[in] remote client Id from which this message has been sent
msgValue[in] pointer to the buffer with SIPC_MSG_SIZE elements
args[in] Argument pointer passed by user when SIPC_registerClient is called

Enumeration Type Documentation

◆ SIPC_fifoFlags

flags to pass with the SIPC_sendMsg Api which indicates the flow of execution when the write FIFO is full

Enumerator
ABORT_ON_FIFO_FULL 
WAIT_IF_FIFO_FULL 

◆ SIPC_coreId

Core Ids to identify different cores.

Enumerator
CORE_ID_R5FSS0_0 
CORE_ID_R5FSS0_1 
CORE_ID_R5FSS1_0 
CORE_ID_R5FSS1_1 
CORE_ID_HSM0_0 
CORE_ID_MAX 

◆ SIPC_SecCoreId

Secure host Id to identify different secure hosts. Max number of secure host on AM263x is 2.

Enumerator
CORE_INDEX_SEC_MASTER_0 
CORE_INDEX_SEC_MASTER_1 
CORE_INDEX_HSM 
MAX_SEC_CORES_WITH_HSM 

Function Documentation

◆ SIPC_Params_init()

void SIPC_Params_init ( SIPC_Params params)

Set default value to SIPC_Params.

Parameters
params[out] Default initialized structure

◆ SIPC_init()

int32_t SIPC_init ( SIPC_Params params)

Initialize Secure IPC notify module.

This API will initialize the HW used for IPC including registering interrupts for receiving messages.

Parameters
params[in] Initializaion parameters

◆ SIPC_deInit()

void SIPC_deInit ( void  )

De-initialize secure IPC Notify module.

This API will de-initialize the HW used for IPC including un-registering interrupts for receiving messages.

◆ SIPC_sendMsg()

int32_t SIPC_sendMsg ( uint8_t  remoteSecCoreId,
uint8_t  remoteClientId,
uint8_t  localClientId,
uint8_t *  msgValue,
SIPC_fifoFlags  waitForFifoNotFull 
)

Send message to a specific remote core and specific client ID on that remote core.

Note
To reduce latency, error checks are avoided in this API. Users need to make sure the client ID value is < SIPC_CLIENT_ID_MAX and message value is < SIPC_CLIENT_ID_MAX
This API can be called from within ISRs and is also thread-safe. Internally this API disables interrupts for a short while to make the API ISR and thread safe.
One cannot send messages to self, i.e remoteCoreId, cannot be same as core ID of the CPU that called this API.
Parameters
remoteSecCoreId[in] Remote core to sent message to, see
remoteClientId[in] Remote core client ID to send message to
localClientId[in] self core client ID from which the meessage is being sent
msgValue[in] Message value to send, MUST be < IPC_NOTIFY_MSG_VALUE_MAX
waitForFifoNotFull[in] 1: wait for message to be inserted into HW or SW FIFO [in] 0: if FIFO is full, dont send message and return with error.
Returns
SystemP_SUCCESS, message sent successfully
SystemP_FAILURE, message could not be sent since HW or SW FIFO for holding the message is full.

◆ SIPC_registerClient()

int32_t SIPC_registerClient ( uint8_t  localClientId,
SIPC_FxnCallback  msgCallback,
void *  args 
)

Register a callback to handle messages received from a specific remote core and for a specific local client ID.

Parameters
localClientId[in] Client ID to which the message has been sent
msgCallback[in] Callback to invoke, if callback is already registered, error will be returned.
args[in] User arguments, that are passed back to user when the callback is invoked
Returns
SystemP_SUCCESS, callback registered sucessfully
SystemP_FAILURE, callback registration failed, either remoteCoreId or localClientId is invalid or callback already registered.

◆ SIPC_unregisterClient()

int32_t SIPC_unregisterClient ( uint16_t  localClientId)

Un-register a previously registered callback.

Parameters
localClientId[in] Client ID to which the message has been sent
Returns
SystemP_SUCCESS, callback un-registered sucessfully
SystemP_FAILURE, callback un-registration failed, either remoteCoreId or localClientId is invalid

◆ SIPC_getSelfCoreId()

uint32_t SIPC_getSelfCoreId ( void  )

Return current core ID.

Returns
Core ID, see SIPC_coreId for valid values.

◆ SIPC_getSelfSecMasterId()

uint32_t SIPC_getSelfSecMasterId ( void  )

Return current core sec master ID.

Returns
Core ID, see SIPC_SecCoreId for valid values.

◆ SIPC_isCoreEnabled()

uint32_t SIPC_isCoreEnabled ( uint32_t  coreId)

Check if a core is enabled for SIPC.

Parameters
coreId[in] Core ID, see SIPC_coreId for valid values.
Returns
1: core is enabled for SIPC, 0: core is not enabled for SIPC