AM261x INDUSTRIAL COMMUNICATIONS SDK  10.02.00

Introduction

Functions

void EIP_drvInit (EIP_Handle icssEipHandle)
 Initialization routine for Ethernet/IP driver functions. More...
 
void EIP_drvStop (EIP_Handle icssEipHandle)
 EIP driver stop API. More...
 
void EIP_drvStart (EIP_Handle icssEipHandle)
 EIP driver start API. More...
 
void EIP_processProtocolFrames (uint32_t *queue_number, void *userArg)
 API to process the real time Packets. More...
 
int8_t EIP_initializeCIPSync (EIP_Handle icssEipHandle)
 API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based on PTP implementation. More...
 
int32_t EIP_configureLLDPForwarding (EIP_Handle icssEipHandle, uint8_t enableFeature)
 API to configure the LLDP forwarding to the other port. More...
 
int32_t EIP_configureLLDPFwdHelper (uint32_t pruBaseAddress, uint8_t val)
 API to configure the value stored at the required offset in ICSS SMEM. More...
 

Function Documentation

◆ EIP_drvInit()

void EIP_drvInit ( EIP_Handle  icssEipHandle)

Initialization routine for Ethernet/IP driver functions.

    This API does the following functionalities:
        Loads the firmware on PRU0 and PRU1 cores
        Call DLR init API
        Call TimeSync(PTP) init API
Parameters
icssEipHandle[in] EIP handle

◆ EIP_drvStop()

void EIP_drvStop ( EIP_Handle  icssEipHandle)

EIP driver stop API.

    This API stops DLR and disables PTP
Parameters
icssEipHandle[in] EIP handle

◆ EIP_drvStart()

void EIP_drvStart ( EIP_Handle  icssEipHandle)

EIP driver start API.

    This API starts DLR and enables PTP
Parameters
icssEipHandle[in] EIP handle

◆ EIP_processProtocolFrames()

void EIP_processProtocolFrames ( uint32_t *  queue_number,
void *  userArg 
)

API to process the real time Packets.

    This API will be registered as Real Tme Rx Call back. Incase of EIP, the driver
    receives DLR and PTP packets. This API receives the packet, checks the packet
    type and passes the packet to DLR driver or PTP driver
Parameters
queue_number[in] Queue where the packet is present
userArg[in] userArgumment. EIP handle

◆ EIP_initializeCIPSync()

int8_t EIP_initializeCIPSync ( EIP_Handle  icssEipHandle)

API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based on PTP implementation.

Parameters
icssEipHandle[in] EIP handle
Return values
0- On success <0 - On failure

◆ EIP_configureLLDPForwarding()

int32_t EIP_configureLLDPForwarding ( EIP_Handle  icssEipHandle,
uint8_t  enableFeature 
)

API to configure the LLDP forwarding to the other port.

Parameters
icssEipHandle[in] EIP handle
enableFeature[in] Option to enable or disable the LLDP forwarding 1 - Feature is enabled 0 - Feature is disabled
Return values
0- On success <0 - On failure

◆ EIP_configureLLDPFwdHelper()

int32_t EIP_configureLLDPFwdHelper ( uint32_t  pruBaseAddress,
uint8_t  val 
)

API to configure the value stored at the required offset in ICSS SMEM.

Parameters
pruBaseAddress[in] PRU Base Address
val[in] Value to program at the SMEM address
Return values
0- On success <0 - On failure