Structure containing the port delay values of the local and remote.
Data Fields | |
uint32_t | rxDelayLocal |
uint32_t | txDelayLocal |
uint32_t | rxDelayRemote |
uint32_t | txDelayRemote |
uint32_t | cableDelay |
uint32_t ptcpPortDelayVal_t::rxDelayLocal |
Local RX port delay
uint32_t ptcpPortDelayVal_t::txDelayLocal |
Local TX port delay
uint32_t ptcpPortDelayVal_t::rxDelayRemote |
Remote RX port delay
uint32_t ptcpPortDelayVal_t::txDelayRemote |
Remote TX port delay
uint32_t ptcpPortDelayVal_t::cableDelay |
Cable delay calculated by device