LRE Interface Statistics.
Data Fields | |
| uint32_t | cntUniqueA |
| uint32_t | cntUniqueB |
| uint32_t | cntDuplicateA |
| uint32_t | cntDuplicateB |
| uint32_t | cntMultiA |
| uint32_t | cntMultiB |
| uint32_t | cntRxA |
| uint32_t | cntRxB |
| uint32_t | cntTxA |
| uint32_t | cntTxB |
| uint32_t | cntOwnRxA |
| uint32_t | cntOwnRxB |
| uint32_t | cntErrWrongLanA |
| uint32_t | cntErrWrongLanB |
| uint32_t | cntErrorsA |
| uint32_t | cntErrorsB |
| uint32_t | cntUniqueC |
| uint32_t | cntDuplicateC |
| uint32_t | cntMultiC |
| uint32_t | cntRxC |
| uint32_t | cntTxC |
| uint32_t | cntErrWrongLanC |
| uint32_t | cntErrorsC |
| uint32_t | cntNodes |
| uint32_t | cntProxyNodes |
| uint32_t lreStatistics::cntUniqueA |
Number of entries in the duplicate detection mechanism on port A for which no duplicate was received
| uint32_t lreStatistics::cntUniqueB |
Number of entries in the duplicate detection mechanism on port B for which no duplicate was received
| uint32_t lreStatistics::cntDuplicateA |
Number of entries in the duplicate detection mechanism on port A for which one single duplicate was received
| uint32_t lreStatistics::cntDuplicateB |
Number of entries in the duplicate detection mechanism on port B for which one single duplicate was received
| uint32_t lreStatistics::cntMultiA |
Number of entries in the duplicate detection mechanism on port A for which more than one duplicate was received
| uint32_t lreStatistics::cntMultiB |
Number of entries in the duplicate detection mechanism on port B for which more than one duplicate was received
| uint32_t lreStatistics::cntRxA |
Number of frames received on the LRE port A
| uint32_t lreStatistics::cntRxB |
Number of frames received on the LRE port B
| uint32_t lreStatistics::cntTxA |
Number of frames sent over port A that are HSR tagged
| uint32_t lreStatistics::cntTxB |
Number of frames sent over port B that are HSR tagged
| uint32_t lreStatistics::cntOwnRxA |
Number of HSR tagged frames received on port A that originated from this device
| uint32_t lreStatistics::cntOwnRxB |
Number of HSR tagged frames received on port B that originated from this device
| uint32_t lreStatistics::cntErrWrongLanA |
Number of frames with the wrong LAN identifier received on the LRE port A
| uint32_t lreStatistics::cntErrWrongLanB |
Number of frames with the wrong LAN identifier received on the LRE port B
| uint32_t lreStatistics::cntErrorsA |
Number of frames with errors received on the LRE port A
| uint32_t lreStatistics::cntErrorsB |
Number of frames with errors received on the LRE port B
| uint32_t lreStatistics::cntUniqueC |
Number of entries in the duplicate detection mechanism on application interface for which no duplicate was received
| uint32_t lreStatistics::cntDuplicateC |
Number of entries in the duplicate detection mechanism on the application interface of the DAN for which one single duplicate was received
| uint32_t lreStatistics::cntMultiC |
Number of entries in the duplicate detection mechanism on the application interface of the DAN for which more than one duplicate was received
| uint32_t lreStatistics::cntRxC |
Number of frames received from the application interface of the DAN
| uint32_t lreStatistics::cntTxC |
Number of frames sent towards the application interface of the DAN
| uint32_t lreStatistics::cntErrWrongLanC |
Number of frames with the wrong LAN identifier received on the interlink
| uint32_t lreStatistics::cntErrorsC |
Number of frames with errors received on the application interface of the DAN
| uint32_t lreStatistics::cntNodes |
Number of entries in the node table
| uint32_t lreStatistics::cntProxyNodes |
Number of entries in the proxy table