Functions | |
| int32_t | PN_setWatchDogTimer (PN_Handle pnHandle, int32_t timerPeriod) |
| API to configure the ICSS watchdog expiry duration. More... | |
Macros | |
| #define | watchDogExpireDuration 7000 |
| #define watchDogExpireDuration 7000 |
ICSS WatchDog Expiry duration in milli seconds
| int32_t PN_setWatchDogTimer | ( | PN_Handle | pnHandle, |
| int32_t | timerPeriod | ||
| ) |
API to configure the ICSS watchdog expiry duration.
| pnHandle | Profinet Handle | |
| [in] | timerPeriod | Time duration (in milliseconds) after which watchdog expires if not tapped in-between. Valid range is from 2 ms to 6553 ms |
| 0 | on success |