AM243x INDUSTRIAL COMMUNICATIONS SDK  2025.00.00

Introduction

Functions

void LRE_open (Lre_Handle lreHandle)
 Opens the LRE driver. More...
 
int32_t LRE_supervisionInit (Lre_Handle lreHandle)
 Initializes the LRE supervision object. More...
 
void LRE_nodesTableInit (Lre_nodestableObj *ntObj)
 Initializes the nodestable. More...
 
void LRE_updateNodeEntry (NodesTable *table, const uint8_t *src_mac, uint16_t sequence_number, uint8_t port, Lre_NodeType node_type)
 Updates the node entry in the node table. More...
 
void LRE_checkNodeTimeouts (NodesTable *table)
 Checks the node timeouts. More...
 
void LRE_printNodesTable (Lre_Handle lreHandle)
 Prints the current state of the node table. More...
 
void LRE_supervisionDeinit (Lre_Handle lreHandle)
 Deinitializes the supervision module. More...
 
void LRE_statisticsInit (Lre_Handle lreHandle)
 Initializes the statistics object. More...
 
void LRE_getStatistics (Lre_Handle lreHandle)
 Updates the LRE statistics. More...
 

Function Documentation

◆ LRE_open()

void LRE_open ( Lre_Handle  lreHandle)

Opens the LRE driver.

This function is called to open the LRE driver.

Parameters
lreHandleLRE handle

◆ LRE_supervisionInit()

int32_t LRE_supervisionInit ( Lre_Handle  lreHandle)

Initializes the LRE supervision object.

This function initializes the LRE supervision object by setting the different fields with required values.

Parameters
lreHandleLRE handle
Returns
Status of the function call

◆ LRE_nodesTableInit()

void LRE_nodesTableInit ( Lre_nodestableObj ntObj)

Initializes the nodestable.

This function is called to initialize the nodestable.

Parameters
ntObjLRE nodestable object

◆ LRE_updateNodeEntry()

void LRE_updateNodeEntry ( NodesTable table,
const uint8_t *  src_mac,
uint16_t  sequence_number,
uint8_t  port,
Lre_NodeType  node_type 
)

Updates the node entry in the node table.

This function is called to update the node entry in the node table.

Parameters
tablePointer to the NodesTable.
src_macPointer to the source MAC address.
sequence_numberSequence number (host byte order).
portThe port on which SV frame was received
node_typeType of the remote node.

◆ LRE_checkNodeTimeouts()

void LRE_checkNodeTimeouts ( NodesTable table)

Checks the node timeouts.

This function is called to check the node timeouts.

Parameters
tablePointer to the NodesTable.

◆ LRE_printNodesTable()

void LRE_printNodesTable ( Lre_Handle  lreHandle)

Prints the current state of the node table.

This function is called to print the current state of the node table.

Parameters
lreHandleLRE handle

◆ LRE_supervisionDeinit()

void LRE_supervisionDeinit ( Lre_Handle  lreHandle)

Deinitializes the supervision module.

This function is called to deinitialize the supervision module.

Parameters
lreHandleLRE handle

◆ LRE_statisticsInit()

void LRE_statisticsInit ( Lre_Handle  lreHandle)

Initializes the statistics object.

This function is called to clear out the statistics.

Parameters
lreHandleLRE handle

◆ LRE_getStatistics()

void LRE_getStatistics ( Lre_Handle  lreHandle)

Updates the LRE statistics.

Parameters
lreHandleLRE handle