Request to handover control of a processor to another host if permitted.
Provides a means for the host with current control to relinquish a physical processor control to another host in the permitted list.
hdr | Generic TISCI message header. |* |
processor_id | Specifies a Processor ID. |
host_id | Specifies the new host to hand over control to. |
Data Fields | |
struct tisci_header | hdr |
uint8_t | processor_id |
uint8_t | host_id |
struct tisci_header tisci_msg_proc_handover_req::hdr |
uint8_t tisci_msg_proc_handover_req::processor_id |
uint8_t tisci_msg_proc_handover_req::host_id |