Request for retrieving the firewall permissions.
- Parameters
-
hdr | Generic TISCI message header. |
fwl_id | firewall ID in question. fwl_id is defined in the TRM. |
region | Region or channel number to set config info |
This field is unused in case of a simple firewall and must be initialized to zero. In case of a region based firewall, this field indicates the region in question (index starting from 0). In case of a channel based firewall, this field indicates the channel in question (index starting from 0).
- Parameters
-
n_permission_regs | Number of permission registers to retrieve |