AM243x MCU+ SDK  09.02.00

Detailed Description

Response to authentication resource release request.

Parameters
hdrGeneric TISCI message header. ACK response indicates that the secure threads are cleaned for pairing to System Firmware's DMA channels and the DMSC access to PKA registers is restored. A NACK response indicates that the resources could not be released to the requesting back to System Firmware.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_sa2ul_auth_res_release_resp::hdr