AM243x MCU+ SDK  09.02.00
cb_socket_lldcfg_update_t Struct Reference

Detailed Description

Structure representing the cb_socket_lldcfg_update instance.

Data Fields

const char * dev
 
uint16_t proto
 
uint16_t vlanid
 
uint32_t nTxPkts
 
uint32_t nRxPkts [MAX_NUM_RX_DMA_CH_PER_INSTANCE]
 
uint32_t pktSize
 
int dmaTxChId
 
int dmaRxChId [MAX_NUM_RX_DMA_CH_PER_INSTANCE]
 
int unusedDmaRx
 
int unusedDmaTx
 
int dmaRxShared
 
int dmaRxOwner
 
void(* rxDefaultDataCb )(void *data, int size, int port, void *cbArg)
 
void * rxDefaultCbArg
 
uint32_t numRxChannels
 

Field Documentation

◆ dev

const char* cb_socket_lldcfg_update_t::dev

Device name to match the expected socket.

◆ proto

uint16_t cb_socket_lldcfg_update_t::proto

Protocol or ethernet type in the ethernet frame header to match the expected socket.

◆ vlanid

uint16_t cb_socket_lldcfg_update_t::vlanid

VLAN ID to match the expected socket.

◆ nTxPkts

uint32_t cb_socket_lldcfg_update_t::nTxPkts

Number of buffers allocated for transmit packets Positive value will be updated to LLDEnetCfg_t.

◆ nRxPkts

uint32_t cb_socket_lldcfg_update_t::nRxPkts[MAX_NUM_RX_DMA_CH_PER_INSTANCE]

Number of buffers allocated for receive packets Positive value will be updated to LLDEnetCfg_t.

◆ pktSize

uint32_t cb_socket_lldcfg_update_t::pktSize

Transmit and receive maximum packet size. Positive value will be updated to LLDEnetCfg_t.

◆ dmaTxChId

int cb_socket_lldcfg_update_t::dmaTxChId

DMA transmit channel ID. 0 or positive value will be updated to LLDEnetCfg_t

◆ dmaRxChId

int cb_socket_lldcfg_update_t::dmaRxChId[MAX_NUM_RX_DMA_CH_PER_INSTANCE]

DMA receive channel ID. 0 or positive value will be updated to LLDEnetCfg_t

◆ unusedDmaRx

int cb_socket_lldcfg_update_t::unusedDmaRx

>0: won't use DMA RX; 0: will use DMA RX 0 or positive value will be updated to LLDEnetCfg_t

◆ unusedDmaTx

int cb_socket_lldcfg_update_t::unusedDmaTx

>0: won't use DMA TX; 0: will use DMA TX 0 or positive value will be updated to LLDEnetCfg_t

◆ dmaRxShared

int cb_socket_lldcfg_update_t::dmaRxShared

Only Sitara AM273x support this param. >0: the dmaRxChId is shared between apps; 0: not shared 0 or positive value will be updated to LLDEnetCfg_t

◆ dmaRxOwner

int cb_socket_lldcfg_update_t::dmaRxOwner

Only Sitara AM273x support this param. >0: the socket owns this RX DMA channel; 0: not own 0 or positive value will be updated to LLDEnetCfg_t

◆ rxDefaultDataCb

void(* cb_socket_lldcfg_update_t::rxDefaultDataCb) (void *data, int size, int port, void *cbArg)

Only Sitara AM273x support this param. Default RX data callback when there is no matching RX filter.

◆ rxDefaultCbArg

void* cb_socket_lldcfg_update_t::rxDefaultCbArg

Only Sitara AM273x support this param. Default RX data callback arg

◆ numRxChannels

uint32_t cb_socket_lldcfg_update_t::numRxChannels

Number of Rx DMA channels, only ICSSG peripheral has more than 1 Rx DMA channels.