hsrPrp_Config Structure storing the global variables
Data Fields | |
uint16_t | redSeqNr |
uint16_t | supSeqNr |
int * | collision_pkt_dropped |
int * | num_of_collision_occured |
ICSS_EMAC_Handle | icssEmacHandle |
uint32_t | redPruCheckTimerHostTableFlag |
uint32_t | redPruCheckTimerNodeTableClear |
ClockP_Object | redPruCheckTimer |
ClockP_Object | redLifeCheckTimer |
RED_FRAME * | redSupFrame |
TaskP_Object | redSupTask |
TaskP_Object | hsrPrpNodetableRefreshTask |
SemaphoreP_Object | redLifeCheckSemaphore |
SemaphoreP_Object | nodesTableSemaphore |
RED_INDEX_ARRAY_ENTRY * | indexArrayBase |
RED_BIN_ARRAY_ENTRY * | binArrayBase |
RED_NODE_TABLE_ENTRY * | nodeTableBase |
uint16_t hsrPrp_Config::redSeqNr |
uint16_t hsrPrp_Config::supSeqNr |
int* hsrPrp_Config::collision_pkt_dropped |
int* hsrPrp_Config::num_of_collision_occured |
ICSS_EMAC_Handle hsrPrp_Config::icssEmacHandle |
uint32_t hsrPrp_Config::redPruCheckTimerHostTableFlag |
uint32_t hsrPrp_Config::redPruCheckTimerNodeTableClear |
ClockP_Object hsrPrp_Config::redPruCheckTimer |
ClockP_Object hsrPrp_Config::redLifeCheckTimer |
RED_FRAME* hsrPrp_Config::redSupFrame |
TaskP_Object hsrPrp_Config::redSupTask |
TaskP_Object hsrPrp_Config::hsrPrpNodetableRefreshTask |
SemaphoreP_Object hsrPrp_Config::redLifeCheckSemaphore |
SemaphoreP_Object hsrPrp_Config::nodesTableSemaphore |
RED_INDEX_ARRAY_ENTRY* hsrPrp_Config::indexArrayBase |
RED_BIN_ARRAY_ENTRY* hsrPrp_Config::binArrayBase |
RED_NODE_TABLE_ENTRY* hsrPrp_Config::nodeTableBase |