#include <ecSlvApiInternal.h>
Data Structures | |
struct | EC_SLV_INT_GEN_MetaInfo |
Data Fields | |
struct EC_SLV_INT_General::EC_SLV_INT_GEN_MetaInfo | metaInfo |
uint16_t | eePDICtrl |
PDI control value. | |
uint16_t | eePDICfg |
PDI configuration value. | |
bool | eePDICtrlSet |
PDI control set by user. | |
bool | eePDICfgSet |
PDI configuration set by user. | |
EC_SLV_API_SSyncManDesc_t | bootStrapMbx [2] |
Bootstrap mailbox configuration. | |
bool | bootStrapMbxSet [2] |
Bootstrap mailbox configuration set by user. | |
EC_SLV_API_SSyncManDesc_t | standardMbx [2] |
Standard mailbox configuration. | |
bool | standardMbxSet [2] |
Standard mailbox configuration set by user. | |
EC_SLV_API_SSyncManDesc_t | syncManCfg [4] |
SyncManager configuration. | |
bool | syncManCfgSet [4] |
SyncManager configuration set by user. | |
uint16_t | stationAlias |
Station Alias value. | |
uint16_t | rsvd |
alignment | |
bool | fwInstallRequired |
Firmware update triggered. | |
uint32_t | maxPDOutputDataSize |
Output process data size. | |
uint32_t | maxPDInputDataSize |
Input process data size. | |