#include <ecSlvApiInternal.h>
Data Fields | |
EC_API_SLV_SCoE_ObjEntry_t * | pEntries |
Pointer to the SDO Entries. | |
uint16_t | entries |
Number of entries. | |
uint8_t | highestEntry |
Record types may not contain consecutive subIndexes, thus store highest subIdx Entry. | |
uint8_t | rsvd |
alignment | |
TOBJECT | sscLayerObject |
SSC SDO Object. | |
void * | cbReadCtxt |
Read callback context. | |
EC_API_SLV_CBObjRead_t | cbRead |
Read callback. | |
void * | cbWriteCtxt |
Write callback context. | |
EC_API_SLV_CBObjWrite_t | cbWrite |
Write callback. | |
struct EC_API_SLV_CoE_Object * | pNext |
Next Object. | |