AM243x MCU+ SDK  09.01.00
DDR_ECCErrorInfo Struct Reference

Detailed Description

Emif ECC Error Information structure.

This structure provides information about the ECC error

Data Fields

uintptr_t singlebitErrorAddress
 
uintptr_t doublebitErrorAddress
 
uint32_t singlebitErrorCount
 

Field Documentation

◆ singlebitErrorAddress

uintptr_t DDR_ECCErrorInfo::singlebitErrorAddress

One Bit ECC error address

◆ doublebitErrorAddress

uintptr_t DDR_ECCErrorInfo::doublebitErrorAddress

Two Bit ECC error address

◆ singlebitErrorCount

uint32_t DDR_ECCErrorInfo::singlebitErrorCount

One Bit ECC error count