Go to the source code of this file.
Data Structures | |
struct | Bootloader_CoreBootInfo |
Data structure containing information about a core specific to the AM64x SOC. More... | |
Macros | |
#define | BOOTLOADER_DEVICE_VARIANT_SINGLE_CORE (0x00000000U) |
#define | BOOTLOADER_DEVICE_VARIANT_DUAL_CORE (0x00040000U) |
#define | BOOTLOADER_DEVICE_VARIANT_QUAD_CORE (0x000C0000U) |
#define | BOOTLOADER_R5FSS0 (0x00000000U) |
#define | BOOTLOADER_R5FSS1 (0x00010000U) |
#define | BOOTLOADER_ICSS_CORE_DEFAULT_FREQUENCY (200000000U) |
Functions | |
int32_t | Bootloader_socCpuRequest (uint32_t cpuId) |
Request for a particular CPU in the AM64x SOC. More... | |
int32_t | Bootloader_socCpuRelease (uint32_t cpuId) |
Release a particular CPU in the AM64x SOC. More... | |
int32_t | Bootloader_socCpuSetClock (uint32_t cpuId, uint32_t cpuHz) |
Set the clock of a particular CPU in the AM64x SOC. More... | |
uint64_t | Bootloader_socCpuGetClock (uint32_t cpuId) |
Get the clock of a particular CPU in the AM64x SOC. More... | |
uint32_t | Bootloader_socCpuGetClkDefault (uint32_t cpuId) |
Get the default clock of a particular CPU in the AM64x SOC. More... | |
int32_t | Bootloader_socCpuPowerOnReset (uint32_t cpuId, void *socCoreOpMode) |
Do power-on-reset of a particular CPU in the AM64x SOC. More... | |
int32_t | Bootloader_socCpuResetRelease (uint32_t cpuId, uintptr_t entryPoint) |
Release a particular CPU in the AM64x SOC from reset. More... | |
int32_t | Bootloader_socCpuResetReleaseSelf (void) |
Release self CPU in the AM64x SOC from reset. More... | |
int32_t | Bootloader_socCpuSetEntryPoint (uint32_t cpuId, uintptr_t entryPoint) |
Set entry point for self CPU in the AM64x SOC from reset. More... | |
uint32_t | Bootloader_socTranslateSectionAddr (uint32_t cslCoreId, uint32_t addr) |
Translate a CPU address to the SOC address wherever applicable. More... | |
uint32_t | Bootloader_socRprcToCslCoreId (uint32_t rprcCoreId) |
Obtain the CSL core ID of a CPU from its RPRC core ID. More... | |
uint32_t * | Bootloader_socGetSelfCpuList (void) |
Get the list of self cpus in the SOC. More... | |
char * | Bootloader_socGetCoreName (uint32_t cpuId) |
Get the name of a core. More... | |
int32_t | Bootloader_socMemInitCpu (uint32_t cpuId) |
Initialize the core memories of a specific core. More... | |
uint32_t | Bootloader_socGetSciclientCpuProcId (uint32_t cpuId) |
Obtain the Sciclient Proc Id corresponding to the CSL core ID. More... | |
uint32_t | Bootloader_socGetSciclientCpuDevId (uint32_t cpuId) |
Obtain the Sciclient Device Id corresponding to the CSL core ID. More... | |
int32_t | Bootloader_socSecHandover (void) |
API to trigger the security handover from SYSFW. More... | |
int32_t | Bootloader_socWaitForFWBoot (void) |
API to wait for boot notification from SYSFW/ROM. More... | |
int32_t | Bootloader_socOpenFirewalls (void) |
API to open required firewalls using SYSFW. More... | |
int32_t | Bootloader_socAuthImage (uint32_t certLoadAddr) |
API to authenticate (and decrypt if needed) an appimage using SYSFW. More... | |
uint32_t | Bootloader_socIsAuthRequired (void) |
API to check if authentication is required for the device. Checks the SYS_STATUS register to see if device is GP, HS-FS, HS-SE etc. More... | |
uint32_t | Bootloader_socIsR5FSSDual (uint32_t ssNum) |
API to check if an R5 cluster/subsystem has dual cores enabled or not. More... | |
uint32_t | Bootloader_socGetCoreVariant (void) |
API to check the GPN variant of the SOC - whether it's a quad core, dual core or a single core variant. More... | |
void | Bootloader_socResetWorkaround (void) |
Workaround API to prevent CPSW register lockup. Checks the reset source and does a warm reset in case of POR MCU , POR MAIN or COLD BOOT reset. More... | |
void | Bootloader_enableMCUPLL (void) |
Enable MCU PLL. The MCU PLL will be initialized by DMSC if devgrp is set to DEVGRP_ALL. If devgrp is set to DEVGRP_00 (0x01) (Main Domain), the MCU PLL will not be initialized. This API initializes MCU PLL when devgrp is set to DEVGRP_00. More... | |
uint32_t | Bootloader_socIsMCUResetIsoEnabled (void) |
Check if MCU domain is reset isolated. More... | |
void | Bootloader_socNotifyFirewallOpen (void) |
Notify other cores firewall open from SBL. Function writes a Software defined magic word to PSRAM address (software defined) to signal Firewall open to MCU cores. This function should only be called from SBL. More... | |
int32_t | Bootloader_socEnableICSSCores (uint32_t clkFreq) |
API to enable ICSS cores when applicable. More... | |
void | Bootloader_socGetBootSeqOid (uint8_t *boot_seq_oid) |
API to get boot sequence oid. More... | |
#define BOOTLOADER_DEVICE_VARIANT_SINGLE_CORE (0x00000000U) |
#define BOOTLOADER_DEVICE_VARIANT_DUAL_CORE (0x00040000U) |
#define BOOTLOADER_DEVICE_VARIANT_QUAD_CORE (0x000C0000U) |
#define BOOTLOADER_R5FSS0 (0x00000000U) |
#define BOOTLOADER_R5FSS1 (0x00010000U) |
#define BOOTLOADER_ICSS_CORE_DEFAULT_FREQUENCY (200000000U) |
int32_t Bootloader_socCpuRequest | ( | uint32_t | cpuId | ) |
Request for a particular CPU in the AM64x SOC.
This API internally makes Sciclient calls to request control of the CPU
cpuId | [in] The CSL ID of the core |
int32_t Bootloader_socCpuRelease | ( | uint32_t | cpuId | ) |
Release a particular CPU in the AM64x SOC.
This API internally makes Sciclient calls to release control of the CPU
cpuId | [in] The CSL ID of the core |
int32_t Bootloader_socCpuSetClock | ( | uint32_t | cpuId, |
uint32_t | cpuHz | ||
) |
Set the clock of a particular CPU in the AM64x SOC.
This API internally makes Sciclient calls to set CPU clock
cpuId | [in] The CSL ID of the core |
cpuHz | [in] Desired clock frequency of the CPU in Hertz |
uint64_t Bootloader_socCpuGetClock | ( | uint32_t | cpuId | ) |
Get the clock of a particular CPU in the AM64x SOC.
This API internally makes Sciclient calls to get the current clock frequency of CPU
cpuId | [in] The CSL ID of the core |
uint32_t Bootloader_socCpuGetClkDefault | ( | uint32_t | cpuId | ) |
Get the default clock of a particular CPU in the AM64x SOC.
This API queries and internal lookup table to fetch the default clock speed at which a particular CPU should run.
cpuId | [in] The CSL ID of the core |
int32_t Bootloader_socCpuPowerOnReset | ( | uint32_t | cpuId, |
void * | socCoreOpMode | ||
) |
Do power-on-reset of a particular CPU in the AM64x SOC.
This API is called only when booting a non-self CPU.
cpuId | [in] The CSL ID of the core |
socCoreOpMode | Lockstep/Dual core mode as per setting in syscfg. |
int32_t Bootloader_socCpuResetRelease | ( | uint32_t | cpuId, |
uintptr_t | entryPoint | ||
) |
Release a particular CPU in the AM64x SOC from reset.
This API is called only when booting a non-self CPU. There is a different API Bootloader_socCpuResetReleaseSelf in the case of a self CPU
cpuId | [in] The CSL ID of the core |
entryPoint | [in] The entryPoint of the CPU, from where it should start execution |
int32_t Bootloader_socCpuResetReleaseSelf | ( | void | ) |
Release self CPU in the AM64x SOC from reset.
int32_t Bootloader_socCpuSetEntryPoint | ( | uint32_t | cpuId, |
uintptr_t | entryPoint | ||
) |
Set entry point for self CPU in the AM64x SOC from reset.
This API need not be called when booting a non-self CPU. The entry point can be specified in the Bootloader_socCpuResetRelease function itself
cpuId | [in] The CSL ID of the core |
entryPoint | [in] The entryPoint of the CPU, from where it should start execution |
uint32_t Bootloader_socTranslateSectionAddr | ( | uint32_t | cslCoreId, |
uint32_t | addr | ||
) |
Translate a CPU address to the SOC address wherever applicable.
This API need not be called when booting a non-self CPU. The entry point can be specified in the Bootloader_socCpuResetRelease function itself
cslCoreId | [in] The CSL ID of the core |
addr | [in] The CPU addr |
uint32_t Bootloader_socRprcToCslCoreId | ( | uint32_t | rprcCoreId | ) |
Obtain the CSL core ID of a CPU from its RPRC core ID.
rprcCoreId | [in] The RPRC ID of the core |
uint32_t* Bootloader_socGetSelfCpuList | ( | void | ) |
Get the list of self cpus in the SOC.
char* Bootloader_socGetCoreName | ( | uint32_t | cpuId | ) |
Get the name of a core.
cpuId | [in] The CSL ID of the core |
int32_t Bootloader_socMemInitCpu | ( | uint32_t | cpuId | ) |
Initialize the core memories of a specific core.
cpuId | [in] The CSL ID of the core |
uint32_t Bootloader_socGetSciclientCpuProcId | ( | uint32_t | cpuId | ) |
Obtain the Sciclient Proc Id corresponding to the CSL core ID.
cpuId | [in] The CSL ID of the core |
uint32_t Bootloader_socGetSciclientCpuDevId | ( | uint32_t | cpuId | ) |
Obtain the Sciclient Device Id corresponding to the CSL core ID.
cpuId | [in] The CSL ID of the core |
int32_t Bootloader_socSecHandover | ( | void | ) |
API to trigger the security handover from SYSFW.
int32_t Bootloader_socWaitForFWBoot | ( | void | ) |
API to wait for boot notification from SYSFW/ROM.
int32_t Bootloader_socOpenFirewalls | ( | void | ) |
API to open required firewalls using SYSFW.
int32_t Bootloader_socAuthImage | ( | uint32_t | certLoadAddr | ) |
API to authenticate (and decrypt if needed) an appimage using SYSFW.
certLoadAddr | [in] The SOC address pointing to the certificate+appimage |
uint32_t Bootloader_socIsAuthRequired | ( | void | ) |
API to check if authentication is required for the device. Checks the SYS_STATUS register to see if device is GP, HS-FS, HS-SE etc.
uint32_t Bootloader_socIsR5FSSDual | ( | uint32_t | ssNum | ) |
API to check if an R5 cluster/subsystem has dual cores enabled or not.
uint32_t Bootloader_socGetCoreVariant | ( | void | ) |
API to check the GPN variant of the SOC - whether it's a quad core, dual core or a single core variant.
void Bootloader_socResetWorkaround | ( | void | ) |
Workaround API to prevent CPSW register lockup. Checks the reset source and does a warm reset in case of POR MCU , POR MAIN or COLD BOOT reset.
void Bootloader_enableMCUPLL | ( | void | ) |
Enable MCU PLL. The MCU PLL will be initialized by DMSC if devgrp is set to DEVGRP_ALL. If devgrp is set to DEVGRP_00 (0x01) (Main Domain), the MCU PLL will not be initialized. This API initializes MCU PLL when devgrp is set to DEVGRP_00.
uint32_t Bootloader_socIsMCUResetIsoEnabled | ( | void | ) |
Check if MCU domain is reset isolated.
void Bootloader_socNotifyFirewallOpen | ( | void | ) |
Notify other cores firewall open from SBL. Function writes a Software defined magic word to PSRAM address (software defined) to signal Firewall open to MCU cores. This function should only be called from SBL.
int32_t Bootloader_socEnableICSSCores | ( | uint32_t | clkFreq | ) |
API to enable ICSS cores when applicable.
clkFreq | [in] Clock frequency of ICSS cores in Hz |
void Bootloader_socGetBootSeqOid | ( | uint8_t * | boot_seq_oid | ) |
API to get boot sequence oid.
boot_seq_oid | [in] pointer to integer array for populating boot sequence oid |