AM243x INDUSTRIAL COMMUNICATIONS SDK  09.01.00
dlrStateMachineVar Struct Reference

Detailed Description

State machine variables, part of DLR Object and L2 implementation.

Data Fields

uint8_t node_state
 
uint8_t ring_state
 
uint8_t topology
 
uint8_t status
 
uint8_t superStatus
 

Field Documentation

◆ node_state

uint8_t dlrStateMachineVar::node_state

device state. Internal

◆ ring_state

uint8_t dlrStateMachineVar::ring_state

ring state. Internal

◆ topology

uint8_t dlrStateMachineVar::topology

network topology. Attribute ID 1

◆ status

uint8_t dlrStateMachineVar::status

network status. Attribute ID 2

◆ superStatus

uint8_t dlrStateMachineVar::superStatus

supervisor status. Attribute ID 3