AM243x INDUSTRIAL COMMUNICATIONS SDK  09.01.00
hsrPrp_red_vlanTable.h File Reference

Introduction

Include file for hsrPrp_red_vlanTable.c.

Copyright (C) 2021 Texas Instruments Incorporated

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Go to the source code of this file.

Functions

RED_STATUS vlan_filter_config (PRUICSS_Handle pruicssHandle, uint8_t command)
 set the VLAN_FLTR_CTRL_SHIFT to enable/disable vlan filtering More...
 
RED_STATUS vlan_untagged_frames_config (PRUICSS_Handle pruicssHandle, uint8_t command)
 set the VLAN_FLTR_UNTAG_HOST_RCV_CTRL_SHIFT to enable/disable untagged frame host receive More...
 
RED_STATUS vlan_priotag_frames_config (PRUICSS_Handle pruicssHandle, uint8_t command)
 set the VLAN_FLTR_PRIOTAG_HOST_RCV_CTRL_SHIFT to enable/disable priority frame host receive More...
 
RED_STATUS vlan_sv_frames_config (PRUICSS_Handle pruicssHandle, uint8_t command)
 set the VLAN_FLTR_SV_CTRL_SHIFT for SV frames to skip/enter VLAN flow More...
 
RED_STATUS vlan_filter_update_vid (PRUICSS_Handle pruicssHandle, uint16_t vid, uint8_t command)
 insert/delete a VID in the VLAN filter table More...
 

Function Documentation

◆ vlan_filter_config()

RED_STATUS vlan_filter_config ( PRUICSS_Handle  pruicssHandle,
uint8_t  command 
)

set the VLAN_FLTR_CTRL_SHIFT to enable/disable vlan filtering

Parameters
pruicssHandleHandle to PRU ICSS instance. Contains pointers to base addresses & offsets
commandinstruction to enable/disable vlan filtering. Command can take 2 values: VLAN_FLTR_DIS 0x00 VLAN_FLTR_ENA 0x01
Returns
RED_OK on success, RED_ERR otherwise

◆ vlan_untagged_frames_config()

RED_STATUS vlan_untagged_frames_config ( PRUICSS_Handle  pruicssHandle,
uint8_t  command 
)

set the VLAN_FLTR_UNTAG_HOST_RCV_CTRL_SHIFT to enable/disable untagged frame host receive

Parameters
pruicssHandleHandle to PRU ICSS instance. Contains pointers to base addresses & offsets
commandinstruction to enable/disable untagged frame host receive. Command can take 2 values: VLAN_FLTR_UNTAG_HOST_RCV_ALL 0x00 VLAN_FLTR_UNTAG_HOST_RCV_NAL 0x01
Returns
RED_OK on success, RED_ERR otherwise

◆ vlan_priotag_frames_config()

RED_STATUS vlan_priotag_frames_config ( PRUICSS_Handle  pruicssHandle,
uint8_t  command 
)

set the VLAN_FLTR_PRIOTAG_HOST_RCV_CTRL_SHIFT to enable/disable priority frame host receive

Parameters
pruicssHandleHandle to PRU ICSS instance. Contains pointers to base addresses & offsets
commandinstruction to enable/disable priority frame host receive. Command can take 2 values: VLAN_FLTR_PRIOTAG_HOST_RCV_ALL 0x00 VLAN_FLTR_PRIOTAG_HOST_RCV_ALL 0x01
Returns
RED_OK on success, RED_ERR otherwise

◆ vlan_sv_frames_config()

RED_STATUS vlan_sv_frames_config ( PRUICSS_Handle  pruicssHandle,
uint8_t  command 
)

set the VLAN_FLTR_SV_CTRL_SHIFT for SV frames to skip/enter VLAN flow

Parameters
pruicssHandleHandle to PRU ICSS instance. Contains pointers to base addresses & offsets
commandinstruction to enable/disable priority frame host receive. Command can take 2 values: VLAN_FLTR_SV_VLAN_FLOW_SKIP 0x00 VLAN_FLTR_SV_VLAN_FLOW_TAKE 0x01
Returns
RED_OK on success, RED_ERR otherwise

◆ vlan_filter_update_vid()

RED_STATUS vlan_filter_update_vid ( PRUICSS_Handle  pruicssHandle,
uint16_t  vid,
uint8_t  command 
)

insert/delete a VID in the VLAN filter table

Parameters
pruicssHandleHandle to PRU ICSS instance. Contains pointers to base addresses & offsets
vidvid to be enabled/disabled in the VLAN filter table
commandinstruction to enable/disable VID host receive. Command can take 2 values: 0 : allow packet to host | ADD_VLAN_VID : set VID to 0x01 1 : do not allow packet to host | REM_VLAN_VID | set VID to 0x00
Returns
RED_OK on success, RED_ERR otherwise