AM243x MCU+ SDK  09.00.00

Detailed Description

CSL_UdmapTR10 specifies a Type 10 Transfer Request.

Data Fields

uint32_t flags
 
uint16_t icnt0
 
uint16_t icnt1
 
uint64_t addr
 
int32_t dim1
 
uint32_t rsvd [3]
 
uint32_t fmtflags
 
int32_t ddim1
 
uint64_t daddr
 

Field Documentation

◆ flags

uint32_t CSL_UdmapTR10::flags

Specifies type of TR and how the TR should be handled. It also supports the TR triggering and output events.

◆ icnt0

uint16_t CSL_UdmapTR10::icnt0

Total loop iteration count for level 0 (innermost)

◆ icnt1

uint16_t CSL_UdmapTR10::icnt1

Total loop iteration count for level 1

◆ addr

uint64_t CSL_UdmapTR10::addr

Starting address for the source data or destination data if it is a half duplex write

◆ dim1

int32_t CSL_UdmapTR10::dim1

Signed dimension for loop level 1 for the source data

◆ rsvd

uint32_t CSL_UdmapTR10::rsvd[3]

Reserved

◆ fmtflags

uint32_t CSL_UdmapTR10::fmtflags

Tells how the data is formatted either between the input and the output or if the data should use different addressing schemes or sizes

◆ ddim1

int32_t CSL_UdmapTR10::ddim1

Signed dimension for loop level 1 for the destination data

◆ daddr

uint64_t CSL_UdmapTR10::daddr

Starting address for the destination of the data