Files | |
file | cb_crc.h |
CRC implementation. | |
Functions | |
uint32_t | cb_crc32_calculate (uint8_t *bufptr, uint32_t bufsize) |
The function implement the CRC32 calculation based on the IEEE-802.3 CRC32 Ethernet Standard. More... | |
uint32_t cb_crc32_calculate | ( | uint8_t * | bufptr, |
uint32_t | bufsize | ||
) |
The function implement the CRC32 calculation based on the IEEE-802.3 CRC32 Ethernet Standard.
Polynomial: 04C11DB7h
Initial value: FFFFFFFFh
Input data reflected: Yes
Result data reflected: Yes
XOR value: FFFFFFFFh
bufptr | input data buffer |
bufsize | input data buffer size |