AM243x MCU+ SDK  09.00.00
USB NCM Example

Introduction

  • This examples demonstrates the use of TinyUSB NCM DEV Class driver. Its implements all the necessary callbacks that are required by TinyUSB NCM DEV class driver.
  • The Remote Network Driver Interface Specification (NCM) is a Microsoft proprietary protocol used mostly on top of USB. NCM_DOC

    NCM Example Block diagram
  • This example integrates LWIP HTTPD webserver running on r5fss0-0 core with TinyUSB NCM class dirver. The class driver's job is to collect the ethernet frames comming over USB and forward it to the Lwip web server and vice versa.
Note
In this example we receive one ethernet packet at a time from NCM class driver and forward it to Lwip webeserver. This is a simplified design to demonstrate the use of NCM net class driver thus to achive better throughput, further optimizations are required.
  • This example also implements a DHCP server which will provide a static ip address to HTTPD web server.Moreover it allocates ip address to the NCM Host PC as well.
  • Refer Enet LwIP HTTP Server On Bare Metal (No-RTOS) to know more about http web server using lwip( TCP/IP) stack.
  • Once NCM device enumearation is successful, AM243x-EVM will be recognised as a separate network interface. The Network interface driver on the Host side will convert and transfer the ethernet traffic Via USB bus as per NCM protocol specification.
  • To enable USB Logging for this example refer USB CDC Echo Example

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_nortos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/usb/device/ncm

Steps to Run the Example

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

HW Setup

AM243X-EVM

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J24 on AM64x/AM243x EVM to the USB host

USB 2.0 Host/Device Connector

AM243X-LP

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J10 on AM243x LP to the USB host
  • USB2.0 is validated from Type C connector
Note
The am243x-LP board is powered by the same J10 connector. It requires USB-type C port that has power delivery classification.
  • Thunderbolt
  • Battery behind USB logo. refer am243x-LP User Guide

USB Type-C Host/Device Connector

Run the example

  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • When application is running observe that ncm network device is detected by HOST PC ( Windows/linux)
  • If the enumeration is successful the following should be displayed on console.

Windows

  • Open command prompt and execute ipconfig. User should see a new network interface detected.

NCM Device Enumeration log
Note
  • NCM Windows driver might be readily available. Follow link to download and install the NCM host class driver for windows.

Linux

  • Open terminal and execute dmesg command. User should see a new network interface over USB detected.

NCM Device Enumeration log.

NCM Download

Note
  • Note that this IP address to host PC and device running lwip webserver will be provided by the dhcp server running along with lwip httpd. Refer Introduction

When the http get request will be successful, following HTML page will be display.

HTTP Get request via USB( NCM ) successful

See Also

USB