AM243x INDUSTRIAL COMMUNICATIONS SDK  09.00.00
icss_eip_driver.h File Reference

Go to the source code of this file.

Data Structures

struct  clockClass_t
 Specifies the properties of a clock. More...
 
struct  descr_t
 Description in unicode. More...
 
struct  portProfileIdentity_t
 Specifies the PTP profile of each port of the device. More...
 
struct  portPhysAddr_t
 Specifies the physical protocol and physical address (e.g. IEEE 802.3) of each port of the device (e.g. MAC address). The maximum number of characters is 16. Unused array elements are zero-filled. More...
 
struct  portProtAddr_t
 Specifies the specifies the network and protocol address of each port of the device (e.g. IP address). The Network Protocol specifies the protocol for the network. More...
 
struct  sysTimeOffset_t
 Specifies the system time in microseconds and the Offset to the local clock value. More...
 
struct  cipSyncConfig_t
 CIP Sync configuration. Instance Attribute for PTP Class (Class Code 0x43. CIP Spec Vol 1) More...
 
struct  eip_Config
 

Macros

#define IEP_CMP_DEFAULT_VAL   0x11
 
#define IEP_CMP4_DEFAULT_VAL   0x5000
 
#define IEP_CMP0_DEFAULT_VAL   0xffffffff
 
#define PRU_IEP_CMP_CFG_REG   0x40
 
#define PRU_IEP_CMP0_REG   0x48
 
#define EIP_TICK_PERIOD   1 /*in milliseconds*/
 
#define LOOPBK_PKT_SEND_PERIOD   1000
 
#define DEFAULT_BC_PKT_SIZE   60
 
#define ONE_SECOND_INTERVAL   1000 /*in milliseconds*/
 
#define TWO_MINUTE_INTERVAL   120000 /*in milliseconds*/
 
#define CRS_STATUS_MASK   0x2
 
#define CRS_STATUS_SHIFT   0x1
 
#define PTP_PROT_TYPE   0x88F7
 
#define DLR_MDIO_PHY0   1
 
#define DLR_MDIO_PHY1   2
 
#define PHYBMSR_OFFSET   0x1
 
#define PHYSTS_OFFSET   0x10
 
#define PHY_LINK_STATUS_MASK   0x4
 
#define PHY_LINK_STATUS_SHIFT   0x2
 

Typedefs

typedef struct eip_Config_s * EIP_Handle
 

Enumerations

enum  clockType { ORDINARY_CLOCK = 0, TRANSPARENT_CLOCK = 1, BOUNDARY_CLOCK = 2 }
 Type of clock supported by PTP Implementation. This is not specified by standard. More...
 

Functions

void EIP_drvInit (EIP_Handle icssEipHandle)
 Initialization routine for Ethernet/IP driver functions. More...
 
void EIP_drvStop (EIP_Handle icssEipHandle)
 EIP driver stop API. More...
 
void EIP_drvStart (EIP_Handle icssEipHandle)
 EIP driver start API. More...
 
void EIP_processProtocolFrames (uint32_t *queue_number, void *userArg)
 API to process the real time Packets. More...
 
int8_t EIP_initializeCIPSync (EIP_Handle icssEipHandle)
 API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based on PTP implementation. More...