AM243x INDUSTRIAL COMMUNICATIONS SDK  09.00.00
PN_HandleDef.h File Reference

Go to the source code of this file.

Data Structures

struct  PN_PtcpDebug
 
struct  PN_PtcpTimerAttrs
 
struct  PN_PtcpConfig
 
struct  PN_IsoMConfig
 
struct  PN_Config
 

Macros

#define PN_TASK_STACK_SIZE   (2048)
 

Typedefs

typedef void(* PN_getMACAddress) (uint8_t index, uint8_t *lclMac)
 

Macro Definition Documentation

◆ PN_TASK_STACK_SIZE

#define PN_TASK_STACK_SIZE   (2048)

Typedef Documentation

◆ PN_getMACAddress

typedef void(* PN_getMACAddress) (uint8_t index, uint8_t *lclMac)