Go to the source code of this file.
Functions | |
float | ti_tmu_sin_pu (float anglePU) |
Computes the trigonometric sine value of the input angle using TMU. More... | |
float | ti_tmu_cos_pu (float anglePU) |
Computes the trigonometric cosine value of the input angle using TMU. More... | |
float | ti_tmu_atan_pu (float x) |
Computes the trigonometric atan value of the input using TMU. More... | |
float | ti_tmu_log_pu (float x) |
Computes the logarithmic value of the input using TMU. More... | |
float | ti_tmu_iexp_pu (float x) |
Computes the inverse exponential value of the input using TMU. More... | |
float | ti_tmu_sin (float angleRad) |
Computes the trigonometric sine value of the input angle using TMU. More... | |
float | ti_tmu_cos (float angleRad) |
Computes the trigonometric cosine value of the input angle using TMU. More... | |
float | ti_tmu_atan (float x) |
Computes the trigonometric atan value of the input angle using TMU. More... | |
float | ti_tmu_atan2 (float x, float y) |
Computes the trigonometric atan2 value of the input values using TMU. Uses the quadratic built in TMU function to comput the ratio and quadrant value, which is then used to comput atan2 value of input. More... | |