AM263x MCU+ SDK  09.01.00
EnetTimeSync_setTimestamp Struct Reference

Detailed Description

Timestamp set.

Data Fields

uint64_t tsLoadVal
 
uint8_t clkMode
 
uint8_t clkSign
 

Field Documentation

◆ tsLoadVal

uint64_t EnetTimeSync_setTimestamp::tsLoadVal

timestamp value in nano seconds unit to set

◆ clkMode

uint8_t EnetTimeSync_setTimestamp::clkMode

mode of the clock. Applicable only to ICSSG peripheral. Says whether given value tsLoadVal is absolute or related. 0: absolute, 1: relative

◆ clkSign

uint8_t EnetTimeSync_setTimestamp::clkSign