AM263x MCU+ SDK  09.01.00

Detailed Description

Input args for CPSW_ALE_IOCTL_SET_POLICER command.

Data Fields

uint32_t ouiAleEntryIdx
 
uint32_t srcMacAleEntryIdx
 
uint32_t dstMacAleEntryIdx
 
uint32_t ivlanAleEntryIdx
 
uint32_t ovlanAleEntryIdx
 
uint32_t etherTypeAleEntryIdx
 
uint32_t srcIpAleEntryIdx
 
uint32_t dstIpAleEntryIdx
 
uint32_t policerEntryIdx
 

Field Documentation

◆ ouiAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::ouiAleEntryIdx

OUI ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OUI in policerMatchEnMask is set

◆ srcMacAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::srcMacAleEntryIdx

MAC address ALE table entry index to match source MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACSRC in policerMatchEnMask is set

◆ dstMacAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::dstMacAleEntryIdx

MAC address ALE table entry index to match destination MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACDST in policerMatchEnMask is set

◆ ivlanAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::ivlanAleEntryIdx

Inner VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_IVLAN in policerMatchEnMask is set

◆ ovlanAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::ovlanAleEntryIdx

Outer VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OVLAN in policerMatchEnMask is set

◆ etherTypeAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::etherTypeAleEntryIdx

EtherType ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_ETHERTYPE in policerMatchEnMask is set

◆ srcIpAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::srcIpAleEntryIdx

IP address ALE table entry index to match as source IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPSRC in policerMatchEnMask is set

◆ dstIpAleEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::dstIpAleEntryIdx

IP address ALE table entry index to match as destination IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPDST in policerMatchEnMask is set

◆ policerEntryIdx

uint32_t CpswAle_SetPolicerEntryOutArgs::policerEntryIdx

ALE policer table entry index