Data structure containing information about a core specific to the SOC.
This structure is used to store the data about cores in the SoC in the form of a lookup table which will be used by various APIs.
Data Fields | |
uint32_t | defaultClockHz |
char | coreName [8] |
uint32_t Bootloader_CoreBootInfo::defaultClockHz |
char Bootloader_CoreBootInfo::coreName[8] |