AM263x MCU+ SDK  09.01.00
sdl_ecc_utils.h File Reference

Go to the source code of this file.

Functions

void SDL_ECC_UTILS_enableECCATCM (void)
 
void SDL_ECC_UTILS_enableECCB0TCM (void)
 
void SDL_ECC_UTILS_enableECCB1TCM (void)
 
void SDL_ECC_UTILS_configSecIntr (uint32_t eventCountInitValue, uint32_t eventTypeBitMap, uint32_t counterNumber)
 

Function Documentation

◆ SDL_ECC_UTILS_enableECCATCM()

void SDL_ECC_UTILS_enableECCATCM ( void  )

◆ SDL_ECC_UTILS_enableECCB0TCM()

void SDL_ECC_UTILS_enableECCB0TCM ( void  )

◆ SDL_ECC_UTILS_enableECCB1TCM()

void SDL_ECC_UTILS_enableECCB1TCM ( void  )

◆ SDL_ECC_UTILS_configSecIntr()

void SDL_ECC_UTILS_configSecIntr ( uint32_t  eventCountInitValue,
uint32_t  eventTypeBitMap,
uint32_t  counterNumber 
)