AM263x MCU+ SDK  09.01.00
Thread functions binding

Introduction

Files

file  cb_thread.h
 Bindings to POSIX thread, mutex and semaphore functions.
 

Data Structures

struct  cb_tsn_thread_attr_t
 parameters to initialize thread More...
 
struct  cb_waitpoint_t
 Wait points that blocks the execution of a thread at a specific code point until an event occurs. More...
 

Functions

static int cb_tsn_thread_attr_init (cb_tsn_thread_attr_t *attr, int pri, int stack_size, const char *name)
 
static int cb_tsn_thread_attr_set_stackaddr (cb_tsn_thread_attr_t *attr, void *stack_addr)
 
static void cb_waitpoint_init (cb_waitpoint_t *wp)
 Wait point initialization. More...
 
static void cb_waitpoint_deinit (cb_waitpoint_t *wp)
 Wait point de-initialization. More...
 
static bool cb_waitpoint_check (cb_waitpoint_t *wp, uint64_t time)
 Wait point check. More...
 
static void cb_waitpoint_wakeup_at (cb_waitpoint_t *wp, uint64_t time, bool dosleep)
 Wait point blocks until wake point has been awoken and after specified time. More...
 

Macros

#define CB_TSN_THREAD_NAME_SIZE   128
 data structure for thread attributes More...
 
#define CB_THREAD_T   pthread_t
 
#define CB_THREAD_CREATE(th, attr, func, arg)   pthread_create(th, NULL, func, arg)
 
#define CB_THREAD_JOIN   pthread_join
 
#define CB_THREAD_EXIT   pthread_exit
 
#define CB_THREAD_MUTEX_T   pthread_mutex_t
 
#define CB_THREAD_MUTEX_LOCK   pthread_mutex_lock
 
#define CB_THREAD_MUTEX_TRYLOCK   pthread_mutex_trylock
 
#define CB_THREAD_MUTEX_TIMEDLOCK   pthread_mutex_timedlock
 
#define CB_THREAD_MUTEX_UNLOCK   pthread_mutex_unlock
 
#define CB_THREAD_MUTEX_INIT   pthread_mutex_init
 
#define CB_THREAD_MUTEX_DESTROY   pthread_mutex_destroy
 
#define CB_THREAD_MUTEXATTR_T   pthread_mutexattr_t
 
#define CB_THREAD_MUTEXATTR_INIT   pthread_mutexattr_init
 
#define CB_THREAD_MUTEXATTR_SETPSHARED   pthread_mutexattr_setpshared
 
#define CB_THREAD_PROCESS_SHARED   PTHREAD_PROCESS_SHARED
 
#define CB_THREAD_PROCESS_PRIVATE   PTHREAD_PROCESS_PRIVATE
 
#define CB_THREAD_COND_T   pthread_cond_t
 
#define CB_THREAD_COND_INIT   pthread_cond_init
 
#define CB_THREAD_COND_DESTROY   pthread_cond_destroy
 
#define CB_THREAD_COND_WAIT   pthread_cond_wait
 
#define CB_THREAD_COND_SIGNAL   pthread_cond_signal
 
#define CB_THREAD_COND_BROADCAST   pthread_cond_broadcast
 
#define CB_SEM_T   sem_t
 
#define CB_SEM_INIT   sem_init
 
#define CB_SEM_GETVALUE   sem_getvalue
 
#define CB_SEM_WAIT   sem_wait
 
#define CB_SEM_TRYWAIT   sem_trywait
 
#define CB_SEM_TIMEDWAIT   sem_timedwait
 
#define CB_SEM_POST   sem_post
 
#define CB_SEM_DESTROY   sem_destroy
 
#define CB_SEM_OPEN   sem_open
 
#define CB_SEM_CLOSE   sem_close
 
#define CB_SEM_UNLINK   sem_unlink
 
#define CB_SEM_FAILED   SEM_FAILED
 
#define cb_waitpoint_wakeup(wp)   CB_THREAD_COND_SIGNAL(&(wp)->condition)
 Wait point wakeup to signal any one thread currently at this wait point. More...
 
#define cb_waitpoint_broadcast(wp)   CB_THREAD_COND_BROADCAST(&(wp)->condition)
 Wait point wakeup to signal all threads currently at this wait point. More...
 
#define cb_waitpoint_lock(wp)   CB_THREAD_MUTEX_LOCK(&(wp)->lock)
 Wait point lock. More...
 
#define cb_waitpoint_unlock(wp)   CB_THREAD_MUTEX_UNLOCK(&(wp)->lock)
 Wait point unlock. More...
 

Macro Definition Documentation

◆ CB_TSN_THREAD_NAME_SIZE

#define CB_TSN_THREAD_NAME_SIZE   128

data structure for thread attributes

◆ CB_THREAD_T

#define CB_THREAD_T   pthread_t

◆ CB_THREAD_CREATE

#define CB_THREAD_CREATE (   th,
  attr,
  func,
  arg 
)    pthread_create(th, NULL, func, arg)

◆ CB_THREAD_JOIN

#define CB_THREAD_JOIN   pthread_join

◆ CB_THREAD_EXIT

#define CB_THREAD_EXIT   pthread_exit

◆ CB_THREAD_MUTEX_T

#define CB_THREAD_MUTEX_T   pthread_mutex_t

◆ CB_THREAD_MUTEX_LOCK

#define CB_THREAD_MUTEX_LOCK   pthread_mutex_lock

◆ CB_THREAD_MUTEX_TRYLOCK

#define CB_THREAD_MUTEX_TRYLOCK   pthread_mutex_trylock

◆ CB_THREAD_MUTEX_TIMEDLOCK

#define CB_THREAD_MUTEX_TIMEDLOCK   pthread_mutex_timedlock

◆ CB_THREAD_MUTEX_UNLOCK

#define CB_THREAD_MUTEX_UNLOCK   pthread_mutex_unlock

◆ CB_THREAD_MUTEX_INIT

#define CB_THREAD_MUTEX_INIT   pthread_mutex_init

◆ CB_THREAD_MUTEX_DESTROY

#define CB_THREAD_MUTEX_DESTROY   pthread_mutex_destroy

◆ CB_THREAD_MUTEXATTR_T

#define CB_THREAD_MUTEXATTR_T   pthread_mutexattr_t

◆ CB_THREAD_MUTEXATTR_INIT

#define CB_THREAD_MUTEXATTR_INIT   pthread_mutexattr_init

◆ CB_THREAD_MUTEXATTR_SETPSHARED

#define CB_THREAD_MUTEXATTR_SETPSHARED   pthread_mutexattr_setpshared

◆ CB_THREAD_PROCESS_SHARED

#define CB_THREAD_PROCESS_SHARED   PTHREAD_PROCESS_SHARED

◆ CB_THREAD_PROCESS_PRIVATE

#define CB_THREAD_PROCESS_PRIVATE   PTHREAD_PROCESS_PRIVATE

◆ CB_THREAD_COND_T

#define CB_THREAD_COND_T   pthread_cond_t

◆ CB_THREAD_COND_INIT

#define CB_THREAD_COND_INIT   pthread_cond_init

◆ CB_THREAD_COND_DESTROY

#define CB_THREAD_COND_DESTROY   pthread_cond_destroy

◆ CB_THREAD_COND_WAIT

#define CB_THREAD_COND_WAIT   pthread_cond_wait

◆ CB_THREAD_COND_SIGNAL

#define CB_THREAD_COND_SIGNAL   pthread_cond_signal

◆ CB_THREAD_COND_BROADCAST

#define CB_THREAD_COND_BROADCAST   pthread_cond_broadcast

◆ CB_SEM_T

#define CB_SEM_T   sem_t

◆ CB_SEM_INIT

#define CB_SEM_INIT   sem_init

◆ CB_SEM_GETVALUE

#define CB_SEM_GETVALUE   sem_getvalue

◆ CB_SEM_WAIT

#define CB_SEM_WAIT   sem_wait

◆ CB_SEM_TRYWAIT

#define CB_SEM_TRYWAIT   sem_trywait

◆ CB_SEM_TIMEDWAIT

#define CB_SEM_TIMEDWAIT   sem_timedwait

◆ CB_SEM_POST

#define CB_SEM_POST   sem_post

◆ CB_SEM_DESTROY

#define CB_SEM_DESTROY   sem_destroy

◆ CB_SEM_OPEN

#define CB_SEM_OPEN   sem_open

◆ CB_SEM_CLOSE

#define CB_SEM_CLOSE   sem_close

◆ CB_SEM_UNLINK

#define CB_SEM_UNLINK   sem_unlink

◆ CB_SEM_FAILED

#define CB_SEM_FAILED   SEM_FAILED

◆ cb_waitpoint_wakeup

#define cb_waitpoint_wakeup (   wp)    CB_THREAD_COND_SIGNAL(&(wp)->condition)

Wait point wakeup to signal any one thread currently at this wait point.

Parameters
wpobject reference to a waitpoint

This interface should be called within and cb_waitpoint_lock/cb_waitpoint_unlock.

◆ cb_waitpoint_broadcast

#define cb_waitpoint_broadcast (   wp)    CB_THREAD_COND_BROADCAST(&(wp)->condition)

Wait point wakeup to signal all threads currently at this wait point.

Parameters
wpobject reference to a waitpoint

This interface should be called within and cb_waitpoint_lock/cb_waitpoint_unlock.

◆ cb_waitpoint_lock

#define cb_waitpoint_lock (   wp)    CB_THREAD_MUTEX_LOCK(&(wp)->lock)

Wait point lock.

Parameters
wpobject reference to a waitpoint

◆ cb_waitpoint_unlock

#define cb_waitpoint_unlock (   wp)    CB_THREAD_MUTEX_UNLOCK(&(wp)->lock)

Wait point unlock.

Parameters
wpobject reference to a waitpoint

Function Documentation

◆ cb_tsn_thread_attr_init()

static int cb_tsn_thread_attr_init ( cb_tsn_thread_attr_t attr,
int  pri,
int  stack_size,
const char *  name 
)
inlinestatic

◆ cb_tsn_thread_attr_set_stackaddr()

static int cb_tsn_thread_attr_set_stackaddr ( cb_tsn_thread_attr_t attr,
void *  stack_addr 
)
inlinestatic

◆ cb_waitpoint_init()

static void cb_waitpoint_init ( cb_waitpoint_t wp)
inlinestatic

Wait point initialization.

Parameters
wpobject reference to a waitpoint

◆ cb_waitpoint_deinit()

static void cb_waitpoint_deinit ( cb_waitpoint_t wp)
inlinestatic

Wait point de-initialization.

Parameters
wpobject reference to a waitpoint

◆ cb_waitpoint_check()

static bool cb_waitpoint_check ( cb_waitpoint_t wp,
uint64_t  time 
)
inlinestatic

Wait point check.

Parameters
wpobject reference to a waitpoint
timereference time, usually the current time
Returns
true if wait time has elapsed and not yet awoke, otherwise false

◆ cb_waitpoint_wakeup_at()

static void cb_waitpoint_wakeup_at ( cb_waitpoint_t wp,
uint64_t  time,
bool  dosleep 
)
inlinestatic

Wait point blocks until wake point has been awoken and after specified time.

Parameters
wpobject reference to a waitpoint
timereference time, usually the current time
dosleepwhether to wait on waitpoint condition or not

This interface should be called within and cb_waitpoint_lock, which is then automatically unlocked before entering blocking state and then automatically locked again when exiting the blocked state.