AM263x MCU+ SDK  09.01.00
Doubly Linked List

Introduction

Files

file  ub_llist.h
 Doubly linked list.
 

Data Structures

struct  ub_list_node
 ub_list node structure More...
 
struct  ub_list
 Link ub_list structure. More...
 

Functions

void ub_list_init (struct ub_list *ub_list)
 Initialize ub_list. More...
 
void ub_list_clear (struct ub_list *ub_list, ub_list_node_clear_h node_clear, void *arg)
 Clear the ub_list without freeing any nodes. More...
 
void ub_list_append (struct ub_list *ub_list, struct ub_list_node *node)
 Append a node at the end of the ub_list. More...
 
void ub_list_prepend (struct ub_list *ub_list, struct ub_list_node *node)
 Append a node at the start of the ub_list. More...
 
void ub_list_insert_before (struct ub_list *ub_list, struct ub_list_node *refnode, struct ub_list_node *node)
 Append a node before a reference node. More...
 
void ub_list_insert_after (struct ub_list *ub_list, struct ub_list_node *refnode, struct ub_list_node *node)
 Append a node after a reference node. More...
 
void ub_list_unlink (struct ub_list *ub_list, struct ub_list_node *node)
 Remove a node from the ub_list. More...
 
void ub_list_sort (struct ub_list *ub_list, ub_list_sort_h *sh, void *arg)
 Sort entries in the ub_list based on comparator. More...
 
struct ub_list_nodeub_list_apply (const struct ub_list *ub_list, bool fwd, ub_list_apply_h *ah, void *arg)
 Apply function to nodes in the ub_list. More...
 
struct ub_list_nodeub_list_head (const struct ub_list *ub_list)
 Get first entry of the ub_list. More...
 
struct ub_list_nodeub_list_tail (const struct ub_list *ub_list)
 Get last entry of the ub_list. More...
 
uint32_t ub_list_count (const struct ub_list *ub_list)
 Get number of entries. More...
 
static void * ub_list_nodedata (const struct ub_list_node *node)
 Get data of node. More...
 
static bool ub_list_isempty (const struct ub_list *ub_list)
 Check if ub_list is empty. More...
 

Typedefs

typedef void() ub_list_node_clear_h(struct ub_list_node *node, void *arg)
 function to clean up node More...
 
typedef bool() ub_list_sort_h(struct ub_list_node *node1, struct ub_list_node *node2, void *arg)
 Comparator function handler for nodes. More...
 
typedef bool() ub_list_apply_h(struct ub_list_node *node, void *arg)
 Apply function handler for nodes. More...
 

Macros

#define UB_LIST_NODE_INIT   {NULL, NULL, NULL}
 Initialize members of ub_list node. More...
 
#define UB_LIST_INIT   {NULL, NULL, 0}
 Initialize ub_list. More...
 
#define UB_LIST_FOREACH_ITER(ub_list, node)    (node) = ub_list_head((ub_list)); (node); (node) = (node)->next
 Traverse the ub_list. More...
 

Macro Definition Documentation

◆ UB_LIST_NODE_INIT

#define UB_LIST_NODE_INIT   {NULL, NULL, NULL}

Initialize members of ub_list node.

◆ UB_LIST_INIT

#define UB_LIST_INIT   {NULL, NULL, 0}

Initialize ub_list.

◆ UB_LIST_FOREACH_ITER

#define UB_LIST_FOREACH_ITER (   ub_list,
  node 
)     (node) = ub_list_head((ub_list)); (node); (node) = (node)->next

Traverse the ub_list.

Typedef Documentation

◆ ub_list_node_clear_h

typedef void() ub_list_node_clear_h(struct ub_list_node *node, void *arg)

function to clean up node

Parameters
nodenode to be applied
argclean up argument

◆ ub_list_sort_h

typedef bool() ub_list_sort_h(struct ub_list_node *node1, struct ub_list_node *node2, void *arg)

Comparator function handler for nodes.

Parameters
node1first node
node2second node
argComparison argument
Note
the result must end up with all true, otherwise it goes to infinite loop

◆ ub_list_apply_h

typedef bool() ub_list_apply_h(struct ub_list_node *node, void *arg)

Apply function handler for nodes.

Parameters
nodenode to be applied
argApply argument

Function Documentation

◆ ub_list_init()

void ub_list_init ( struct ub_list ub_list)

Initialize ub_list.

Parameters
ub_listpointer to link ub_list structure

◆ ub_list_clear()

void ub_list_clear ( struct ub_list ub_list,
ub_list_node_clear_h  node_clear,
void *  arg 
)

Clear the ub_list without freeing any nodes.

Parameters
ub_listpointer to link ub_list structure
node_clearclean up callback fuction
argclean up argument

◆ ub_list_append()

void ub_list_append ( struct ub_list ub_list,
struct ub_list_node node 
)

Append a node at the end of the ub_list.

Parameters
ub_listPointer to link ub_list structure
nodeentry to be appended

◆ ub_list_prepend()

void ub_list_prepend ( struct ub_list ub_list,
struct ub_list_node node 
)

Append a node at the start of the ub_list.

Parameters
ub_listPointer to link ub_list structure
nodeentry to be appended

◆ ub_list_insert_before()

void ub_list_insert_before ( struct ub_list ub_list,
struct ub_list_node refnode,
struct ub_list_node node 
)

Append a node before a reference node.

Parameters
ub_listPointer to link ub_list structure
refnodeReference node
nodeentry to be inserted

◆ ub_list_insert_after()

void ub_list_insert_after ( struct ub_list ub_list,
struct ub_list_node refnode,
struct ub_list_node node 
)

Append a node after a reference node.

Parameters
ub_listPointer to link ub_list structure
refnodeReference node
nodeentry to be appended

◆ ub_list_unlink()

void ub_list_unlink ( struct ub_list ub_list,
struct ub_list_node node 
)

Remove a node from the ub_list.

Parameters
ub_listPointer to link ub_list structure
nodeentry to be removed

◆ ub_list_sort()

void ub_list_sort ( struct ub_list ub_list,
ub_list_sort_h sh,
void *  arg 
)

Sort entries in the ub_list based on comparator.

Parameters
ub_listPointer to link ub_list structure
shSort comparator handler
argSort argument

◆ ub_list_apply()

struct ub_list_node* ub_list_apply ( const struct ub_list ub_list,
bool  fwd,
ub_list_apply_h ah,
void *  arg 
)

Apply function to nodes in the ub_list.

Parameters
ub_listPointer to link ub_list structure
fwdForward or reverse movement
ahApply function handler
argApply argument

◆ ub_list_head()

struct ub_list_node* ub_list_head ( const struct ub_list ub_list)

Get first entry of the ub_list.

Parameters
ub_listPointer to link ub_list structure

◆ ub_list_tail()

struct ub_list_node* ub_list_tail ( const struct ub_list ub_list)

Get last entry of the ub_list.

Parameters
ub_listPointer to link ub_list structure

◆ ub_list_count()

uint32_t ub_list_count ( const struct ub_list ub_list)

Get number of entries.

Parameters
ub_listPointer to link ub_list structure
Returns
number of entries

◆ ub_list_nodedata()

static void* ub_list_nodedata ( const struct ub_list_node node)
inlinestatic

Get data of node.

Parameters
nodeNode entry
Returns
pointer to data

◆ ub_list_isempty()

static bool ub_list_isempty ( const struct ub_list ub_list)
inlinestatic

Check if ub_list is empty.

Parameters
ub_listPointer to link ub_list structure
Returns
true if node exist, otherwise false