Top level header that contains all Digital Controller Library functions.
Go to the source code of this file.
Data Structures | |
struct | POWER_MEAS_SINE_ANALYZER |
Defines the POWER_MEAS_SINE_ANALYZER structure. More... | |
Macros | |
#define | IEEE754_TYPES |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
Functions | |
static void | POWER_MEAS_SINE_ANALYZER_reset (POWER_MEAS_SINE_ANALYZER *v) |
Resets internal data to zero. More... | |
static void | POWER_MEAS_SINE_ANALYZER_config (POWER_MEAS_SINE_ANALYZER *v, float32_t isrFrequency, float32_t threshold, float32_t gridMaxFreq, float32_t gridMinFreq) |
Configures the power measurment module. More... | |
static void | POWER_MEAS_SINE_ANALYZER_run (POWER_MEAS_SINE_ANALYZER *v) |
Perform calculations using the POWER_MEAS_SINE_ANALYZER module. More... | |