Go to the source code of this file.
Data Structures | |
struct | EMAVG |
Defines the Exponential Moving Average (EMAVG) structure. More... | |
Macros | |
#define | IEEE754_TYPES |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
Functions | |
static void | EMAVG_reset (EMAVG *v) |
resets internal storage data More... | |
static void | EMAVG_config (EMAVG *v, float32_t multiplier) |
configures EMAVG module More... | |
static void | EMAVG_run (EMAVG *v, float in) |
Run EMAVG module. More... | |