Contains PI2 (double integrator) controller with its related structures and functions.
Go to the source code of this file.
Data Structures | |
struct | DCL_PI2_SPS |
Defines DCL_PI2 shadow parameter set used for updating controller parameter. More... | |
struct | dcl_pi2 |
DCL_PI2 object for storing PI2 specific parameters PI2 - PI controller with double integrators. More... | |
Macros | |
#define | PI2_SPS_DEFAULTS { 1.0f, 0.0f, 1.0f, -1.0f } |
Defines default values to initialize DCL_PI2_SPS. More... | |
#define | PI2_DEFAULTS |
Defines default values to initialize DCL_PI2. More... | |
#define | PI2_INT_DEFAULTS |
Macro for internal default values to initialize DCL_PI2 Example: DCL_PI2 pi2_ctrl = { .Kp = 1.0f, .Ki = 0.0f, .Umax = 1.0f, .Umin = -1.0f, PI2_INT_DEFAULTS };. More... | |
#define | DCL_initPI2() &(DCL_PI2)PI2_DEFAULTS |
Initialize DCL_PI2 struct with default parameters Example: DCL_PI2 pi2_ctrl = DCL_initPI2();. More... | |
#define | DCL_initPI2asParam(kp, ki, umax, umin) |
Initialize DCL_PI2 struct with input controller parameters Example: DCL_PI2* pi2_ctrl = DCL_initPI2asParam(1.0f,0.0f,1.0f,-1.0f); Note: input parameter needs to be in the same order as listed in PI2_SPS struct. More... | |
#define | DCL_initPI2asSPS(pi2_ptr, sps_ptr) |
Initialize DCL_PI2 struct with sps parameters Example: DCL_PI2_SPS pi2_sps = { .Kp = , .Ki = , ...}; DCL_PI2 pi2_ctrl; DCL_initPI2asSPS(&pi2_ctrl,&pi2_sps);. More... | |
Typedefs | |
typedef _DCL_VOLATILE struct dcl_pi2 | DCL_PI2 |
typedef _DCL_VOLATILE struct dcl_pi2 * | PI2_Handle |
Functions | |
_DCL_CODE_ACCESS void | DCL_resetPI2 (DCL_PI2 *pi2) |
Resets PI2 internal storage data with interrupt protection. More... | |
_DCL_CODE_ACCESS void | DCL_forceUpdatePI2 (DCL_PI2 *pi2) |
Loads PI2 tuning parameter from its SPS parameter without interrupt protection. More... | |
_DCL_CODE_ACCESS _DCL_CODE_SECTION void | DCL_updatePI2NoCheck (DCL_PI2 *pi2) |
Loads PI2 tuning parameter from its SPS parameter with interrupt protection. More... | |
_DCL_CODE_ACCESS _DCL_CODE_SECTION bool | DCL_updatePI2 (DCL_PI2 *pi2) |
A conditional update based on the update flag. If the update status is set, the function will update PI2 parameter from its SPS parameter and clear the status flag on completion. Note: Use DCL_setUpdateStatus(pi2) to set the update status. More... | |
_DCL_CODE_ACCESS _DCL_CODE_SECTION float32_t | DCL_runPI2Series (DCL_PI2 *pi2, float32_t rk, float32_t yk) |
Executes an inline series form PI2 controller on the FPU32. More... | |