![]() |
![]() |
MSP430UltrasonicLibrary
02_20_00_16
|
This structure is passed to USS_calculateOffsets API and define the test calibration configuration. More...
#include <ussSwLib.h>
Data Fields | |
uint16_t | numOfTestIterations |
bool | isUseLPMCapture |
bool | isCalculateUpsAbsTofOffset |
bool | isCalculateDnsAbsTofOffset |
bool | isCalculateDToFOffset |
This structure is passed to USS_calculateOffsets API and define the test calibration configuration.
uint16_t _USS_dTof_absTof_offset_test_config_::numOfTestIterations |
Specifies the number of time to run offset calibration. Setting a value of 0 will run the calibration one, setting a value of 1 will run calibration twice, etc. minimum: 0 maximum: 64999
Referenced by USS_calculateOffsets().
bool _USS_dTof_absTof_offset_test_config_::isUseLPMCapture |
Specifies the type of capture to use for offset calibration test true = invokes USS_startLowPowerUltrasonicCapture false = invokes USS_startUltrasonicMeasurement
Referenced by USS_calculateOffsets().
bool _USS_dTof_absTof_offset_test_config_::isCalculateUpsAbsTofOffset |
Specifies if calibration returns averaged Absolute Time of Flight for UPS channel true = averaged Absolute Time of Flight for UPS is calculated false = averaged Absolute Time of Flight for UPS is not calculated
Referenced by USS_calculateOffsets().
bool _USS_dTof_absTof_offset_test_config_::isCalculateDnsAbsTofOffset |
Specifies if calibration returns averaged Absolute Time of Flight for DNS channel true = averaged Absolute Time of Flight for DNS is calculated false = averaged Absolute Time of Flight for DNS is not calculated
Referenced by USS_calculateOffsets().
bool _USS_dTof_absTof_offset_test_config_::isCalculateDToFOffset |
Specifies if calibration returns averaged Delta Time of Flight true = averaged Delta Time of Flight is calculated false = averaged Delta Time of Flight is not calculated
Referenced by USS_calculateOffsets().