MSP430UltrasonicLibrary
02_30_00_03
|
Contains USS SW Lib Meter Configuration. More...
#include <ussSwLib.h>
Data Fields | |
float | volumeScaleFactor |
float | volumeAddlScaleFactor |
float | acousticLength |
Acoustic length in usec at room temperature. More... | |
uint32_t | transducerFreq |
Transducer Frequency in Hz. More... | |
Contains USS SW Lib Meter Configuration.
float _USS_Meter_Configuration_::volumeScaleFactor |
Volume scale factor (Area x Length) length^3. This value is used by the library to calculate volume flow rate and is converted to iq21 format as follows _IQ21(volumeScaleFactor/1e6). Therefore, to prevent saturation of volumeflow rate calculation volumeScaleFactor should fall beetween this range [-1.024e9 and 1.023e9]
float _USS_Meter_Configuration_::volumeAddlScaleFactor |
Volume Additional scale factor. This value is used if the volumeScaleFactor needs to be larger than the defined range.
Referenced by USS_scaleVolumeFlowRate().
float _USS_Meter_Configuration_::acousticLength |
Acoustic length in usec at room temperature.
uint32_t _USS_Meter_Configuration_::transducerFreq |
Transducer Frequency in Hz.