MSP430UltrasonicLibrary
02_30_00_03
|
Functions | |
USS_message_code | USS_testPPGconfiguration (USS_SW_Library_configuration *config, USS_test_channel PPGChannel) |
The following API will output current PPG configuration. PPG configuration is controlled via the following USS_Measurement_Configuration parameter: More... | |
USS_message_code | USS_testSDHSconversion (USS_SW_Library_configuration *config, USS_test_channel SDHSChannel, USS_capture_power_mode_option mode) |
The following trigger manual SDHS conversion with current SDHS configuration. SDHS configuration is controlled via the USS_Measurement_Configuration struct and . The API will perform the following operations: More... | |
USS_message_code | USS_startPPGToneGeneration (USS_SW_Library_configuration *config, USS_test_channel PPGChannel) |
The following API will the tone generation output in the SAPH module. Tone generation is controlled via the following USS_Measurement_Configuration parameter: More... | |
USS_message_code | USS_stopPPGToneGeneration (USS_SW_Library_configuration *config) |
The following API will stop the tone generation output in the SAPH module. More... | |
int16_t * | USS_getUPSPtr (USS_SW_Library_configuration *config) |
The following API allows to obtain the address were UPS capture starts. IMPORTANT: USS_configureUltrasonicMeasurement API must be call in the application first before using this API. More... | |
int16_t * | USS_getDNSPtr (USS_SW_Library_configuration *config) |
The following API allows to obtain the address were DNS capture starts. IMPORTANT: USS_configureUltrasonicMeasurement API must be call in the application first before using this API. More... | |
uint8_t * | USS_getAlgorithmObjPtr (void) |
The following API allows to obtain the address where the library algorithm object is stored. The length of the object can be accessed using the USS_getAlgorithmObjLength API. More... | |
uint16_t | USS_getAlgorithmObjLength (void) |
The following API allows to obtain the length of the library algorithm object. More... | |
USS_message_code USS_testPPGconfiguration | ( | USS_SW_Library_configuration * | config, |
USS_test_channel | PPGChannel | ||
) |
The following API will output current PPG configuration.
PPG configuration is controlled via the following USS_Measurement_Configuration parameter:
The user can select the USS channel to test the PPG via the "pPGChannel" input parameter.
[in] | config | is a pointer to the USS SW Library user configuration. |
[in] | PPGChannel | The following are valid options:
|
References commonConfigurePPGForManualMode(), commonPowerDownUSS(), commonTurnOffHSPLLXTAL(), GENERIC_SAPH_KEY, GENERIC_SAPH_PPGTRIG, USS_message_code_no_error, USS_updateSAPHConfiguration(), and USS_updateUUPSConfiguration().
USS_message_code USS_testSDHSconversion | ( | USS_SW_Library_configuration * | config, |
USS_test_channel | SDHSChannel, | ||
USS_capture_power_mode_option | mode | ||
) |
The following trigger manual SDHS conversion with current SDHS configuration. SDHS configuration is controlled via the USS_Measurement_Configuration struct and .
The API will perform the following operations:
[in] | config | is a pointer to the USS SW Library user configuration. |
[in] | SDHSChannel | The following are valid options:
|
[in] | mode | Specifies the capture mode, valid modes are (active or LMP0) |
References commonClearUSSInterrupts(), commonEnableManualSDHSTriggerInterrupts(), commonIsconversionSuccessfull(), commonPowerUpUSS(), commonPrepareForUSSPowerUp(), commonSDHSRestoreSDHSDTCA(), commonWaitForconversion(), GENERIC_SAPH_BCTL, GENERIC_SAPH_ICTL0, GENERIC_SAPH_KEY, USS_message_code_no_error, USS_updateHSPLLConfiguration(), and USS_updateSDHSConfiguration().
USS_message_code USS_startPPGToneGeneration | ( | USS_SW_Library_configuration * | config, |
USS_test_channel | PPGChannel | ||
) |
The following API will the tone generation output in the SAPH module.
Tone generation is controlled via the following USS_Measurement_Configuration parameter:
The user can select the USS channel to test the PPG via the "pPGChannel" input parameter.
[in] | config | is a pointer to the USS SW Library user configuration. |
[in] | PPGChannel | The following are valid options:
|
References commonConfigurePPGDutyCyle(), commonPowerUpUSS(), commonPrepareForUSSPowerUp(), GENERIC_SAPH_KEY, GENERIC_SAPH_PGCTL, _USS_SW_Library_configuration_::measurementConfig, _USS_Measurement_Configuration_::pulseConfig, _USS_Pulse_Configuration_::pulseGenMode, USS_message_code_no_error, USS_test_channel_1, and USS_updateHSPLLConfiguration().
USS_message_code USS_stopPPGToneGeneration | ( | USS_SW_Library_configuration * | config | ) |
The following API will stop the tone generation output in the SAPH module.
[in] | config | is a pointer to the USS SW Library user configuration. |
References commonPowerDownUSS(), commonTurnOffHSPLLXTAL(), GENERIC_SAPH_KEY, GENERIC_SAPH_PGCTL, USS_message_code_no_error, USS_updateSAPHConfiguration(), and USS_updateUUPSConfiguration().
int16_t* USS_getUPSPtr | ( | USS_SW_Library_configuration * | config | ) |
The following API allows to obtain the address were UPS capture starts. IMPORTANT: USS_configureUltrasonicMeasurement API must be call in the application first before using this API.
Referenced by USS_calibrateSignalGain(), and USS_estimateDCoffset().
int16_t* USS_getDNSPtr | ( | USS_SW_Library_configuration * | config | ) |
The following API allows to obtain the address were DNS capture starts. IMPORTANT: USS_configureUltrasonicMeasurement API must be call in the application first before using this API.
Referenced by USS_calibrateSignalGain(), and USS_estimateDCoffset().
uint8_t* USS_getAlgorithmObjPtr | ( | void | ) |
The following API allows to obtain the address where the library algorithm object is stored. The length of the object can be accessed using the USS_getAlgorithmObjLength API.
uint16_t USS_getAlgorithmObjLength | ( | void | ) |
The following API allows to obtain the length of the library algorithm object.