![]() |
![]() |
|
MSP430UltrasonicLibrary
02_30_00_03
|
Contains USS SW Lib Algorithms User Configuration. More...
#include <ussSwLib.h>

Data Fields | |
| uint16_t | absTOFInterval |
| float | ADCAdditionalCaptureDelay |
| float | dcOffset |
| The constant value calibrated by Zero flow drift (sec) More... | |
| float | ratioOfTrackLobeToPeak |
| The ratio of side lobe closest to threshold and peak lobe amplitudes. More... | |
| uint8_t | numPulsesBeforeThreshold |
| The number of pulses/cycles before selected threshold value. More... | |
| uint8_t | windowingMode |
| float | signalValueThresholdCheck |
| uint8_t | numCycleSearchCorrPeak |
| The number of cycles to search for correlation peak. More... | |
| uint16_t | searchLobeSampleSteps |
| float | maxRatioPeak2PeakVariation |
| uint8_t | winStartIndexBackOffNumCycles |
| uint8_t | winTrapzRampOverNumCycles |
| The number of cycles over which the trapezoid window should ramp. More... | |
| uint8_t | winPeakIndex2EdgeNumCycles |
| float | corrValueThresholdCheckFactor |
| int16_t | calibratedDCOffsetUPS |
| int16_t | calibratedDCOffsetDNS |
| bool | isInitAlgorithms |
| This flag is used to indicate if the algorithms have been initialized. More... | |
| USS_dtof_volume_flow_calculation_interval | dtofVolInterval |
| int16_t * | pLEAMemBuffer1 |
| int32_t * | pNvMemBuffer |
| USS_highFlow_option | highFlowOption |
| float | cycleSlipThreshold |
| int32_t | thresholdX1X3 |
| _iq27 | clockRelativeError |
| uint32_t | winNumCycles |
| bool | enableFilter |
| uint16_t | filterLength |
| This parameter is used to specify the filter length. More... | |
| int16_t * | filterCoeffs |
| USS_Alg_AbsToF_Calculation_Option | absToFOption |
| User selection for Absolute Time of Flight calculation option. More... | |
| int16_t * | pLEAMemBuffer2 |
| int16_t * | hilbertTransformCoeffs |
| Pointer to hilbert coefficients, coefficients must 32-bit aligned. More... | |
| uint16_t | hilbertTransformCoeffsLength |
| Length of hilbert coefficients. More... | |
| int16_t | negSearchRange |
| Negative search range for tracking envelope maximum. More... | |
| int16_t | posSearchRange |
| Positive search range for tracking envelope maximum. More... | |
| float | crossThreshold |
| Threshold for tracking crossing point of envelope relative to envelope maximum. More... | |
| int16_t * | pBinaryPattern |
| uint16_t | binaryPatternLength |
| uint16_t | maxBinaryPatternLenght |
| int16_t * | pAdditionalBinaryPattern |
| uint16_t | additionalPatternLength |
| Length of additional binary pattern the length. More... | |
| uint16_t | maxAdditionalBinaryPatternLength |
| USS_Alg_dToF_Calculation_Option | dtoFCalcOption |
| Specifies Delta ToF Calculation option. More... | |
| USS_Alg_volume_flow_Calculation_Option | volumeCalOption |
| Specifies Volume Flow Rate Calculation option. More... | |
| int16_t | maxSampleShift |
| const int16_t(* | pInterpCorrectionTablePtr )[2] |
| int16_t | interpCorrectionTableLenght |
| USS_Alg_volume_flow_Calibration_Option | volumeCalibrationOption |
| Specifies Volume Flow Rate Calibration option. More... | |
| union { | |
| USS_Alg_volume_Flow_Calib_Object * flowCalibObject | |
| USS_Alg_volume_Flow_Temperature_Calib_Object * flowTempCalibObject | |
| } | calibObject |
| USS_Alg_temperature_Calculation_Object * | tempCalcObject |
| USS_Alg_temperature_Calculation_Option | temperatureCalcOption |
| Specifies Temperature Calculation option. More... | |
Contains USS SW Lib Algorithms User Configuration.
| uint16_t _USS_Algorithms_User_Configuration_::absTOFInterval |
This parameter determines the interval to calculate absolute Time of Flight. The interval at which Absolute Time of Flight is calculated has a dependency with dtofVolInterval configuration. If dtofVolInterval == USS_dtof_volume_flow_calculation_interval_1 and absTOFInterval == 1 absolute Time of Flight everytime USS_runAlgorithmsFixedPoint or USS_runAlgorithms API are called. If dtofVolInterval == USS_dtof_volume_flow_calculation_interval_2 and absTOFInterval == 10 absolute Time of Flight is calculated the 20th time USS_runAlgorithmsFixedPoint and USS_runAlgorithms are invoked. The last calculation of Absolute time of flight is return until the next update occurs. Increasing the value for "absTOFIteration" reduces the average consumption of the application. (valid range 1-65535)
| float _USS_Algorithms_User_Configuration_::ADCAdditionalCaptureDelay |
The additional time it takes during firing and capturing the data, which is not accounted for anywhere else.
| float _USS_Algorithms_User_Configuration_::dcOffset |
The constant value calibrated by Zero flow drift (sec)
| float _USS_Algorithms_User_Configuration_::ratioOfTrackLobeToPeak |
The ratio of side lobe closest to threshold and peak lobe amplitudes.
| uint8_t _USS_Algorithms_User_Configuration_::numPulsesBeforeThreshold |
The number of pulses/cycles before selected threshold value.
| uint8_t _USS_Algorithms_User_Configuration_::windowingMode |
This variable is used to define which windowing configuration is enabled . When windowing is enabled, it allows you to specify the window type to be used. This window is only applied on the captured DNS & UPS signals for the Delta ToF (DToF) computation. The options below are only applicable when using USS_ALG_DTOF_COMPUTATION_MODE= USS_ALG_DTOF_COMPUTATION_OPTION_ESTIMATE. The memory (in bytes) required when windowing is not USS_ALG_DTOF_EST_WINDOW_OPTION_DISABLED can be calculated using: USS_SW_LIB_APP_MAX_WINDOW_RAMP_SIZE = 2 * [ROUND ( USS_ALG_WIN_TRAP_RAMP_NUM_CYCLES * [(USS_PLL_FREQ / USS_SDHS_OVER_SAMPLE_RATE) / USS_F1_FREQ ] ) + 2];
USS_ALG_DTOF_EST_WINDOW_OPTION_DISABLED : This setting disables the window application on the captured signal.
USS_ALG_DTOF_EST_WINDOW_OPTION_STATIC: The applied window is static with reference to the start of the capture signal. Even if the captured DNS and UPS signals move because of changes in flow rates or due to temperature, the applied window is always the same with reference to the start of the capture signal. The applied window is trapezoidal in nature and specified by .winTrapzRampOverNumCycles (USS_ALG_WIN_TRAP_RAMP_NUM_CYCLES), .winNumCycles (USS_ALG_WIN_NUM_CYCLES) and .winStartIndexBackOffNumCycles (USS_ALG_WIN_START_INDEX_BACK_OFF_NUM_CYCLES). In all these parameters, the NumCycles refers to the number of transducer cycles. winStartIndexBackOffNumCycles defines the window start with reference to the start of the capture signal. The window is 0 from the start of the capture to winStartIndexBackOffNumCycles. winTrapzRampOverNumCycles defines the number of cycles over which the window ramps from 0 to 1. It similarly defines the number of cycles over which the window ramps down from 1 to 0. winNumCycles defines the length of the window in terms of transducer cycles when it is 1. In effect, the total window length is defined by winTrapzRampOverNumCycles + winNumCycles + winTrapzRampOverNumCycles and the position is defined by winStartIndexBackOffNumCycles.
USS_ALG_DTOF_EST_WINDOW_OPTION_ESTIMATE: The applied window is static in terms of the length but the start position of the applied window is dependent on the start of the signal defined by AbsToF for UPS and DNS independently. The applied window shape is similar to the window defined in USS_ALG_DTOF_EST_WINDOW_OPTION_STATIC.
USS_ALG_DTOF_EST_WINDOW_OPTION_DYNAMIC: The applied window is dynamic in terms of the size of the window itself and is defined with reference to the position of the peak of the signal. The applied window is trapezoidal in nature and specified by .winTrapzRampOverNumCycles (USS_ALG_WIN_TRAP_RAMP_NUM_CYCLES), .winStartIndexBackOffNumCycles (USS_ALG_WIN_START_INDEX_BACK_OFF_NUM_CYCLES) and .winPeakIndex2EdgeNumCycles (USS_ALG_WIN_PEAK_INDEX_2_EDGES_NUM_CYLES). winStartIndexBackOffNumCycles defines the window start with reference to the start of the capture signal. winTrapzRampOverNumCycles defines the number of cycles over which the window ramps from 0 to 1. It similarly defines the number of cycles over which the window ramps down from 1 to 0. The window is set to 1 till winPeakIndex2EdgeNumCycles after the peak of the signal. In effect, the total window length is not known and is dependent on the position of the peak of the signal.
If USS_ALG_DTOF_COMPUTATION_MODE= USS_ALG_DTOF_COMPUTATION_OPTION_WATER, then the windowingMode is a flag to enable or disable windowing. Memory in bytes required for windowing is USS_SW_LIB_APP_MAX_WINDOW_RAMP_SIZE = 2 * (USS_SW_LIB_APP_MAX_CAPTURE_SIZE + USS_SW_LIB_APP_MAX_FILTER_LENGTH) The options below are only applicable when using USS_ALG_DTOF_COMPUTATION_MODE= USS_ALG_DTOF_COMPUTATION_OPTION_WATER.
USS_ALG_DTOF_WATER_WINDOW_OPTION_DISABLED: This setting disables the window application on the captured signal
USS_ALG_DTOF_WATER_WINDOW_OPTION_ENABLE: The applied window is static in terms of the length but the start position of the applied window is dependent on the start of the signal defined by AbsToF for DNS. The same start position is also used for UPS. The applied window shape is similar to the window defined in USS_ALG_DTOF_EST_WINDOW_OPTION_STATIC.
| float _USS_Algorithms_User_Configuration_::signalValueThresholdCheck |
The signal value check parameter which has to be crossed for a valid signal
| uint8_t _USS_Algorithms_User_Configuration_::numCycleSearchCorrPeak |
The number of cycles to search for correlation peak.
| uint16_t _USS_Algorithms_User_Configuration_::searchLobeSampleSteps |
The number of samples to increment/decrement while searching/tracking the side lobe
| float _USS_Algorithms_User_Configuration_::maxRatioPeak2PeakVariation |
The maximum ratio of allowed peak to peak variation from one measurement to another before setting flag for search.
| uint8_t _USS_Algorithms_User_Configuration_::winStartIndexBackOffNumCycles |
The number of cycles to back off from start of received pulse (derived from absTOF) (applies to static windowing only)
| uint8_t _USS_Algorithms_User_Configuration_::winTrapzRampOverNumCycles |
The number of cycles over which the trapezoid window should ramp.
| uint8_t _USS_Algorithms_User_Configuration_::winPeakIndex2EdgeNumCycles |
The number of cycles from peak of signal to edge (or start) of window down ramp (applies to dynamic windowing only)
| float _USS_Algorithms_User_Configuration_::corrValueThresholdCheckFactor |
The factor of maximum lobe energy which has to be crossed for a valid correlation value
| int16_t _USS_Algorithms_User_Configuration_::calibratedDCOffsetUPS |
This is a constant value which is subtracted to UPS captures before running the Delta ToF algorithms. This parameter can be obtained using USS_estimateDCoffset API
Referenced by USS_estimateDCoffset().
| int16_t _USS_Algorithms_User_Configuration_::calibratedDCOffsetDNS |
This is a constant value which is subtracted to DNS captures before running the Delta ToF algorithms. This parameter can be obtained using USS_estimateDCoffset API
Referenced by USS_estimateDCoffset().
| bool _USS_Algorithms_User_Configuration_::isInitAlgorithms |
This flag is used to indicate if the algorithms have been initialized.
| USS_dtof_volume_flow_calculation_interval _USS_Algorithms_User_Configuration_::dtofVolInterval |
This configuration specifies the interval at which delta ToF and volume flow are calculated. The last calculated DToF and volume flow will be return between intervals.
| int16_t* _USS_Algorithms_User_Configuration_::pLEAMemBuffer1 |
pointer to LEA RAM memory reserved to place windowing coefficients. memory minimum size (sampleSize*numberOfAcquisitions + filterLength * 2) bytes
| int32_t* _USS_Algorithms_User_Configuration_::pNvMemBuffer |
pointer to non volatile memory reserved for algorithm computations. memory minimum size (sampleSize*2) bytes
| USS_highFlow_option _USS_Algorithms_User_Configuration_::highFlowOption |
Setting this configuration to true will enable highflow rate (> 5 gpm) operation. NOTE: enabling this option will increase power consumption
| float _USS_Algorithms_User_Configuration_::cycleSlipThreshold |
This setting is only need if USS_highFlow_option_version1 is selected typical values are 1.1 and 1.2
| int32_t _USS_Algorithms_User_Configuration_::thresholdX1X3 |
| _iq27 _USS_Algorithms_User_Configuration_::clockRelativeError |
This setting is used to correct AbsToF calculation clockRelativeError = (clk_freq_measured-clock_freq_nominal)/clock_freq_nominal Users can take advantage of USS_verifyHSPLLFrequency API. Which will return the the expected timer counts and actual measured timer count For more details about USS_verifyHSPLLFrequency implementation please refer the Library API guide. Valid range is [_IQ27(-0.1),_IQ27(0.1)] If USS_verifyHSPLLFrequency API is used then the error can be calculated as follows: gUssSWConfig.algorithmsConfig->clockRelativeError = _IQ27div((int32_t)(hspll_results.actualTestCount - hspll_results.expectedResult),hspll_results.expectedResult);
| uint32_t _USS_Algorithms_User_Configuration_::winNumCycles |
This parameter is used to control the windowLength when enableWindowing is set to true. winLength = (2* winRampLength) + (numSamplesPerCycle *winNumCycles) Where, winRampLength = numSamplesPerCycle * winTrapzRampOverNumCycles; numSamplesPerCycle = sampleFreq/transducerFreq; For DToF Gas SingleTone Correlated: winLength is Dynamic internally and set as winLength = numSamples2Peak + (numSamplesPerCycle * winPeakIndex2EdgeNumCycles)
| bool _USS_Algorithms_User_Configuration_::enableFilter |
This parameter is used to enabling filtering of the signal before running AbsToF, DeltaToF and Volume algorithms
| uint16_t _USS_Algorithms_User_Configuration_::filterLength |
This parameter is used to specify the filter length.
Referenced by commonSDHSRestoreSDHSDTCA().
| int16_t* _USS_Algorithms_User_Configuration_::filterCoeffs |
This parameter is used to provide the memory location were the filter coefficients will be loaded from
| USS_Alg_AbsToF_Calculation_Option _USS_Algorithms_User_Configuration_::absToFOption |
User selection for Absolute Time of Flight calculation option.
| int16_t* _USS_Algorithms_User_Configuration_::pLEAMemBuffer2 |
pointer to LEA RAM memory reserved temporary LEA operations. This section of memory can be reused in the application for temporary operations. The content of in this memory is not preserved during when USS_run* functions are called.
| int16_t* _USS_Algorithms_User_Configuration_::hilbertTransformCoeffs |
Pointer to hilbert coefficients, coefficients must 32-bit aligned.
| uint16_t _USS_Algorithms_User_Configuration_::hilbertTransformCoeffsLength |
Length of hilbert coefficients.
| int16_t _USS_Algorithms_User_Configuration_::negSearchRange |
Negative search range for tracking envelope maximum.
| int16_t _USS_Algorithms_User_Configuration_::posSearchRange |
Positive search range for tracking envelope maximum.
| float _USS_Algorithms_User_Configuration_::crossThreshold |
Threshold for tracking crossing point of envelope relative to envelope maximum.
| int16_t* _USS_Algorithms_User_Configuration_::pBinaryPattern |
Pointer to array containing binary reference pattern used by USS_Alg_AbsToF_Calculation_Option_lobeWide and USS_Alg_AbsToF_Calculation_Option_hilbertWide The library can use the binary pattern calculated by USS_generateMonoDualToneBinaryPattern and USS_generateMultiToneBinaryPattern APIs or user can passed a predefined binary pattern.
| uint16_t _USS_Algorithms_User_Configuration_::binaryPatternLength |
Length of binary pattern the length is automatically calculated by USS_generateMonoDualToneBinaryPattern and USS_generateMultiToneBinaryPattern APIS if using predefined binary patterns user must specify the length of the pattern.
| uint16_t _USS_Algorithms_User_Configuration_::maxBinaryPatternLenght |
This value is used by USS_generateMultiToneBinaryPattern and USS_generateMonoDualToneBinaryPattern to avoid overflowing the binary pattern array
| int16_t* _USS_Algorithms_User_Configuration_::pAdditionalBinaryPattern |
Pointer to additional binary pattern. This pattern will be append to the binary pattern calculated by USS_generateMonoDualToneBinaryPattern USS_generateMultiToneBinaryPattern
| uint16_t _USS_Algorithms_User_Configuration_::additionalPatternLength |
Length of additional binary pattern the length.
| uint16_t _USS_Algorithms_User_Configuration_::maxAdditionalBinaryPatternLength |
This value is used by USS_generateMultiToneBinaryPattern and USS_generateMonoDualToneBinaryPattern to avoid overflowing the binary pattern array
| USS_Alg_dToF_Calculation_Option _USS_Algorithms_User_Configuration_::dtoFCalcOption |
Specifies Delta ToF Calculation option.
| USS_Alg_volume_flow_Calculation_Option _USS_Algorithms_User_Configuration_::volumeCalOption |
Specifies Volume Flow Rate Calculation option.
| int16_t _USS_Algorithms_User_Configuration_::maxSampleShift |
Maximum shift in samples for calculating deltaTOF (setting for high flow) Parameter specifying maximum shift in samples for deltaTOF calculation, e.g. setting of 8 with 4 samples per cycle supports high flow +/- 2 cycles.
| const int16_t(* _USS_Algorithms_User_Configuration_::pInterpCorrectionTablePtr)[2] |
Pointer to look-up table (LUT) used for interpolation correction. A null pointer will disable using offset correction (less accuracy for absTOF).
| int16_t _USS_Algorithms_User_Configuration_::interpCorrectionTableLenght |
Length of look-up table (LUT) used for interpolation correction. Must be a power of two.
| USS_Alg_volume_flow_Calibration_Option _USS_Algorithms_User_Configuration_::volumeCalibrationOption |
Specifies Volume Flow Rate Calibration option.
Referenced by USS_calibrateVolumeFlowRate(), and USS_scaleVolumeFlowRate().
| USS_Alg_volume_Flow_Calib_Object* _USS_Algorithms_User_Configuration_::flowCalibObject |
Specifies Volume Flow Rate Flow (only) Calibration object, it must be initialized for when volumeCalibrationOption = USS_Alg_volume_flow_Calibration_Option_flow
Referenced by USS_calibrateVFRFlow().
| USS_Alg_volume_Flow_Temperature_Calib_Object* _USS_Algorithms_User_Configuration_::flowTempCalibObject |
Specifies Volume Flow Rate Flow + Temperature Calibration object, it must be initialized for when volumeCalibrationOption = USS_Alg_volume_flow_Calibration_Option_flow_temperature
Referenced by USS_calculateVolumeFlowRate(), USS_calibrateVFRFlowTemperature(), USS_initialSearchQuad(), USS_isPtInside(), and USS_searchNeighborQuad().
| union { ... } _USS_Algorithms_User_Configuration_::calibObject |
| USS_Alg_temperature_Calculation_Object* _USS_Algorithms_User_Configuration_::tempCalcObject |
Specifies Temperature Calculation object used to calculate temperature using UPS and DNS absToF.
Referenced by USS_calculateVelocity(), and USS_computeTemperature().
| USS_Alg_temperature_Calculation_Option _USS_Algorithms_User_Configuration_::temperatureCalcOption |
Specifies Temperature Calculation option.
Referenced by USS_runAlgorithms().