This package provides API documentation for all the peripherals in the MSP430 Driver Library. MSP430 Driver Library provides an easy to use API for developing applications for the MSP430FR2xx_4xx devices.
The easiest way to get started is to click on the "Modules" tab above. This will provide an alphabetical list of peripherals available in the MSP430 Driver Library.
This API documentation is broken out into the following sections:
Also note the existence of the following content available on disk. This is not part of this API but contains useful example code and documentation.