MSP430 DriverLib for MSP430FR5xx_6xx Devices  2.21.00.08
 All Data Structures Functions Variables Modules Pages
Timer_A_initCaptureModeParam Struct Reference

Used in the Timer_A_initCaptureMode() function as the param parameter. More...

#include <timer_a.h>

Data Fields

uint16_t captureRegister
 
uint16_t captureMode
 
uint16_t captureInputSelect
 
uint16_t synchronizeCaptureSource
 
uint16_t captureInterruptEnable
 
uint16_t captureOutputMode
 

Detailed Description

Used in the Timer_A_initCaptureMode() function as the param parameter.

Field Documentation

uint16_t Timer_A_initCaptureModeParam::captureInputSelect

Decides the Input Select
Valid values are:

  • TIMER_A_CAPTURE_INPUTSELECT_CCIxA
  • TIMER_A_CAPTURE_INPUTSELECT_CCIxB
  • TIMER_A_CAPTURE_INPUTSELECT_GND
  • TIMER_A_CAPTURE_INPUTSELECT_Vcc

Referenced by Timer_A_initCaptureMode().

uint16_t Timer_A_initCaptureModeParam::captureInterruptEnable

Is to enable or disable timer captureComapre interrupt.
Valid values are:

  • TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE [Default]
  • TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE

Referenced by Timer_A_initCaptureMode().

uint16_t Timer_A_initCaptureModeParam::captureMode

Is the capture mode selected.
Valid values are:

  • TIMER_A_CAPTUREMODE_NO_CAPTURE [Default]
  • TIMER_A_CAPTUREMODE_RISING_EDGE
  • TIMER_A_CAPTUREMODE_FALLING_EDGE
  • TIMER_A_CAPTUREMODE_RISING_AND_FALLING_EDGE

Referenced by Timer_A_initCaptureMode().

uint16_t Timer_A_initCaptureModeParam::captureOutputMode

Specifies the output mode.
Valid values are:

  • TIMER_A_OUTPUTMODE_OUTBITVALUE [Default]
  • TIMER_A_OUTPUTMODE_SET
  • TIMER_A_OUTPUTMODE_TOGGLE_RESET
  • TIMER_A_OUTPUTMODE_SET_RESET
  • TIMER_A_OUTPUTMODE_TOGGLE
  • TIMER_A_OUTPUTMODE_RESET
  • TIMER_A_OUTPUTMODE_TOGGLE_SET
  • TIMER_A_OUTPUTMODE_RESET_SET

Referenced by Timer_A_initCaptureMode().

uint16_t Timer_A_initCaptureModeParam::captureRegister

Selects the Capture register being used. Refer to datasheet to ensure the device has the capture compare register being used.
Valid values are:

  • TIMER_A_CAPTURECOMPARE_REGISTER_0
  • TIMER_A_CAPTURECOMPARE_REGISTER_1
  • TIMER_A_CAPTURECOMPARE_REGISTER_2
  • TIMER_A_CAPTURECOMPARE_REGISTER_3
  • TIMER_A_CAPTURECOMPARE_REGISTER_4
  • TIMER_A_CAPTURECOMPARE_REGISTER_5
  • TIMER_A_CAPTURECOMPARE_REGISTER_6

Referenced by Timer_A_initCaptureMode().

uint16_t Timer_A_initCaptureModeParam::synchronizeCaptureSource

Decides if capture source should be synchronized with timer clock
Valid values are:

  • TIMER_A_CAPTURE_ASYNCHRONOUS [Default]
  • TIMER_A_CAPTURE_SYNCHRONOUS

Referenced by Timer_A_initCaptureMode().


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated