Used in the RTC_C_configureCalendarAlarm() function as the param parameter. More...
#include <rtc_c.h>
Data Fields | |
uint8_t | minutesAlarm |
uint8_t | hoursAlarm |
uint8_t | dayOfWeekAlarm |
uint8_t | dayOfMonthAlarm |
Used in the RTC_C_configureCalendarAlarm() function as the param parameter.
uint8_t RTC_C_configureCalendarAlarmParam::dayOfMonthAlarm |
Is the alarm condition for the day of the month.
Valid values are:
Referenced by RTC_C_configureCalendarAlarm().
uint8_t RTC_C_configureCalendarAlarmParam::dayOfWeekAlarm |
Is the alarm condition for the day of week.
Valid values are:
Referenced by RTC_C_configureCalendarAlarm().
uint8_t RTC_C_configureCalendarAlarmParam::hoursAlarm |
Is the alarm condition for the hours.
Valid values are:
Referenced by RTC_C_configureCalendarAlarm().
uint8_t RTC_C_configureCalendarAlarmParam::minutesAlarm |
Is the alarm condition for the minutes.
Valid values are:
Referenced by RTC_C_configureCalendarAlarm().