Used in the MPU_initThreeSegments() function as the param parameter. More...
#include <mpu.h>
Data Fields | |
uint16_t | seg1boundary |
Valid values can be found in the Family User's Guide. | |
uint16_t | seg2boundary |
Valid values can be found in the Family User's Guide. | |
uint8_t | seg1accmask |
uint8_t | seg2accmask |
uint8_t | seg3accmask |
Used in the MPU_initThreeSegments() function as the param parameter.
uint8_t MPU_initThreeSegmentsParam::seg1accmask |
Is the bit mask of access right for memory segment 1.
Logical OR of any of the following:
Referenced by MPU_initThreeSegments().
uint8_t MPU_initThreeSegmentsParam::seg2accmask |
Is the bit mask of access right for memory segment 2.
Logical OR of any of the following:
Referenced by MPU_initThreeSegments().
uint8_t MPU_initThreeSegmentsParam::seg3accmask |
Is the bit mask of access right for memory segment 3.
Logical OR of any of the following:
Referenced by MPU_initThreeSegments().