Used in the LCD_C_init() function as the initParams parameter.
More...
#include <lcd_c.h>
Used in the LCD_C_init() function as the initParams parameter.
uint16_t LCD_C_initParam::clockDivider |
Selects the divider for LCD_frequency.
Valid values are:
- LCD_C_CLOCKDIVIDER_1 [Default]
- LCD_C_CLOCKDIVIDER_2
- LCD_C_CLOCKDIVIDER_3
- LCD_C_CLOCKDIVIDER_4
- LCD_C_CLOCKDIVIDER_5
- LCD_C_CLOCKDIVIDER_6
- LCD_C_CLOCKDIVIDER_7
- LCD_C_CLOCKDIVIDER_8
- LCD_C_CLOCKDIVIDER_9
- LCD_C_CLOCKDIVIDER_10
- LCD_C_CLOCKDIVIDER_11
- LCD_C_CLOCKDIVIDER_12
- LCD_C_CLOCKDIVIDER_13
- LCD_C_CLOCKDIVIDER_14
- LCD_C_CLOCKDIVIDER_15
- LCD_C_CLOCKDIVIDER_16
- LCD_C_CLOCKDIVIDER_17
- LCD_C_CLOCKDIVIDER_18
- LCD_C_CLOCKDIVIDER_19
- LCD_C_CLOCKDIVIDER_20
- LCD_C_CLOCKDIVIDER_21
- LCD_C_CLOCKDIVIDER_22
- LCD_C_CLOCKDIVIDER_23
- LCD_C_CLOCKDIVIDER_24
- LCD_C_CLOCKDIVIDER_25
- LCD_C_CLOCKDIVIDER_26
- LCD_C_CLOCKDIVIDER_27
- LCD_C_CLOCKDIVIDER_28
- LCD_C_CLOCKDIVIDER_29
- LCD_C_CLOCKDIVIDER_30
- LCD_C_CLOCKDIVIDER_31
- LCD_C_CLOCKDIVIDER_32
Referenced by LCD_C_init().
uint16_t LCD_C_initParam::clockPrescalar |
Selects the prescalar for frequency.
Valid values are:
- LCD_C_CLOCKPRESCALAR_1 [Default]
- LCD_C_CLOCKPRESCALAR_2
- LCD_C_CLOCKPRESCALAR_4
- LCD_C_CLOCKPRESCALAR_8
- LCD_C_CLOCKPRESCALAR_16
- LCD_C_CLOCKPRESCALAR_32
Referenced by LCD_C_init().
uint16_t LCD_C_initParam::clockSource |
Selects the clock that will be used by the LCD.
Valid values are:
- LCD_C_CLOCKSOURCE_ACLK [Default]
- LCD_C_CLOCKSOURCE_VLOCLK
Referenced by LCD_C_init().
uint16_t LCD_C_initParam::muxRate |
Selects LCD mux rate.
Valid values are:
- LCD_C_STATIC [Default]
- LCD_C_2_MUX
- LCD_C_3_MUX
- LCD_C_4_MUX
- LCD_C_5_MUX
- LCD_C_6_MUX
- LCD_C_7_MUX
- LCD_C_8_MUX
Referenced by LCD_C_init().
uint16_t LCD_C_initParam::segments |
Sets LCD segment on/off.
Valid values are:
- LCD_C_SEGMENTS_DISABLED [Default]
- LCD_C_SEGMENTS_ENABLED
Referenced by LCD_C_init().
uint16_t LCD_C_initParam::waveforms |
Selects LCD waveform mode.
Valid values are:
- LCD_C_STANDARD_WAVEFORMS [Default]
- LCD_C_LOW_POWER_WAVEFORMS
Referenced by LCD_C_init().
The documentation for this struct was generated from the following file: