MSP430 DriverLib for MSP430FR5xx_6xx Devices  2.21.00.08
 All Data Structures Functions Variables Modules Pages
EUSCI_B_SPI_changeMasterClockParam Struct Reference

Used in the EUSCI_B_SPI_changeMasterClock() function as the param parameter. More...

#include <eusci_b_spi.h>

Data Fields

uint32_t clockSourceFrequency
 Is the frequency of the selected clock source.
 
uint32_t desiredSpiClock
 Is the desired clock rate for SPI communication.
 

Detailed Description

Used in the EUSCI_B_SPI_changeMasterClock() function as the param parameter.


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated