Functions | |
void | Ref_A_setReferenceVoltage (uint16_t baseAddress, uint8_t referenceVoltageSelect) |
Sets the reference voltage for the voltage generator. More... | |
void | Ref_A_disableTempSensor (uint16_t baseAddress) |
Disables the internal temperature sensor to save power consumption. More... | |
void | Ref_A_enableTempSensor (uint16_t baseAddress) |
Enables the internal temperature sensor. More... | |
void | Ref_A_enableReferenceVoltageOutput (uint16_t baseAddress) |
Outputs the reference voltage to an output pin. More... | |
void | Ref_A_disableReferenceVoltageOutput (uint16_t baseAddress) |
Disables the reference voltage as an output to a pin. More... | |
void | Ref_A_enableReferenceVoltage (uint16_t baseAddress) |
Enables the reference voltage to be used by peripherals. More... | |
void | Ref_A_disableReferenceVoltage (uint16_t baseAddress) |
Disables the reference voltage. More... | |
uint16_t | Ref_A_getBandgapMode (uint16_t baseAddress) |
Returns the bandgap mode of the Ref_A module. More... | |
bool | Ref_A_isBandgapActive (uint16_t baseAddress) |
Returns the active status of the bandgap in the Ref_A module. More... | |
uint16_t | Ref_A_isRefGenBusy (uint16_t baseAddress) |
Returns the busy status of the reference generator in the Ref_A module. More... | |
bool | Ref_A_isRefGenActive (uint16_t baseAddress) |
Returns the active status of the reference generator in the Ref_A module. More... | |
bool | Ref_A_isBufferedBandgapVoltageReady (uint16_t baseAddress) |
Returns the busy status of the reference generator in the Ref_A module. More... | |
bool | Ref_A_isVariableReferenceVoltageOutputReady (uint16_t baseAddress) |
Returns the busy status of the variable reference voltage in the Ref_A module. More... | |
void | Ref_A_setReferenceVoltageOneTimeTrigger (uint16_t baseAddress) |
Enables the one-time trigger of the reference voltage. More... | |
void | Ref_A_setBufferedBandgapVoltageOneTimeTrigger (uint16_t baseAddress) |
Enables the one-time trigger of the buffered bandgap voltage. More... | |
void Ref_A_disableReferenceVoltage | ( | uint16_t | baseAddress | ) |
Disables the reference voltage.
This function is used to disable the generated reference voltage. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFON of REFCTL0 register.
void Ref_A_disableReferenceVoltageOutput | ( | uint16_t | baseAddress | ) |
Disables the reference voltage as an output to a pin.
This function is used to disables the reference voltage being generated to be given to an output pin. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFOUT of REFCTL0 register.
void Ref_A_disableTempSensor | ( | uint16_t | baseAddress | ) |
Disables the internal temperature sensor to save power consumption.
This function is used to turn off the internal temperature sensor to save on power consumption. The temperature sensor is enabled by default. Please note, that giving ADC12 module control over the Ref_A module, the state of the temperature sensor is dependent on the controls of the ADC12 module. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFTCOFF of REFCTL0 register.
void Ref_A_enableReferenceVoltage | ( | uint16_t | baseAddress | ) |
Enables the reference voltage to be used by peripherals.
This function is used to enable the generated reference voltage to be used other peripherals or by an output pin, if enabled. Please note, that giving ADC12 module control over the Ref_A module, the state of the reference voltage is dependent on the controls of the ADC12 module. Please note, ADC10_A does not support the reference request. If the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFON of REFCTL0 register.
void Ref_A_enableReferenceVoltageOutput | ( | uint16_t | baseAddress | ) |
Outputs the reference voltage to an output pin.
This function is used to output the reference voltage being generated to an output pin. Please note, the output pin is device specific. Please note, that giving ADC12 module control over the Ref_A module, the state of the reference voltage as an output to a pin is dependent on the controls of the ADC12 module. If ADC12_A reference burst is disabled or DAC12_A is enabled, this output is available continuously. If ADC12_A reference burst is enabled, this output is available only during an ADC12_A conversion. For devices with CTSD16, Ref_enableReferenceVoltage() needs to be invoked to get VREFBG available continuously. Otherwise, VREFBG is only available externally when a module requests it. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFOUT of REFCTL0 register.
void Ref_A_enableTempSensor | ( | uint16_t | baseAddress | ) |
Enables the internal temperature sensor.
This function is used to turn on the internal temperature sensor to use by other peripherals. The temperature sensor is enabled by default. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
Modified bits are REFTCOFF of REFCTL0 register.
uint16_t Ref_A_getBandgapMode | ( | uint16_t | baseAddress | ) |
Returns the bandgap mode of the Ref_A module.
This function is used to return the bandgap mode of the Ref_A module, requested by the peripherals using the bandgap. If a peripheral requests static mode, then the bandgap mode will be static for all modules, whereas if all of the peripherals using the bandgap request sample mode, then that will be the mode returned. Sample mode allows the bandgap to be active only when necessary to save on power consumption, static mode requires the bandgap to be active until no peripherals are using it anymore.
baseAddress | is the base address of the REF_A module. |
bool Ref_A_isBandgapActive | ( | uint16_t | baseAddress | ) |
Returns the active status of the bandgap in the Ref_A module.
This function is used to return the active status of the bandgap in the Ref_A module. If the bandgap is in use by a peripheral, then the status will be seen as active.
baseAddress | is the base address of the REF_A module. |
bool Ref_A_isBufferedBandgapVoltageReady | ( | uint16_t | baseAddress | ) |
Returns the busy status of the reference generator in the Ref_A module.
This function is used to return the buys status of the buffered bandgap voltage in the Ref_A module. If the ref generator is on and ready to use, then the status will be seen as active.
baseAddress | is the base address of the REF_A module. |
bool Ref_A_isRefGenActive | ( | uint16_t | baseAddress | ) |
Returns the active status of the reference generator in the Ref_A module.
This function is used to return the active status of the reference generator in the Ref_A module. If the ref generator is on and ready to use, then the status will be seen as active.
baseAddress | is the base address of the REF_A module. |
uint16_t Ref_A_isRefGenBusy | ( | uint16_t | baseAddress | ) |
Returns the busy status of the reference generator in the Ref_A module.
This function is used to return the busy status of the reference generator in the Ref_A module. If the ref generator is in use by a peripheral, then the status will be seen as busy.
baseAddress | is the base address of the REF_A module. |
bool Ref_A_isVariableReferenceVoltageOutputReady | ( | uint16_t | baseAddress | ) |
Returns the busy status of the variable reference voltage in the Ref_A module.
This function is used to return the busy status of the variable reference voltage in the Ref_A module. If the ref generator is on and ready to use, then the status will be seen as active.
baseAddress | is the base address of the REF_A module. |
void Ref_A_setBufferedBandgapVoltageOneTimeTrigger | ( | uint16_t | baseAddress | ) |
Enables the one-time trigger of the buffered bandgap voltage.
Triggers the one-time generation of the buffered bandgap voltage. Once the buffered bandgap voltage request is set, this bit is cleared by hardware
baseAddress | is the base address of the REF_A module. |
Modified bits are REFBGOT of REFCTL0 register.
void Ref_A_setReferenceVoltage | ( | uint16_t | baseAddress, |
uint8_t | referenceVoltageSelect | ||
) |
Sets the reference voltage for the voltage generator.
This function sets the reference voltage generated by the voltage generator to be used by other peripherals. This reference voltage will only be valid while the Ref_A module is in control. Please note, if the Ref_A_isRefGenBusy() returns Ref_A_BUSY, this function will have no effect.
baseAddress | is the base address of the REF_A module. |
referenceVoltageSelect | is the desired voltage to generate for a reference voltage. Valid values are:
|
void Ref_A_setReferenceVoltageOneTimeTrigger | ( | uint16_t | baseAddress | ) |
Enables the one-time trigger of the reference voltage.
Triggers the one-time generation of the variable reference voltage. Once the reference voltage request is set, this bit is cleared by hardware
baseAddress | is the base address of the REF_A module. |
Modified bits are REFGENOT of REFCTL0 register.