MSP430 DriverLib for MSP430FR5xx_6xx Devices  2.21.00.08
 All Data Structures Functions Variables Modules Pages
framctl

Functions

void FRAMCtl_write8 (uint8_t *dataPtr, uint8_t *framPtr, uint16_t numberOfBytes)
 Write data into the fram memory in byte format. More...
 
void FRAMCtl_write16 (uint16_t *dataPtr, uint16_t *framPtr, uint16_t numberOfWords)
 Write data into the fram memory in word format. More...
 
void FRAMCtl_write32 (uint32_t *dataPtr, uint32_t *framPtr, uint16_t count)
 Write data into the fram memory in long format, pass by reference. More...
 
void FRAMCtl_fillMemory32 (uint32_t value, uint32_t *framPtr, uint16_t count)
 Write data into the fram memory in long format, pass by value. More...
 
void FRAMCtl_enableInterrupt (uint8_t interruptMask)
 Enables selected FRAMCtl interrupt sources. More...
 
uint8_t FRAMCtl_getInterruptStatus (uint16_t interruptFlagMask)
 Returns the status of the selected FRAMCtl interrupt flags. More...
 
void FRAMCtl_disableInterrupt (uint16_t interruptMask)
 Disables selected FRAMCtl interrupt sources. More...
 
void FRAMCtl_configureWaitStateControl (uint8_t waitState)
 Configures the access time of the FRAMCtl module. More...
 
void FRAMCtl_delayPowerUpFromLPM (uint8_t delayStatus)
 Configures when the FRAMCtl module will power up after LPM exit. More...
 

Detailed Description

Function Documentation

void FRAMCtl_configureWaitStateControl ( uint8_t  waitState)

Configures the access time of the FRAMCtl module.

Configures the access time of the FRAMCtl module.

Parameters
waitStatedefines the number of CPU cycles required for access time defined in the datasheet Valid values are:
  • FRAMCTL_ACCESS_TIME_CYCLES_0
  • FRAMCTL_ACCESS_TIME_CYCLES_1
  • FRAMCTL_ACCESS_TIME_CYCLES_2
  • FRAMCTL_ACCESS_TIME_CYCLES_3
  • FRAMCTL_ACCESS_TIME_CYCLES_4
  • FRAMCTL_ACCESS_TIME_CYCLES_5
  • FRAMCTL_ACCESS_TIME_CYCLES_6
  • FRAMCTL_ACCESS_TIME_CYCLES_7

Modified bits are NWAITS of GCCTL0 register.

Returns
None
void FRAMCtl_delayPowerUpFromLPM ( uint8_t  delayStatus)

Configures when the FRAMCtl module will power up after LPM exit.

Configures when the FRAMCtl module will power up after LPM exit. The module can either wait until the first FRAMCtl access to power up or power up immediately after leaving LPM. If FRAMCtl power is disabled, a memory access will automatically insert wait states to ensure sufficient timing for the FRAMCtl power-up and access.

Parameters
delayStatuschooses if FRAMCTL should power up instantly with LPM exit or to wait until first FRAMCTL access after LPM exit Valid values are:
  • FRAMCTL_DELAY_FROM_LPM_ENABLE
  • FRAMCTL_DELAY_FROM_LPM_DISABLE
Returns
None
void FRAMCtl_disableInterrupt ( uint16_t  interruptMask)

Disables selected FRAMCtl interrupt sources.

Disables the indicated FRAMCtl interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
interruptMaskis the bit mask of the memory buffer interrupt sources to be disabled. Mask value is the logical OR of any of the following:
  • FRAMCTL_PUC_ON_UNCORRECTABLE_BIT - Enable PUC reset if FRAMCtl uncorrectable bit error detected.
  • FRAMCTL_UNCORRECTABLE_BIT_INTERRUPT - Interrupts when an uncorrectable bit error is detected.
  • FRAMCTL_CORRECTABLE_BIT_INTERRUPT - Interrupts when a correctable bit error is detected.
Returns
None
void FRAMCtl_enableInterrupt ( uint8_t  interruptMask)

Enables selected FRAMCtl interrupt sources.

Enables the indicated FRAMCtl interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor. Does not clear interrupt flags.

Parameters
interruptMaskis the bit mask of the memory buffer interrupt sources to be disabled. Mask value is the logical OR of any of the following:
  • FRAMCTL_PUC_ON_UNCORRECTABLE_BIT - Enable PUC reset if FRAMCtl uncorrectable bit error detected.
  • FRAMCTL_UNCORRECTABLE_BIT_INTERRUPT - Interrupts when an uncorrectable bit error is detected.
  • FRAMCTL_CORRECTABLE_BIT_INTERRUPT - Interrupts when a correctable bit error is detected.

Modified bits of GCCTL0 register and bits of FRCTL0 register.

Returns
None
void FRAMCtl_fillMemory32 ( uint32_t  value,
uint32_t *  framPtr,
uint16_t  count 
)

Write data into the fram memory in long format, pass by value.

Parameters
valueis the value to written to FRAMCTL memory
framPtris the pointer into which to write the data
countis the number of 32 bit addresses to fill
Returns
None
uint8_t FRAMCtl_getInterruptStatus ( uint16_t  interruptFlagMask)

Returns the status of the selected FRAMCtl interrupt flags.

Parameters
interruptFlagMaskis a bit mask of the interrupt flags status to be returned. Mask value is the logical OR of any of the following:
  • FRAMCTL_ACCESS_TIME_ERROR_FLAG - Interrupt flag is set if a wrong setting for NPRECHG and NACCESS is set and FRAMCtl access time is not hold.
  • FRAMCTL_UNCORRECTABLE_BIT_FLAG - Interrupt flag is set if an uncorrectable bit error has been detected in the FRAMCtl memory error detection logic.
  • FRAMCTL_CORRECTABLE_BIT_FLAG - Interrupt flag is set if a correctable bit error has been detected and corrected in the FRAMCtl memory error detection logic.
Returns
Logical OR of any of the following:
  • FRAMCtl_ACCESS_TIME_ERROR_FLAG Interrupt flag is set if a wrong setting for NPRECHG and NACCESS is set and FRAMCtl access time is not hold.
  • FRAMCtl_UNCORRECTABLE_BIT_FLAG Interrupt flag is set if an uncorrectable bit error has been detected in the FRAMCtl memory error detection logic.
  • FRAMCtl_CORRECTABLE_BIT_FLAG Interrupt flag is set if a correctable bit error has been detected and corrected in the FRAMCtl memory error detection logic.
    indicating the status of the masked flags
void FRAMCtl_write16 ( uint16_t *  dataPtr,
uint16_t *  framPtr,
uint16_t  numberOfWords 
)

Write data into the fram memory in word format.

Parameters
dataPtris the pointer to the data to be written
framPtris the pointer into which to write the data
numberOfWordsis the number of words to be written
Returns
None
void FRAMCtl_write32 ( uint32_t *  dataPtr,
uint32_t *  framPtr,
uint16_t  count 
)

Write data into the fram memory in long format, pass by reference.

Parameters
dataPtris the pointer to the data to be written
framPtris the pointer into which to write the data
countis the number of 32 bit words to be written
Returns
None
void FRAMCtl_write8 ( uint8_t *  dataPtr,
uint8_t *  framPtr,
uint16_t  numberOfBytes 
)

Write data into the fram memory in byte format.

Parameters
dataPtris the pointer to the data to be written
framPtris the pointer into which to write the data
numberOfBytesis the number of bytes to be written
Returns
None

Copyright 2015, Texas Instruments Incorporated