Data Fields
Graphics_Font Struct Reference

This structure describes a font used for drawing text onto the screen. More...

#include <grlib.h>

Data Fields

uint8_t format
 The format of the font. Can be one of FONT_FMT_UNCOMPRESSED or FONT_FMT_PIXEL_RLE. More...
 
uint8_t maxWidth
 The maximum width of a character; this is the width of the widest character in the font, though any individual character may be narrower than this width. More...
 
uint8_t height
 The height of the character cell; this may be taller than the font data for the characters (to provide inter-line spacing). More...
 
uint8_t baseline
 The offset between the top of the character cell and the baseline of the glyph. The baseline is the bottom row of a capital letter, below which only the descenders of the lower case letters occur. More...
 
uint16_t offset [96]
 The offset within data to the data for each character in the font. More...
 
const uint8_t * data
 A pointer to the data for the font. More...
 

Detailed Description

This structure describes a font used for drawing text onto the screen.

Field Documentation

uint8_t Graphics_Font::format

The format of the font. Can be one of FONT_FMT_UNCOMPRESSED or FONT_FMT_PIXEL_RLE.

Referenced by Graphics_drawString(), and Graphics_getStringWidth().

uint8_t Graphics_Font::maxWidth

The maximum width of a character; this is the width of the widest character in the font, though any individual character may be narrower than this width.

Referenced by Graphics_getFontMaxWidth(), and Graphics_getStringMaxWidth().

uint8_t Graphics_Font::height

The height of the character cell; this may be taller than the font data for the characters (to provide inter-line spacing).

Referenced by Graphics_getFontHeight(), and Graphics_getStringHeight().

uint8_t Graphics_Font::baseline

The offset between the top of the character cell and the baseline of the glyph. The baseline is the bottom row of a capital letter, below which only the descenders of the lower case letters occur.

Referenced by Graphics_drawStringCentered(), Graphics_getFontBaseline(), and Graphics_getStringBaseline().

uint16_t Graphics_Font::offset[96]

The offset within data to the data for each character in the font.

Referenced by Graphics_drawString(), and Graphics_getStringWidth().

const uint8_t* Graphics_Font::data

A pointer to the data for the font.

Referenced by Graphics_drawString(), and Graphics_getStringWidth().


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated